I need pcap and I thought it easiest to just try and build the full image but it doesn't build.
I need a toolchain with pcap and lots of other things in the sysroot so that I can build my application.
I don't need a kernel or rootfs. Just the toolchain.
My target machine is t2080rdb-64b. For a recipe I am trying fsl-image-full and that is what gave the error in the subject.
Perhaps there is another image recipe to choose?
I am using Hob.
thanks,
Kevin
解決済! 解決策の投稿を見る。
Hello Kevin Dankwardt,
I think the package name should be "libpcap" rather than "pcap".
Please check whether the following procedure could help you to implement your purpose.
1. Please install Cache ISO QorIQ-SDK-V1.7-PPC64E6500-CACHE-20141218-yocto.iso and SOURCE ISO QorIQ-SDK-V1.7-SOURCE-20141218-yocto.iso.
2. source ./poky/fsl-setup-poky -m t2080rdb-64b
3. Execute "bitbake fsl-toolchain" to deploy Toolchain environment, and get GCC toolchain deploy environment in build_t2080rdb-64b_release/tmp/sysroots/x86_64-linux/usr/bin/ppc64e6500-fsl-linux/.
4. Execute "bitbake libpcap" and libpcap will be deployed into sysroot environment.
5. Execute "bitbake fsl-image-core" to deploy other package into sysroot.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Kevin Dankwardt,
I think the package name should be "libpcap" rather than "pcap".
Please check whether the following procedure could help you to implement your purpose.
1. Please install Cache ISO QorIQ-SDK-V1.7-PPC64E6500-CACHE-20141218-yocto.iso and SOURCE ISO QorIQ-SDK-V1.7-SOURCE-20141218-yocto.iso.
2. source ./poky/fsl-setup-poky -m t2080rdb-64b
3. Execute "bitbake fsl-toolchain" to deploy Toolchain environment, and get GCC toolchain deploy environment in build_t2080rdb-64b_release/tmp/sysroots/x86_64-linux/usr/bin/ppc64e6500-fsl-linux/.
4. Execute "bitbake libpcap" and libpcap will be deployed into sysroot environment.
5. Execute "bitbake fsl-image-core" to deploy other package into sysroot.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------