Nomenclature of T-Series and P-Series processors.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Nomenclature of T-Series and P-Series processors.

Jump to solution
1,262 Views
Amit-Kumar
Contributor II

Hi Members,

Sorry if this is silly .. but can you please let me know the significance of the digits, what does it say ?
What does '0' and '3' stand for ?

T1023

T1 - Family of processors.
2   -  Two cores.

 Guide me to any related documentation if there is.
This will help us quickly get an intuition of what differs between processors .. like T1024 and T1023.

And does this nomenclature differ for P - Series ? Which follow same suite..

0 Kudos
Reply
1 Solution
1,248 Views
ufedor
NXP Employee
NXP Employee

"3" for T1023 means the silicon personality.

For details refer to the QorIQ T1024 Reference Manual, Appendix B Appendix T1023.

 

Nomenclature is the same for "P" family.

 

View solution in original post

2 Replies
1,239 Views
Amit-Kumar
Contributor II

Okay , Thanks.

0 Kudos
Reply
1,249 Views
ufedor
NXP Employee
NXP Employee

"3" for T1023 means the silicon personality.

For details refer to the QorIQ T1024 Reference Manual, Appendix B Appendix T1023.

 

Nomenclature is the same for "P" family.