I am attempting to secure boot using the p4080 (v2) and U-boot.
when I try to use both the RCW with SB_EN enabled and U-Boot with #define CONFIG_SECBOOT, rebooting the serial console results in the system immediately locking up (I get no output back whatsoever). I have tried waiting for a while thinking that it needs some time to make it to the prompt, but it never happens. To be clear, if I build U-Boot with just CONFIG_SECBOOT (no other modifications) and use the RCW with SB_EN bit set, then the system locks up entirely.
status register of sec mon block (location CCSRBAR +0x314014). : Shows as everything is OK
SCRATCHRW2 register : Shows as everything is OK
Sec Mon in Trusted State (0xd) : So everything is OK
Check the entry point field in the ESBC header : Appears to be okay. I have tried moving it around to different suggested locations and that doesn't seem to get anywhere.
------------
NOTE : If you comment on this question, please don't mark it as 'assumed answered' It feels like the response are slow enough, and that only slows them more..
解決済! 解決策の投稿を見る。
Look at the following pages for secure boot. Do you use this command sequence?
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Yep those are all the steps that I followed for the p4080 I am working with.