Need an optimized memory copy routine for e5500 (t1042)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Need an optimized memory copy routine for e5500 (t1042)

1,343 次查看
michayardeny
Contributor III

We are facing an issue of memory copy speed we used to have an optimized version for P2020 using SPE optimization. On the core we are using now we can't use that kind of optimization and we need something to optimize under the t1042 (32Bit Mode).

标记 (2)
0 项奖励
回复
1 回复

1,227 次查看
Pavel
NXP Employee
NXP Employee

NXP SDK uses memcpy procedure. See the following page:

https://www.embedded.com/design/configurable-systems/4024961/Optimizing-Memcpy-improves-speed

 

Look at also the following page about GCC optimization. Find inline possibility for memcpy.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复