Mounting SD card with FAT32 file system in T1040RDB board through onboard SD card slot.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Mounting SD card with FAT32 file system in T1040RDB board through onboard SD card slot.

6,845件の閲覧回数
abhinavbipnesh
Contributor I

Hi,

Currently I am running fsl-image-core on T1040RDB board using NFS boot. I was trying to mount the SD card (which I have put in on board SD slot). The file system is FAT32 on that card. So I am not able to find how to mount that SD card in the OS. Do I need to re-compile the kernel to support for FAT32 and also SD card.

Please suggest on the same.

-Abhinav

タグ(1)
0 件の賞賛
返信
8 返答(返信)

5,112件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Abhinav Bipnesh,


eSDHC driver and FAT32 filesystem support have already been enabled in the default Kernel configuration file.

After the system boot up, you only need to mount the specific partition, I supposed there is a FAT32 partition /dev/mmcblk0p1 on your SD card.

# mkdir /mnt/sd

# mount -t vfat /dev/mmcblk0p1 /mnt/sd

# ls /mnt/sd/

# cp /bin/busybox /mnt/sd

# ls /mnt/sd

busybox vim

Do you encounter any problem?

The following is Kernel configuration

Device Drivers --->

<*> MMC/SD/SDIO card support ---

>

<*> MMC block device

driver

(8) Number of minors per block device

[*] Use bounce buffer for simple hosts

Enables SD/MMC block device driver support

*** MMC/SD/SDIO Host Controller Drivers

***

<*> Secure Digital Host Controller

Interface support

<*> SDHCI support on OpenFirmware

platforms

[*] SDHCI OF support

FAT32 filesystem suppot

File systems  --->

    DOS/FAT/NT Filesystems  --->

    <*> VFAT (Windows-95) fs support


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

5,112件の閲覧回数
abhinavbipnesh
Contributor I

SHi,

I have already tried to mount SD card with FAT32 but getting below error while trying to mount it.

root@t1040rdb:~# mount /dev/mmcblk0p1

mount: wrong fs type, bad option, bad superblock on /dev/mmcblk0p1,

       missing codepage or helper program, or other error

       In some cases useful info is found in syslog - try

       dmesg | tail or so.

dmesg logs

[   53.505361] FAT-fs (mmcblk0p1): codepage cp437 not found

Even I have verified all the Kernel options which you have suggested and find all the options by default. I have made the module to be present as part of the kernel but still same error I am getting.

Later I have format the card as NTFS and then tried to mount it. We was able to do but getting error while trying to write on it. Below is the output for the same

root@t1040rdb:/media/card# mount

. . .

/dev/mmcblk0p1 on /media/card type ntfs (rw,relatime,sync,uid=0,gid=0,fmask=0177,dmask=077,nls=iso8859-1,errors=continue,mft_zone_multiplier=1)

root@t1040rdb:/media/card# mkdir temp

mkdir: cannot create directory 'temp': Operation not permitted

So any thoughts to fix this issue.

-Abhinav

0 件の賞賛
返信

5,112件の閲覧回数
abhinavbipnesh
Contributor I

I able to solve the error for codepage cp437 for the vfat mount using below option in Kernel config

File Systems --> Native language support

and selecting CP437.

After that rebuild the kernel and boot back and mount the card and it work.

But still not able to get why the default kernel module was not able to detect it (

Along with it how to resolve the issue for NTFS read/write through native drivers or we have to use another one.

Thanks,

Abhinav

0 件の賞賛
返信

5,112件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Abhinav,

I verified the default Kernel on T1040RDB, and could reproduce the codepage problem, the Kernel configuration which your mentioned is necessary.

NTFS file system is also configured in the default Kernel, what problem did you encounter for NTFS?

Thanks,

Yiping

0 件の賞賛
返信

5,112件の閲覧回数
abhinavbipnesh
Contributor I

Hi Yiping,

When tried to mount NTFS based SD card it get mounted out of box. But when I tried to create an directory or try to write some on thing on the device I get an Permission denied error. Same is given below

root@t1040rdb:/media/card# mount

. . .

/dev/mmcblk0p1 on /media/card type ntfs (rw,relatime,sync,uid=0,gid=0,fmask=0177,dmask=077,nls=iso8859-1,errors=continue,mft_zone_multiplier=1)

root@t1040rdb:/media/card# mkdir temp

mkdir: cannot create directory 'temp': Operation not permitted

I have re-configured kernel to have NTFS write support but still same error is being reported. So is we need to have NTFS-3G driver for doing. But I am looking for something from default kernel.

So any thoughts on the same.

-Abhinav

0 件の賞賛
返信

5,112件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Abhinav Bipnesh,

Mounting NTFS file system with read write access permissions, you need to install additional packages such as fuse and ntfs-3g, these packages have been integrated into SDK 1.7.

Please add "ntfs-3g" into the variable "IMAGE_INSTALL" in meta-fsl-networking/images/fsl-image-core.bb, and rebuild the rootfs filesystem.

Then you could use “ntfs-3g  /dev/mmcblk0p1 /mnt/<mount point>”

If further assistance is needed, please feel free to let me know.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

5,112件の閲覧回数
abhinavbipnesh
Contributor I

Hi Yiping,

So we don't have to re-compile the kernel for any additional support? Or even after adding these packages we need to re-configure the kernel for the same.

Thanks,

Abhinav

0 件の賞賛
返信

5,112件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Abhinav Bipnesh,

No need to recompile Kernel, according to your previous description, you have already enabled NTFS_FS and NTFS_RW in Kernel, please add the package "ntfs-3g " and rebuild the filesystem with command "bitbake fsl-image-core".

For any problem, please feel free to let me know.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信