Layerscape PCIe Endpoint Development Boards

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Layerscape PCIe Endpoint Development Boards

4,504 次查看
mikedubya
Contributor I

Are there any NXP or third-party development boards that feature a Layerscape processor such as the LS1021A as a PCIe Endpoint?  All of the NXP development boards focus on the LS processors as PCIe RC.

There is this note here on modifying the LS1046A-RDB board so that mPCIe Slot 2 can be converted from RC to EP mode:

https://community.nxp.com/t5/QorIQ-Knowledge-Base/LS1046A-RDB-in-PCIe-Endpoint-Mode/ta-p/1107415

But even with that change, you would be left with a female mPCIe Slot on the board.  I could not find an adapter that would allow you to connect that mPCIe Slot to a PCIe x1 connector on a desktop PC.

If we wanted to debug a PCIe driver to a Layerscape processor, it would be better to do so on a development board before performing a custom design.

 

0 项奖励
回复
5 回复数

4,492 次查看
mikedubya
Contributor I

Is PCIe EP mode supported on any of the Layerscape processors?  From the KnowledgeBase note, it looks like it is supported on the LS1046.

Related to that, are there any NXP or third-party boards that have a PCIe x1 or x4 interface to a Layerscape processor in PCIe EP mode?

0 项奖励
回复

4,496 次查看
ufedor
NXP Employee
NXP Employee

PCIe EP mode is not supported by LS1021A - refer to the QorIQ LS1021A Reference Manual, 28.2.2 Features:

"Supports Root Complex (RC) mode"

EP mode is not announced.

0 项奖励
回复

4,491 次查看
mikedubya
Contributor I

Is PCIe EP mode supported on any of the Layerscape processors?  From the KnowledgeBase note, it looks like it is supported on the LS1046.

Related to that, are there any NXP or third-party boards that have a PCIe x1 or x4 interface to a Layerscape processor in PCIe EP mode?

0 项奖励
回复

4,480 次查看
mikedubya
Contributor I

Based upon a couple of sources (Table 4 of the Layerscape SDK for Yocto and Linux v5.12-rc7 Documentation/devicetree/bindings/pci/layerscape-pci.txt) it looks like the Layerscape processors that support PCIe EP mode are:

LS1046A
LS1088A
LS2088A
LX2160A (r2)

But I still could not find an NXP or third-party PCIe x1 or x4 development board that exercises this interface.

0 项奖励
回复

4,469 次查看
ufedor
NXP Employee
NXP Employee

I'm not aware about evaluation boards for LS1046A, LS1088A, LS2088A, LX2160A having PCIe EP.

0 项奖励
回复
An error has occurred when reading existing sub-variable "Language_PG_Configuration"; see cause exception! The type of the containing value was: extended_hash+string (lithium.coreapi.webui.template.models.NamedValueByNameTemplateModel wrapped into f.e.b.StringModel) ---- FTL stack trace ("~" means nesting-related): - Failed at: #assign redirect_lingo_page_url = web... [in template "language_macro_header.ftl" at line 173, column 1] - Reached through: #include "language_macro_header.ftl" [in template "Language_translator_Dashboard" at line 3, column 1] ----