LX2162 DPDK dynamic_dpl.sh runs for a long time

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LX2162 DPDK dynamic_dpl.sh runs for a long time

934 Views
embedded_eng_
Contributor III

Hi,

I'm running DPDK on a LX2162 based machine.

SW: LSDK-21.08.

I'm running dynamic_dpl.sh script every boot, and I need it to be as fast as possible.

At the moment, it takes ~20 seconds, is there a way to make it run faster?

Here is the code:

 

export ENABLE_PL_BIT=1
export DPDMAI_COUNT=48
./dynamic_dpl.sh dpmac.5
export DPRC=dprc.2

 

Here is the output:

 

parent - dprc.1
Creating DPRC with PL Bit enabled for RBP usages
Creating Non nested DPRC
NEW DPRCs
dprc.1
  dprc.2
Using board type as 2160
Using High Performance Buffers
MC error: Configuration error (status 0x6)
Invalid --object arg: ''
MC error: Configuration error (status 0x6)
Invalid --object arg: ''
MC error: Configuration error (status 0x6)
Invalid --object arg: ''
MC error: Configuration error (status 0x6)
Invalid --object arg: ''
MC error: Configuration error (status 0x6)
Invalid --object arg: ''
MC error: Configuration error (status 0x6)
Invalid --object arg: ''
MC error: Configuration error (status 0x6)
Invalid --object arg: ''
MC error: Configuration error (status 0x6)
Invalid --object arg: ''
MC error: Configuration error (status 0x6)
Invalid --object arg: ''
MC error: Configuration error (status 0x6)
Invalid --object arg: ''
MC error: Configuration error (status 0x6)
Invalid --object arg: ''
MC error: Configuration error (status 0x6)
Invalid --object arg: ''
MC error: Configuration error (status 0x6)
Invalid --object arg: ''
MC error: Configuration error (status 0x6)
Invalid --object arg: ''
MC error: Configuration error (status 0x6)
Invalid --object arg: ''
MC error: Configuration error (status 0x6)
Invalid --object arg: ''

##################### Container  dprc.2  is created ####################

Container dprc.2 have following resources :=>

 * 3 DPMCP
 * 16 DPBP
 * 8 DPCON
 * 0 DPSECI
 * 1 DPNI
 * 34 DPIO
 * 2 DPCI
 * 48 DPDMAI
 * 0 DPRTC


######################### Configured Interfaces #########################

Interface Name        Endpoint              Mac Address
==============        ========              ==================
dpni.1                dpmac.5               -Dynamic-

 

 

How can I fix these errors?

 

Thanks!

Tags (3)
0 Kudos
Reply
1 Reply

909 Views
yipingwang
NXP TechSupport
NXP TechSupport

I run command "./dynamic_dpl.sh dpmac.5" on LX2160ARDB with LSDK 21.08 images, it took about 10 seconds.

Please make sure that you use the latest MC firmware mc_lx2160a_10.28.1.itb from LSDK 21.08.

0 Kudos
Reply