Hi
I've had issues getting the eth interfaces to work in my LX2160ARDB board.
Booting from lsdk2012_yocto_tiny_LS_arm64.itb brings up no network interfaces at all.
root@TinyLinux:~# ip addr
1: lo: <LOOPBACK,UP,LOWER_UP> mtu 65536 qdisc noqueue qlen 1000
link/loopback 00:00:00:00:00:00 brd 00:00:00:00:00:00
inet 127.0.0.1/8 scope host lo
valid_lft forever preferred_lft forever
inet6 ::1/128 scope host
valid_lft forever preferred_lft forever
2: sit0@NONE: <NOARP> mtu 1480 qdisc noop qlen 1000
link/sit 0.0.0.0 brd 0.0.0.0
Booting native lsdk1906 makes them show up and IP addresses are able to be set, but I cant reach any networks with it.
1906 gives me:
[root@TinyLSDK ~]$ ip addr
1: lo: <LOOPBACK,UP,LOWER_UP> mtu 65536 qdisc noqueue qlen 1000
link/loopback 00:00:00:00:00:00 brd 00:00:00:00:00:00
inet 127.0.0.1/8 scope host lo
valid_lft forever preferred_lft forever
inet6 ::1/128 scope host
valid_lft forever preferred_lft forever
2: sit0@NONE: <NOARP> mtu 1480 qdisc noop qlen 1000
link/sit 0.0.0.0 brd 0.0.0.0
3: eth0: <BROADCAST,MULTICAST> mtu 1500 qdisc noop qlen 1000
link/ether 00:04:9f:05:**:** brd ff:ff:ff:ff:ff:ff
4: eth1: <BROADCAST,MULTICAST> mtu 1500 qdisc noop qlen 1000
link/ether 00:04:9f:05:**:** brd ff:ff:ff:ff:ff:ff
I've tried to load latest 2012 composite FW by following the guide:
tftp a0000000 firmware_lx2160ardb_rev2_uboot_xspiboot.img
sf probe 0:1
sf erase 0 +$filesize && sf write 0xa0000000 0 $filesize
Without result
Solved! Go to Solution.
I rebuilt the firmware with flex-builder and flashed it to xspi as I did in my previous post, and then booted up yocto from xspi
and now ethernet works.
However eth1 and eth0 has swapped ports but otherwise works without issue.
I rebuilt the firmware with flex-builder and flashed it to xspi as I did in my previous post, and then booted up yocto from xspi
and now ethernet works.
However eth1 and eth0 has swapped ports but otherwise works without issue.