Hi,
I am trying to compile the linux5.4 from LSDK19.09.
I tried to use command.
flex-builder -c linux:linux:v5.4 -a arm64
But I got an error about fsl-ls1043a-rdb-sdk.dtb, see below.
make[3]: Entering directory '/home/kaiw/fijowave/fijosat-base/sdk/flexbuild_lsdk1909_update_221019/build/linux/linux/arm64/LS/output/v5.2'
Using /home/kaiw/fijowave/fijosat-base/sdk/flexbuild_lsdk1909_update_221019/packages/linux/linux as source for kernel
make[4]: *** No rule to make target 'arch/arm64/boot/dts/freescale/fsl-ls1043a-rdb-sdk.dtb'. Stop.
I found the targets are defined in flexbuild_lsdk1909_update_221019/packages/linux/Makefile, because I am building the Linux kernel for ls1012a processor, so I commented out the UEFI_DTB_LIST in the Makefile.
UEFI_DTB_LIST = freescale/fsl-ls1043a-rdb-sdk.dtb freescale/fsl-ls1046a-rdb-sdk.dtb freescale/fsl-ls2088a-rdb.dtb freescale/fsl-lx2160a-rdb.dtb
Then I tried to run the flex-builder command again, the build process goes further, but I met the problem with cryptodev_linux, see below.
ERROR: "crypto_givcipher_type" [/home/kaiw/fijowave/fijosat-base/sdk/flexbuild_lsdk1909_update_221019/packages/linux/cryptodev_linux/cryptodev.ko] undefined!
/home/kaiw/fijowave/fijosat-base/sdk/flexbuild_lsdk1909_update_221019/packages/linux/linux/scripts/Makefile.modpost:91: recipe for target '__modpost' failed
Any help will be much appreciated. Thank you.
解決済! 解決策の投稿を見る。
Hello Kai Wu ,
In file configs/build_lsdk.cfg, please disable options CONFIG_KERL_GPU_MODULE
and CONFIG_KERL_CRYPTODEV_LINUX, please refer to the following, then rebuild Linux Kernel.
#CONFIG_KERL_GPU_MODULE=y
#CONFIG_KERL_CRYPTODEV_LINUX=y
Thanks,
Yiping
Hello Kai Wu ,
In file configs/build_lsdk.cfg, please disable options CONFIG_KERL_GPU_MODULE
and CONFIG_KERL_CRYPTODEV_LINUX, please refer to the following, then rebuild Linux Kernel.
#CONFIG_KERL_GPU_MODULE=y
#CONFIG_KERL_CRYPTODEV_LINUX=y
Thanks,
Yiping
Thanks, Yiping, it works.