[LS2160ARDB] Auto Negotiation Off

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

[LS2160ARDB] Auto Negotiation Off

1,121 次查看
kousik_nandi
Contributor I

Dear NXP Folks,

I am working on LS2160ARDB board.
I need to connect the board to a Dell Server.
LS2160ARDB is having a 25G port. Dell server has a 10G port.
When I try to connect them - the connection is unsuccessfull.

When I check the Auto Negotiation parameter the output is confusing via ethtool.

root@localhost:~# ethtool eth3
Settings for eth3:
Supported ports: [ ]
Supported link modes: Not reported
Supported pause frame use: No
Supports auto-negotiation: No
Supported FEC modes: Not reported
Advertised link modes: Not reported
Advertised pause frame use: No
Advertised auto-negotiation: No
Advertised FEC modes: Not reported
Speed: 25000Mb/s
Duplex: Full
Port: Twisted Pair
PHYAD: 0
Transceiver: internal
Auto-negotiation: on
MDI-X: Unknown
Link detected: no

What I observe is that the auto negotiation is on but the Advertised auto-negotiation is no. 
How can i make Advertised auto-negotiation as yes? 

Please help.

Regards
Kousik

标签 (1)
0 项奖励
回复
0 回复数