LS1046ARDB USB console can't work

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1046ARDB USB console can't work

Jump to solution
2,305 Views
anegoiko
Contributor III

Hi,


I got LS1046ARDB and started booting it but the USB console port is not working. All the switches and jumpers are in default mode, but I realized that D8 LED is blinking when I plugged the USB console cable to PC with the board switched off. The D8 LED is off wheen I switch on the board, so I assume that the CMSIS-DAP firmware is not loaded.

Some months ago I worked with LS1043ARDB board and I had a similar problem that I solved following the steps that are in the next thread: LS1043ARDB-PD USB console can't work


However, in this case I could not found the *.bin file in the designer file.


Could somebody provide me the file that I should put in order to program the firmware?


Thanks in advance,

1 Solution
2,128 Views
anegoiko
Contributor III

As penman  says in LS1012a RDB only appears as bootloader? , the firmware binary that is mentioned in the thread https://community.nxp.com/thread/483925  can be used for LS1046ARDB.

I have just tried and it works!

View solution in original post

1 Reply
2,129 Views
anegoiko
Contributor III

As penman  says in LS1012a RDB only appears as bootloader? , the firmware binary that is mentioned in the thread https://community.nxp.com/thread/483925  can be used for LS1046ARDB.

I have just tried and it works!