LS1046ARDB Eval Board 1V Supply - What is the purpose of the sense line resistors?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1046ARDB Eval Board 1V Supply - What is the purpose of the sense line resistors?

Jump to solution
1,328 Views
matthej
Contributor II

Hi,

 

I am looking at the LS1046ARDB eval board which utilizes the LTC7150 1V/0.9V supply. I was confused as to how the VDD sense lines were connected. I have attached the design of this.

What is the purpose of the 0 ohm resistors (R894, R896, and R62)?

Thanks!

 

0 Kudos
1 Solution
1,298 Views
ufedor
NXP Employee
NXP Employee

The zero ohm resistors R894, R896 are added so that the sense path can be isolated if needed. Also if a different resistor value is needed to avoid noise then this resistor pairs were suggested by Linear Technology (analog team).

 

R62 was also recommended by Linear Technology team to be added.

View solution in original post

0 Kudos
3 Replies
1,299 Views
ufedor
NXP Employee
NXP Employee

The zero ohm resistors R894, R896 are added so that the sense path can be isolated if needed. Also if a different resistor value is needed to avoid noise then this resistor pairs were suggested by Linear Technology (analog team).

 

R62 was also recommended by Linear Technology team to be added.

0 Kudos
1,321 Views
ufedor
NXP Employee
NXP Employee

Which exactly schematics is in question?

Please provide complete PDF for inspection.

0 Kudos
1,316 Views
matthej
Contributor II

Sorry its actually the LS1046 FRWY board.

 

See p.7 of attached schematics.

 

Thanks!

0 Kudos