LS1043ardb IFC NAND with 40bit ECC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043ardb IFC NAND with 40bit ECC

1,650 Views
akeshchacko
Contributor II

hi,

For our custom board we are using a MLC NAND flash with minimum required ECC  of 40-bit per 1117 bytes of data. But from the driver files, it support only 4/8-bit ECC. Is there is any option for enabling 40-bit ECC in sdk 0.5??

Tags (1)
0 Kudos
Reply
4 Replies

1,049 Views
akeshchacko
Contributor II

hi pavel,

Our nand have 40-bit ECC, not 4/8-bit. For that i think we need to change nand_ecclayout in both kernel and u-boot. I need some help for finding some variables which i dont know what it means. Those variables are " .eccbytes " inside nand_ecclayout, nand->ecc.size and nand->ecc.bytes (in file fsl_ifc_nand.c).

These are our nand related data

– Page size x8: 8936 bytes (8192 + 744 bytes)

– Block size: 256 pages (2048K + 186K bytes)

– Plane size: 2 planes x 2048 blocks per plane

– 40-bit ECC per 1117 bytes of data

0 Kudos
Reply

1,049 Views
Pavel
NXP Employee
NXP Employee

U-boot for the LS1043A board supports 4-bit and 8-bit ECC. Change the IFC_CSOR for your NAND Flash in u-boot configuration file.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,049 Views
akeshchacko
Contributor II

Hi,

From the reference manual we have seen that it supports 40-bit ECC per sector of 1 KB. But from the driver we have seen that it supports 4/8 bit ECC. Is there is any option for enabling 40-bit ECC in sdk?? Is there is anything that we can refer for this?

0 Kudos
Reply

1,049 Views
Pavel
NXP Employee
NXP Employee

The LS1043 IFC supports BCH code for 4-bit and 8-bit error correction per sector of 512 bytes and 24 and 40-bit ECC per sector of 1 KB.

Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply