LS1043A DDR4 Interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1043A DDR4 Interface

1,007件の閲覧回数
julien_cavallo
Contributor IV

Dear Sir,

 

I develop a custom board with the LS1043A CPU.

 

 I have somes questions about the DDR4 memory interface of the LS1043A CPU.

 

We would like to use 4GB of ddr4 memory for our custom board.

 

For this I have connected two DDR4 MT40A1G16RC-062E_ITB memory (2GB, 1Gbit*16) from Micron on the LS1043A CPU DDR memory interface.

 

My questions:

 

1) Do I use one chip select signal  for the two DDR memory (D1_MCS0_B signal) or two chip select signals (D1_MCS0_B for the first and D1_MCS1_B for the second DDR4) ?


Chapter 2.2.1 of the  "QorIQ LS1043A Reference Manual" said than you can connect only 1 chip select signal.

 

2) There is no problem to use two MT40A1G16RC-062E_ITB memory with the LS1043A CPU ?


Thank is you in advance for your reply.

 

Best regards.

タグ(1)
0 件の賞賛
返信
3 返答(返信)

917件の閲覧回数
ufedor
NXP Employee
NXP Employee

1) One - MCS0

2) It is OK to use two MT40A1G16RC-062E_ITB devices with the LS1043A.

Please refer to the AN5097 - Hardware and Layout Design Considerations for DDR4 SDRAM

0 件の賞賛
返信

917件の閲覧回数
julien_cavallo
Contributor IV

Dear Sir,

Thank you very much. 

With your quick answer my design is finished :smileyhappy:

Best regards

0 件の賞賛
返信

917件の閲覧回数
ufedor
NXP Employee
NXP Employee

LS1043ARDB-PD Design Files are available here:

QorIQ® LS1043A Development Board | NXP 

The RDB board has two memory banks (i.e. MCS0 and MCS1 are used).

0 件の賞賛
返信