LS1043 USB1-3.0can not detect

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043 USB1-3.0can not detect

2,637 Views
allan_yi
Contributor I

please ref the attachment which is the schematic of usb. we found the usb1 port only detect USB2.0,can not detect usb3.0.

the usb3.0 terminal can work on other usb3.0 host.

pastedImage_1.png

0 Kudos
Reply
3 Replies

2,574 Views
Pavel
NXP Employee
NXP Employee

Check the values of the USBx_GHWPARAMS3 and USBx_DCFG registers.

The LS1046a USB register after reset are configured for SuperSpeed mode.

Have a great day,
Pavel Chubakov

 

 

0 Kudos
Reply

2,574 Views
Pavel
NXP Employee
NXP Employee

Check your board using attached files. These files contains documentation and schematic for the LS1043ARDB USB and layout guidelines for high-speed interfaces (USB, PCI).

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,574 Views
allan_yi
Contributor I

we had checked the schematic and compare with the reference design of LS1043RDB,however,we did not found any problem.

whether do some configs abou software or not? such as rcw or Register

0 Kudos
Reply