LS1028ARDB Deploying BSP images using removable storage

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1028ARDB Deploying BSP images using removable storage

12,617件の閲覧回数
jeremy_impson
Contributor III

I'm working through the Layerscape LS1028A BSP User Guide, Rev. 0.3, 04/2019, section 3.1.4.2 Option 1 - Deploy LS1028A BSP images using removable storage device . There are what appear to be some errors in this section, which I've detailed in another post.(https://community.nxp.com/thread/514671)

I've built two such bootable removable SD cards. Both came with the Layerscape units that I bought, and both are Kingston brand Canvas Select 16 GB cards (SDS/16GB). I've had no problems reading and writing from them from my Ubuntu host PC. But every time I boot from them on the Layerscape box, there are the following I/O errors:

print_req_error: I/O error, dev mmcblk0 sector 1228801

Buffer I/O error on dev mmcblk0p2, logical block 131072, lost sync page write

The sector number will vary, the logical block number will vary, the device might be mmcblk0p3, and sometimes it says "lost async page write" instead of "lost sync page write".

Sometimes there is an accompanying filesystem error:

JBD2: Error -5 detected when updating journal superblock for mmcblk0ps-8

Aborting journal on device mmcblk0p2-8.

The referenced device will vary.

These errors will either cause the system boot up process to dump into emergency / maintenance mode, or other times it seems to boot correctly but then the root filesystem gets marked readonly. They have never booted up without these I/O and journal errors, which will continue at random intervals after boot.

We have had no issue with reads or writes on these SD cards under the Ubuntu host PC or on another Windows PC. We have even reformatted one of the cards with the SD Associaton's official Formatter Tool (https://www.sdcard.org/downloads/formatter/). Nothing else has had any issue with reading or writing these cards.

I do have four more cards (because we bought six total Layerscape LS1028ARDB boards and got one card with each). Is it worth my time to try out every one to find one that works with these boards? I am getting the feeling that the LS1028ARDB is a very new product, and that the documentation and perhaps the software are not ready for prime time. My suspicion is that the problem lies in the MMC driver software, although I assume that since these cards came with the units, they are expected to be compatible.

The output of uname -a on the system that I've built is Linux localhost 4.14.47 #1 SMP PREEMPTY Tue Apr 16 22:18:43 CST 2019 aarch64 aarch64 aarch64 GNU/Linux.

I am simultaneously working through section 3.1.4.3 Option 2 - Deploy BSP images directly to the storage device on a board.but as described in yet another forum post (https://community.nxp.com/thread/514775), I've encountered roadblocks there as well.

Incidentally, all these cards arrived with stickers on the back that say "BSP 0.1-pre" on them. The two I have looked at were formatted and had empty filesystems, however.

タグ(3)
0 件の賞賛
返信
9 返答(返信)

12,147件の閲覧回数
jeremy_impson
Contributor III

Thanks for your reply, Yiping,

I will add the console logs you've requested as separate replies. Here's a summary of what happened.

(host-console-flex-installer.txt) I ran the flex-installer command on my host PC successfully. I had to provide a relative path to the rootfs image, and the SD card device on my host PC is /dev/sdc because I used an SD card reader/writer. When finished I showed the partitions and contents of each.

(target-console-uboot-first-hung.log) I placed the SD card into the LS1028ARDB unit and interrupted the boot. I ran the "load mmc..." command and got an error as you'll see in the log. I carried on and ran the remaining uboot commands, including the "mmc write..." command. When I entered the qixis_reset sd command, the system was unresponsive. I waited 5 minutes before shutting down the unit to remove the card.

(host-console-after-uboot-first-hung.txt) I put the card back into the Host PC to look at it. Note that the first partition got corrupted and no longer mounts, but the second and third are fine. I assume this is due to the failures of the "load mmc..." command followed by the "mmc write..." command.

Please note that I already have a workaround for the "load mmc..." failure, and when using it I am able to boot my Ubuntu rootfs, and that is when I get the mmc device and JBD2 errors that I have reported in the original post of this thread.

My workaround is that when I run flex-installer, I add "-f firmware_ls1028ardb_uboot_sdboot.img" to the command line. I've since found out from Pavel Chubakov that I can also just use the command "sudo dd if=firmware...img of=/dev/sdc bs=512 seek=8" if I've already run the installer without the "-f" flag. So I recreated the SD card this way, but did not capture a log of that process.

(target-console-succesful-boot-io-errors.log) Then I put the re-imaged SDcard into the unit, rebooted, and stopped the boot. I typed the following uboot commands: mmc rescan; mmc dev 0; qixis_reset sd; This booted the MMC device 0 but as you can see at the end, there were the I/O errors as I described in my post above.

In previous attempts, sometimes the boot will get as far as attempting to start Services but then fails into a Ubuntu's Emergency/Maintenance mode, but this time it looks like there was an I/O error so early in boot that the services were not attempted, and the kernel just remounted the root as readonly and dropped me into a shell.

I'm beginning to think that my SD cards are just bad. I have 6 units all together, therefore 6 cards. Two cards are bad. I will try the rest.

0 件の賞賛
返信

12,147件の閲覧回数
jeremy_impson
Contributor III

target-console-succesful-boot-io-errors.log

=~=~=~=~=~=~=~=~=~=~=~= PuTTY log 2019.10.16 18:25:19 =~=~=~=~=~=~=~=~=~=~=~=


U-Boot 2018.03-00139-ge124969f47-dirty (Dec 20 2018 - 15:22:43 +0530)

SoC: LS1028AE Rev1.0 (0x870b0010)
Clock Configuration:
CPU0(A72):1300 MHz CPU1(A72):1300 MHz
Bus: 400 MHz DDR: 1600 MT/s
Reset Configuration Word (RCW):
00000000: 34004010 00000030 00000000 00000000
00000010: 00000000 008f0000 0030c000 00000000
00000020: 006031a0 00002580 00000000 00003296
00000030: 00000000 00000010 00000000 00000000
00000040: 00000000 00000000 00000000 00000000
00000050: 00000000 00000000 00000000 00000000
00000060: 00000000 00000000 20067054 00000000
00000070: bb580000 00000000
Model: NXP Layerscape 1028a RDB Board
Board: LS1028AE Rev1.0-RDB, Version: A, boot from NOR
FPGA: v6 (RELEASED: RDB_2018_1206_2148)
SERDES1 Reference : Clock1 = 100.00MHz Clock2 = 100.00MHz
I2C: ready
DRAM: Initializing DDR....
Detected UDIMM Fixed DDR on board
3.9 GiB
DDR 3.9 GiB (DDR4, 32-bit, CL=11, ECC on)
PPA Firmware: Version LSDK-18.09
Using SERDES1 Protocol: 47960 (0xbb58)
PCIe0: pcie@3400000 Root Complex: no link
PCIe1: pcie@3500000 Root Complex: no link
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from SPI Flash... SF: Detected mt35xu02g with page size 256 Bytes, erase size 128 KiB, total 2 GiB
OK
In: serial
Out: serial
Err: serial
Net: eth0: enetc#0
Warning: enetc#1 (eth1) using random MAC address - fe:ec:e4:6e:d5:b0
, eth1: enetc#1, eth2: enetc#2, eth3: netc_mdio
MDIO MUX: no MDIO MUX node
Hit any key to stop autoboot: 0 0
=> mmc rescan
=> mmc dev 0
switch to partitions #0, OK
mmc0 is current device
=> ls mmc 0:1

0 file(s), 0 dir(s)

=> ls mmc 0:1 2
<DIR> 4096 .
<DIR> 4096 ..
<DIR> 16384 lost+found
163946 config-4.14.47
22327 fsl-ls1028a-qds.dtb
20586 fsl-ls1028a-rdb.dtb
2176 hdr_ls1028aqds_bs.out
2176 hdr_ls1028ardb_bs.out
22776320 Image
9930242 Image.gz
992 ls1028aqds_boot.scr
992 ls1028ardb_boot.scr
19710564 lsdk_linux_arm64_LS_tiny.itb
9572804 ramdisk_rootfs_arm64.ext4.gz
<DIR> 4096 secboot_hdrs
992 srk_hash.txt
9930242 vmlinuz-4.14.47
=> ls mmc 0:2 3
<DIR> 4096 .
<DIR> 4096 ..
<DIR> 16384 lost+found
<DIR> 4096 bin
<DIR> 4096 boot
<DIR> 4096 dev
<DIR> 4096 etc
<DIR> 4096 home
<DIR> 4096 lib
<DIR> 4096 media
<DIR> 4096 mnt
<DIR> 4096 opt
<DIR> 4096 proc
<DIR> 4096 root
<DIR> 4096 run
<DIR> 4096 sbin
<DIR> 4096 srv
<DIR> 4096 sys
<DIR> 4096 tmp
<DIR> 4096 usr
<DIR> 4096 var
=> qixis_reset sd
=> NOTICE: Fixed DDR on board

NOTICE: 4 GB DDR4, 32-bit, CL=11, ECC on
NOTICE: BL2: v1.5(release):ls1028a-early-access-bsp0.3
NOTICE: BL2: Built : 13:05:19, Oct 7 2019
NOTICE: BL2: Booting BL31 NOTICE: BL31: v1.5(release):ls1028a-early-access-bsp0.3
NOTICE: BL31: Built : 13:05:24, Oct 7 2019
NOTICE: Welcome to LS1028 BL31 Phase


U-Boot 2018.09 (Oct 07 2019 - 13:04:43 -0400)

SoC: LS1028AE Rev1.0 (0x870b0010)
Clock Configuration:
CPU0(A72):1300 MHz CPU1(A72):1300 MHz
Bus: 400 MHz DDR: 1600 MT/s
Reset Configuration Word (RCW):
00000000: 34004010 00000030 00000000 00000000
00000010: 00000000 00bf0000 0030c000 00000000
00000020: 02403150 00002580 00000000 00003496
00000030: 00000000 00000010 00000000 00000000
00000040: 00000000 00000000 00000000 00000000
00000050: 00000000 00000000 00000000 00000000
00000060: 00000000 00000000 200e705a 00000000
00000070: bb580000 00000000
Model: NXP Layerscape 1028a RDB Board
Board: LS1028AE Rev1.0-RDB, Version: A, boot from SD
FPGA: v6 (RELEASED: RDB_2018_1206_2148)
SERDES1 Reference : Clock1 = 100.00MHz Clock2 = 100.00MHz
I2C: ready
DRAM: 3.9 GiB
DDR 3.9 GiB (DDR4, 32-bit, CL=11, ECC on)
Using SERDES1 Protocol: 47960 (0xbb58)
PCIe0: pcie@3400000 Root Complex: no link
PCIe1: pcie@3500000 Root Complex: no link
Now running in RAM - U-Boot at: fbd3f000
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... *** Warning - bad CRC, using default environment

EEPROM: Read failed.
In: serial
Out: serial
Err: serial
Net:
Warning: enetc#0 (eth0) using random MAC address - 46:c4:61:e0:8a:d1
eth0: enetc#0
Warning: enetc#1 (eth1) using random MAC address - 4e:cc:48:9a:06:dd
, eth1: enetc#1
Warning: enetc#2 (eth2) using random MAC address - aa:cb:0b:df:f9:49
, eth2: enetc#2
Warning: netc_mdio (eth3) using random MAC address - 00:00:00:00:00:00
, eth3: netc_mdio
Warning: enetc#3 (eth4) using random MAC address - 9a:98:df:05:9c:4d
, eth4: enetc#3
MDIO MUX: no MDIO MUX node
Hit any key to stop autoboot: 10 9 8 7 6 5 4 3 2 1 0
Trying load HDP firmware from SD..
Device: FSL_SDHC
Manufacturer ID: 41
OEM: 3432
Name: SD16G
Bus Speed: 50000000
Mode : SD High Speed (50MHz)
Rd Block Len: 512
SD version 3.0
High Capacity: Yes
Capacity: 14.5 GiB
Bus Width: 4-bit
Erase Group Size: 512 Bytes

MMC read: dev # 0, block # 18432, count 512 ... 512 blocks read: OK
Loading hdp firmware from 0x00000000a0000000 offset 0x0000000000002000
Loading hdp firmware Complete
switch to partitions #0, OK
mmc0 is current device
Scanning mmc 0:1...
Scanning mmc 0:2...
Found U-Boot script /ls1028ardb_boot.scr
992 bytes read in 6 ms (161.1 KiB/s)
## Executing script at 80000000
22776320 bytes read in 973 ms (22.3 MiB/s)
20586 bytes read in 9 ms (2.2 MiB/s)
## Flattened Device Tree blob at 90000000
Booting using the fdt blob at 0x90000000
Using Device Tree in place at 0000000090000000, end 0000000090008069
NOTICE: RNG: INSTANTIATED

Starting kernel ...

[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 4.14.47 (jenkins@saturn) (gcc version 7.3.0 (Ubuntu/Linaro 7.3.0-16ubuntu3)) #1 SMP PREEMPT Tue Apr 16 22:18:43 CST 2019
[ 0.000000] Boot CPU: AArch64 Processor [410fd083]
[ 0.000000] Machine model: LS1028A RDB Board
[ 0.000000] earlycon: uart8250 at MMIO 0x00000000021c0500 (options '')
[ 0.000000] bootconsole [uart8250] enabled
[ 0.000000] efi: Getting EFI parameters from FDT:
[ 0.000000] efi: UEFI not found.
[ 0.000000] cma: Reserved 256 MiB at 0x00000000ebc00000
[ 0.000000] NUMA: No NUMA configuration found
[ 0.000000] NUMA: Faking a node at [mem 0x0000000000000000-0x00000020ffffffff]
[ 0.000000] NUMA: NODE_DATA [mem 0x20fffd7a80-0x20fffd923f]
[ 0.000000] Zone ranges:
[ 0.000000] DMA [mem 0x0000000080000000-0x00000000ffffffff]
[ 0.000000] Normal [mem 0x0000000100000000-0x00000020ffffffff]
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000080000000-0x00000000fbdfffff]
[ 0.000000] node 0: [mem 0x0000002080000000-0x00000020ffffffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000020ffffffff]
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: MIGRATE_INFO_TYPE not supported.
[ 0.000000] psci: SMC Calling Convention v1.1
[ 0.000000] percpu: Embedded 24 pages/cpu @ffff80207ffa2000 s59992 r8192 d30120 u98304
[ 0.000000] Detected PIPT I-cache on CPU0
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 1015296
[ 0.000000] Policy zone: Normal
[ 0.000000] Kernel command line: console=ttyS0,115200 earlycon=uart8250,mmio,0x21c0500 root=PARTUUID=ff2452c7-03 rw rootwait video=1920x1080-32@60 cma=256M
[ 0.000000] PID hash table entries: 4096 (order: 3, 32768 bytes)
[ 0.000000] software IO TLB [mem 0xe7c00000-0xebc00000] (64MB) mapped at [ffff800067c00000-ffff80006bbfffff]
[ 0.000000] Memory: 3709404K/4126720K available (13756K kernel code, 1570K rwdata, 5676K rodata, 1216K init, 975K bss, 155172K reserved, 262144K cma-reserved)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] modules : 0xffff000000000000 - 0xffff000008000000 ( 128 MB)
[ 0.000000] vmalloc : 0xffff000008000000 - 0xffff7dffbfff0000 (129022 GB)
[ 0.000000] .text : 0xffff000008080000 - 0xffff000008df0000 ( 13760 KB)
[ 0.000000] .rodata : 0xffff000008df0000 - 0xffff000009380000 ( 5696 KB)
[ 0.000000] .init : 0xffff000009380000 - 0xffff0000094b0000 ( 1216 KB)
[ 0.000000] .data : 0xffff0000094b0000 - 0xffff000009638a00 ( 1571 KB)
[ 0.000000] .bss : 0xffff000009638a00 - 0xffff00000972c8e8 ( 976 KB)
[ 0.000000] fixed : 0xffff7dfffe7f9000 - 0xffff7dfffec00000 ( 4124 KB)
[ 0.000000] PCI I/O : 0xffff7dfffee00000 - 0xffff7dffffe00000 ( 16 MB)
[ 0.000000] vmemmap : 0xffff7e0000000000 - 0xffff800000000000 ( 2048 GB maximum)
[ 0.000000] 0xffff7e0000000000 - 0xffff7e0082000000 ( 2080 MB actual)
[ 0.000000] memory : 0xffff800000000000 - 0xffff802080000000 (133120 MB)
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] RCU restricting CPUs from NR_CPUS=64 to nr_cpu_ids=2.
[ 0.000000] Tasks RCU enabled.
[ 0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000] GICv3: no VLPI support, no direct LPI support
[ 0.000000] ITS [mem 0x06020000-0x0603ffff]
[ 0.000000] ITS@0x0000000006020000: allocated 65536 Devices @20fb880000 (flat, esz 8, psz 64K, shr 0)
[ 0.000000] ITS: using cache flushing for cmd queue
[ 0.000000] GIC: using LPI property table @0x00000020fb830000
[ 0.000000] ITS: Allocated 1792 chunks for LPIs
[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000006040000
[ 0.000000] CPU0: using LPI pending table @0x00000020fb840000
[ 0.000000] GIC: using cache flushing for LPI property table
[ 0.000000] arch_timer: cp15 timer(s) running at 25.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x5c409fb33, max_idle_ns: 440795203156 ns
[ 0.000002] sched_clock: 56 bits at 25MHz, resolution 39ns, wraps every 4398046511103ns
[ 0.008384] Console: colour dummy device 80x25
[ 0.012906] Calibrating delay loop (skipped), value calculated using timer frequency.. 50.00 BogoMIPS (lpj=100000)
[ 0.023375] pid_max: default: 32768 minimum: 301
[ 0.028102] Security Framework initialized
[ 0.034058] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes)
[ 0.042356] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes)
[ 0.049538] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.056343] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.079595] ASID allocator initialised with 32768 entries
[ 0.085096] Hierarchical SRCU implementation.
[ 0.097547] PCI/MSI: /interrupt-controller@6000000/gic-its@6020000 domain created
[ 0.105181] Platform MSI: /interrupt-controller@6000000/gic-its@6020000 domain created
[ 0.113218] fsl-mc MSI: /interrupt-controller@6000000/gic-its@6020000 domain created
[ 0.121302] EFI services will not be available.
[ 0.133893] smp: Bringing up secondary CPUs ...
[ 0.166618] Detected PIPT I-cache on CPU1
[ 0.166637] GICv3: CPU1: found redistributor 1 region 0:0x0000000006060000
[ 0.166693] CPU1: using LPI pending table @0x00000020fb3b0000
[ 0.166711] CPU1: Booted secondary processor [410fd083]
[ 0.166754] smp: Brought up 1 node, 2 CPUs
[ 0.193005] SMP: Total of 2 processors activated.
[ 0.197764] CPU features: detected feature: GIC system register CPU interface
[ 0.204981] CPU features: detected feature: 32-bit EL0 Support
[ 0.210875] CPU features: detected feature: Kernel page table isolation (KPTI)
[ 0.223167] CPU: All CPU(s) started at EL2
[ 0.227314] alternatives: patching kernel code
[ 0.232398] devtmpfs: initialized
[ 0.237515] random: get_random_u32 called from bucket_table_alloc+0x108/0x258 with crng_init=0
[ 0.246494] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.256365] futex hash table entries: 512 (order: 3, 32768 bytes)
[ 0.266078] xor: measuring software checksum speed
[ 0.310282] 8regs : 5541.000 MB/sec
[ 0.354307] 8regs_prefetch: 4821.000 MB/sec
[ 0.398331] 32regs : 6231.000 MB/sec
[ 0.442356] 32regs_prefetch: 5265.000 MB/sec
[ 0.447020] xor: using function: 32regs (6231.000 MB/sec)
[ 0.452482] pinctrl core: initialized pinctrl subsystem
[ 0.458625] DMI not present or invalid.
[ 0.462720] NET: Registered protocol family 16
[ 0.471238] cpuidle: using governor menu
[ 0.475560] vdso: 2 pages (1 code @ ffff000008df6000, 1 data @ ffff0000094b5000)
[ 0.483201] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.490595] DMA: preallocated 256 KiB pool for atomic allocations
[ 0.497049] Serial: AMBA PL011 UART driver
[ 0.520477] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.593371] raid6: int64x1 gen() 869 MB/s
[ 0.665749] raid6: int64x1 xor() 626 MB/s
[ 0.738153] raid6: int64x2 gen() 1388 MB/s
[ 0.810511] raid6: int64x2 xor() 1049 MB/s
[ 0.882903] raid6: int64x4 gen() 1958 MB/s
[ 0.955281] raid6: int64x4 xor() 1170 MB/s
[ 1.027336] raid6: int64x8 gen() 1702 MB/s
[ 1.099352] raid6: int64x8 xor() 1150 MB/s
[ 1.171394] raid6: neonx1 gen() 1673 MB/s
[ 1.243436] raid6: neonx1 xor() 1563 MB/s
[ 1.315478] raid6: neonx2 gen() 2578 MB/s
[ 1.387503] raid6: neonx2 xor() 2277 MB/s
[ 1.459556] raid6: neonx4 gen() 3469 MB/s
[ 1.531588] raid6: neonx4 xor() 2522 MB/s
[ 1.603624] raid6: neonx8 gen() 3187 MB/s
[ 1.675662] raid6: neonx8 xor() 2675 MB/s
[ 1.679979] raid6: using algorithm neonx4 gen() 3469 MB/s
[ 1.685435] raid6: .... xor() 2522 MB/s, rmw enabled
[ 1.690454] raid6: using neon recovery algorithm
[ 1.695348] ACPI: Interpreter disabled.
[ 1.701381] vgaarb: loaded
[ 1.704295] SCSI subsystem initialized
[ 1.708288] usbcore: registered new interface driver usbfs
[ 1.714041] usbcore: registered new interface driver hub
[ 1.719442] usbcore: registered new device driver usb
[ 1.724787] imx-i2c 2000000.i2c: fsl-scl-gpio not found
[ 1.730112] imx-i2c 2000000.i2c: can't get pinctrl, bus recovery not supported
[ 1.737548] i2c i2c-0: IMX I2C adapter registered
[ 1.742312] i2c i2c-0: can't use DMA, using PIO instead.
[ 1.747966] pps_core: LinuxPPS API ver. 1 registered
[ 1.752991] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <[email protected]>
[ 1.762258] PTP clock support registered
[ 1.766292] EDAC MC: Ver: 3.0.0
[ 1.769659] dmi: Firmware registration failed.
[ 1.774253] No BMan portals available!
[ 1.778364] QMan: Allocated lookup table at ffff00000aecd000, entry count 65537
[ 1.785852] No QMan portals available!
[ 1.789747] No USDPAA memory, no 'fsl,usdpaa-mem' in device-tree
[ 1.796142] Advanced Linux Sound Architecture Driver Initialized.
[ 1.802717] clocksource: Switched to clocksource arch_sys_counter
[ 1.808975] VFS: Disk quotas dquot_6.6.0
[ 1.812976] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 1.820000] pnp: PnP ACPI: disabled
[ 1.826772] NET: Registered protocol family 2
[ 1.831511] TCP established hash table entries: 32768 (order: 6, 262144 bytes)
[ 1.838978] TCP bind hash table entries: 32768 (order: 7, 524288 bytes)
[ 1.845976] TCP: Hash tables configured (established 32768 bind 32768)
[ 1.852665] UDP hash table entries: 2048 (order: 4, 65536 bytes)
[ 1.858780] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes)
[ 1.865410] NET: Registered protocol family 1
[ 1.869986] RPC: Registered named UNIX socket transport module.
[ 1.876016] RPC: Registered udp transport module.
[ 1.880776] RPC: Registered tcp transport module.
[ 1.885532] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 1.892430] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available
[ 1.900381] kvm [1]: 8-bit VMID
[ 1.904316] kvm [1]: GICv3: no GICV resource entry
[ 1.909164] kvm [1]: disabling GICv2 emulation
[ 1.913671] kvm [1]: GIC system register CPU interface enabled
[ 1.919594] kvm [1]: vgic interrupt IRQ1
[ 1.923618] kvm [1]: Hyp mode initialized successfully
[ 1.930310] audit: initializing netlink subsys (disabled)
[ 1.935837] audit: type=2000 audit(1.835:1): state=initialized audit_enabled=0 res=1
[ 1.938750] workingset: timestamp_bits=44 max_order=20 bucket_order=0
[ 1.943936] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 1.948057] NFS: Registering the id_resolver key type
[ 1.948067] Key type id_resolver registered
[ 1.948068] Key type id_legacy registered
[ 1.948074] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 1.948143] fuse init (API version 7.26)
[ 1.948231] 9p: Installing v9fs 9p2000 file system support
[ 1.949781] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245)
[ 1.953886] io scheduler noop registered
[ 1.953912] io scheduler cfq registered (default)
[ 1.953914] io scheduler mq-deadline registered
[ 1.953915] io scheduler kyber registered
[ 1.957269] Galcore version 6.2.4.163672
[ 2.052397] OF: PCI: host bridge /soc/pcie@1f0000000 ranges:
[ 2.058144] OF: PCI: MEM 0x1f8000000..0x1f815ffff -> 0x00000000
[ 2.064349] OF: PCI: MEM 0x1f8160000..0x1f81cffff -> 0x00000000
[ 2.070520] OF: PCI: MEM 0x1f81d0000..0x1f81effff -> 0x00000000
[ 2.076691] OF: PCI: MEM 0x1f81f0000..0x1f820ffff -> 0x00000000
[ 2.082859] OF: PCI: MEM 0x1f8210000..0x1f822ffff -> 0x00000000
[ 2.089026] OF: PCI: MEM 0x1f8230000..0x1f824ffff -> 0x00000000
[ 2.095196] OF: PCI: MEM 0x1fc000000..0x1fc3fffff -> 0x00000000
[ 2.101404] pci-host-generic 1f0000000.pcie: ECAM at [mem 0x1f0000000-0x1f00fffff] for [bus 00]
[ 2.110277] pci-host-generic 1f0000000.pcie: PCI host bridge to bus 0000:00
[ 2.117325] pci_bus 0000:00: root bus resource [bus 00]
[ 2.122617] pci_bus 0000:00: root bus resource [mem 0x1f8000000-0x1f815ffff] (bus address [0x00000000-0x0015ffff])
[ 2.133090] pci_bus 0000:00: root bus resource [mem 0x1f8160000-0x1f81cffff pref] (bus address [0x00000000-0x0006ffff])
[ 2.144008] pci_bus 0000:00: root bus resource [mem 0x1f81d0000-0x1f81effff] (bus address [0x00000000-0x0001ffff])
[ 2.154482] pci_bus 0000:00: root bus resource [mem 0x1f81f0000-0x1f820ffff pref] (bus address [0x00000000-0x0001ffff])
[ 2.165391] pci_bus 0000:00: root bus resource [mem 0x1f8210000-0x1f822ffff] (bus address [0x00000000-0x0001ffff])
[ 2.175867] pci_bus 0000:00: root bus resource [mem 0x1f8230000-0x1f824ffff pref] (bus address [0x00000000-0x0001ffff])
[ 2.186776] pci_bus 0000:00: root bus resource [mem 0x1fc000000-0x1fc3fffff] (bus address [0x00000000-0x003fffff])
[ 2.197338] pci 0000:00:00.0: VF(n) BAR0 space: [mem 0x1f81d0000-0x1f81effff 64bit] (contains BAR0 for 2 VFs)
[ 2.207374] pci 0000:00:00.0: VF(n) BAR2 space: [mem 0x1f81f0000-0x1f820ffff 64bit pref] (contains BAR2 for 2 VFs)
[ 2.218011] pci 0000:00:00.1: VF(n) BAR0 space: [mem 0x1f8210000-0x1f822ffff 64bit] (contains BAR0 for 2 VFs)
[ 2.228044] pci 0000:00:00.1: VF(n) BAR2 space: [mem 0x1f8230000-0x1f824ffff 64bit pref] (contains BAR2 for 2 VFs)
[ 2.239300] /soc/pcie@1f0000000: Invalid msi-map translation - no match for rid 0xf8 on (null)
[ 2.249251] OF: PCI: host bridge /soc/pcie@3400000 ranges:
[ 2.254812] OF: PCI: IO 0x8000010000..0x800001ffff -> 0x00000000
[ 2.261158] OF: PCI: MEM 0x8040000000..0x807fffffff -> 0x40000000
[ 2.267594] layerscape-pcie 3400000.pcie: PCI host bridge to bus 0001:00
[ 2.274378] pci_bus 0001:00: root bus resource [bus 00-ff]
[ 2.279925] pci_bus 0001:00: root bus resource [io 0x0000-0xffff]
[ 2.286178] pci_bus 0001:00: root bus resource [mem 0x8040000000-0x807fffffff] (bus address [0x40000000-0x7fffffff])
[ 2.297051] pci 0001:00:00.0: BAR 6: assigned [mem 0x8040000000-0x80400007ff pref]
[ 2.304718] pci 0001:00:00.0: PCI bridge to [bus 01]
[ 2.309862] pcieport 0001:00:00.0: Signaling PME with IRQ 92
[ 2.315661] pcieport 0001:00:00.0: AER enabled with IRQ 93
[ 2.321369] OF: PCI: host bridge /soc/pcie@3500000 ranges:
[ 2.326934] OF: PCI: IO 0x8800010000..0x880001ffff -> 0x00000000
[ 2.333277] OF: PCI: MEM 0x8840000000..0x887fffffff -> 0x40000000
[ 2.339703] layerscape-pcie 3500000.pcie: PCI host bridge to bus 0002:00
[ 2.346484] pci_bus 0002:00: root bus resource [bus 00-ff]
[ 2.352038] pci_bus 0002:00: root bus resource [io 0x10000-0x1ffff] (bus address [0x0000-0xffff])
[ 2.361100] pci_bus 0002:00: root bus resource [mem 0x8840000000-0x887fffffff] (bus address [0x40000000-0x7fffffff])
[ 2.371963] pci 0002:00:00.0: BAR 6: assigned [mem 0x8840000000-0x88400007ff pref]
[ 2.379625] pci 0002:00:00.0: PCI bridge to [bus 01]
[ 2.384756] pcieport 0002:00:00.0: Signaling PME with IRQ 94
[ 2.390578] pcieport 0002:00:00.0: AER enabled with IRQ 95
[ 2.398346] Freescale LS2 console driver
[ 2.402400] fsl-ls2-console: device fsl_mc_console registered
[ 2.408257] fsl-ls2-console: device fsl_aiop_console registered
[ 2.417046] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 2.424535] console [ttyS0] disabled
[ 2.428185] 21c0500.serial: ttyS0 at MMIO 0x21c0500 (irq = 86, base_baud = 12500000) is a 16550A
[ 2.437100] console [ttyS0] enabled
[ 2.437100] console [ttyS0] enabled
[ 2.444393] bootconsole [uart8250] disabled
[ 2.444393] bootconsole [uart8250] disabled
[ 2.453159] 21c0600.serial: ttyS1 at MMIO 0x21c0600 (irq = 86, base_baud = 12500000) is a 16550A
[ 2.462297] SuperH (H)SCI(F) driver initialized
[ 2.467038] msm_serial: driver initialized
[ 2.471955] arm-smmu 5000000.iommu: probing hardware configuration...
[ 2.478431] arm-smmu 5000000.iommu: SMMUv2 with:
[ 2.483066] arm-smmu 5000000.iommu: stage 1 translation
[ 2.488400] arm-smmu 5000000.iommu: stage 2 translation
[ 2.493734] arm-smmu 5000000.iommu: nested translation
[ 2.498986] arm-smmu 5000000.iommu: stream matching with 128 register groups
[ 2.506152] arm-smmu 5000000.iommu: 64 context banks (0 stage-2 only)
[ 2.512710] arm-smmu 5000000.iommu: Supported page sizes: 0x61311000
[ 2.519176] arm-smmu 5000000.iommu: Stage-1: 48-bit VA -> 48-bit IPA
[ 2.525644] arm-smmu 5000000.iommu: Stage-2: 48-bit IPA -> 48-bit PA
[ 2.533181] [drm] found ARM Mali-DP500 version r1p2
[ 2.538219] [drm] Resolution 3840x2160@60 is enabled
[ 2.543208] [drm] Resolution 1920x1080@60 is enabled
[ 2.548192] [drm] Resolution 1280x720@60 is enabled
[ 2.553090] [drm] Resolution 720x480@60 is enabled
[ 2.557901] i.mx8-hdp f1f0000.phy: lane_mapping 0x4e
[ 2.562887] i.mx8-hdp f1f0000.phy: edp_link_rate 0x06
[ 2.567958] i.mx8-hdp f1f0000.phy: dp_num_lanes 0x04
[ 2.573105] [drm] Started firmware!
[ 2.576608] [drm] CDN_API_CheckAlive returned ret = 0
[ 2.581678] [drm] Firmware version: 23029, Lib version: 20691
[ 2.587465] [drm] CDN_API_MainControl_blocking (ret = 0 resp = 1)
[ 2.593615] [drm] CDN_API_General_Test_Echo_Ext_blocking (ret = 0 echo_resp = echo test)
[ 2.601746] [drm] CDN_API_General_Write_Register_blockin ... setting LANES_CONFIG
[ 2.609317] [drm] pixel engine reset
[ 2.612913] [drm] CDN_*_Write_Register_blocking ... setting LANES_CONFIG 4e
[ 2.621670] [drm] AFE_init
[ 2.624396] [drm] deasserted reset
[ 2.627897] Wait for A2 ACK
[ 2.652253] [drm] AFE_power exit
[ 2.655495] [drm] CDN_API_DPTX_SetVideo_blocking (ret = 0)
[ 2.661083] mali-dp f080000.display: bound f1f0000.phy (ops imx_hdp_imx_ops)
[ 2.668273] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 2.674916] [drm] No driver support for vblank timestamp query.
[ 2.680909] [drm] Cannot find any crtc or sizes
[ 2.685761] [drm] Initialized mali-dp 1.0.0 20160106 for f080000.display on minor 0
[ 2.696998] brd: module loaded
[ 2.703463] loop: module loaded
[ 2.707811] ahci-qoriq 3200000.sata: AHCI 0001.0301 32 slots 1 ports 6 Gbps 0x1 impl platform mode
[ 2.716853] ahci-qoriq 3200000.sata: flags: 64bit ncq sntf pm clo only pmp fbs pio slum part ccc sds apst
[ 2.727105] scsi host0: ahci-qoriq
[ 2.730609] ata1: SATA max UDMA/133 mmio [mem 0x03200000-0x0320ffff] port 0x100 irq 91
[ 2.739465] nxp-fspi 20c0000.flexspi: mt35xu02g (262144 Kbytes)
[ 2.746866] libphy: Fixed MDIO Bus: probed
[ 2.751299] tun: Universal TUN/TAP device driver, 1.6
[ 2.756592] CAN device driver interface
[ 2.760592] flexcan 2180000.can: 2180000.can supply xceiver not found, using dummy regulator
[ 2.769359] flexcan 2180000.can: device registered (reg_base=ffff00000eef0000, irq=96)
[ 2.777358] flexcan 2190000.can: 2190000.can supply xceiver not found, using dummy regulator
[ 2.786070] flexcan 2190000.can: device registered (reg_base=ffff00000ef10000, irq=97)
[ 2.794501] Freescale FM module, FMD API version 21.1.0
[ 2.799818] Freescale FM Ports module
[ 2.803496] fsl_mac: fsl_mac: FSL FMan MAC API based driver
[ 2.809140] fsl_dpa: FSL DPAA Ethernet driver
[ 2.813553] fsl_advanced: FSL DPAA Advanced drivers:
[ 2.818535] fsl_proxy: FSL DPAA Proxy initialization driver
[ 2.824167] fsl_oh: FSL FMan Offline Parsing port driver
[ 2.829635] iommu: Adding device 0000:00:00.0 to group 0
[ 2.862725] [drm] HDMI/DP Cable Plug Out
[ 2.942732] fsl_enetc 0000:00:00.0: enabling device (0400 -> 0402)
[ 2.948994] fsl_enetc 0000:00:00.0: no MAC address specified for SI0, using f6:61:8d:e3:98:f7
[ 2.957554] fsl_enetc 0000:00:00.0: no MAC address specified for SI1, using e2:fe:b3:ae:d7:e0
[ 2.966114] fsl_enetc 0000:00:00.0: no MAC address specified for SI2, using 3a:57:d7:32:c7:ef
[ 2.974901] libphy: Freescale ENETC MDIO Bus: probed
[ 2.980790] fsl_enetc 0000:00:00.0 eth0: ENETC PF driver v0.9
[ 2.986606] fsl_enetc 0000:00:00.0: enetc_tsn_init: setup done
[ 2.992583] iommu: Adding device 0000:00:00.1 to group 1
[ 2.997988] fsl_enetc 0000:00:00.1: device is disabled, skipping
[ 3.004081] iommu: Adding device 0000:00:00.2 to group 2
[ 3.052293] ata1: SATA link down (SStatus 0 SControl 300)
[ 3.114729] fsl_enetc 0000:00:00.2: enabling device (0400 -> 0402)
[ 3.120965] fsl_enetc 0000:00:00.2: no MAC address specified for SI0, using 56:a9:f1:fd:b2:5b
[ 3.130569] fsl_enetc 0000:00:00.2 eth1: ENETC PF driver v0.9
[ 3.136348] fsl_enetc 0000:00:00.2: enetc_tsn_init: setup done
[ 3.142322] iommu: Adding device 0000:00:00.6 to group 3
[ 3.254728] fsl_enetc 0000:00:00.6: enabling device (0400 -> 0402)
[ 3.260961] fsl_enetc 0000:00:00.6: no MAC address specified for SI0, using 7e:44:ca:14:ff:71
[ 3.270381] fsl_enetc 0000:00:00.6 eth2: ENETC PF driver v0.9
[ 3.276160] fsl_enetc 0000:00:00.6: enetc_tsn_init: setup done
[ 3.282188] iommu: Adding device 0000:00:00.4 to group 4
[ 3.287615] fsl_enetc_ptp 0000:00:00.4: enabling device (0404 -> 0406)
[ 3.294274] ptp_qoriq: device tree node missing required elements, try automatic configuration
[ 3.303091] pps pps0: new PPS source ptp0
[ 3.307248] iommu: Adding device 0000:00:00.3 to group 5
[ 3.312747] libphy: Freescale PCI ENETC-RCIE MDIO Bus: probed
[ 3.320104] e1000: Intel(R) PRO/1000 Network Driver - version 7.3.21-k8-NAPI
[ 3.327208] e1000: Copyright (c) 1999-2006 Intel Corporation.
[ 3.333010] e1000e: Intel(R) PRO/1000 Network Driver - 3.2.6-k
[ 3.338882] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[ 3.344857] igb: Intel(R) Gigabit Ethernet Network Driver - version 5.4.0-k
[ 3.351848] igb: Copyright (c) 2007-2014 Intel Corporation.
[ 3.357467] igbvf: Intel(R) Gigabit Virtual Function Network Driver - version 2.4.0-k
[ 3.365329] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[ 3.371440] sky2: driver version 1.30
[ 3.375230] iommu: Adding device 0000:00:00.5 to group 6
[ 3.388911] Vitesse VSC8514 1f8100000:10: attached PHY driver [Vitesse VSC8514] (mii_bus:phy_addr=1f8100000:10, irq=POLL)
[ 3.400177] Vitesse VSC8514 1f8100000:11: attached PHY driver [Vitesse VSC8514] (mii_bus:phy_addr=1f8100000:11, irq=POLL)
[ 3.411394] Vitesse VSC8514 1f8100000:12: attached PHY driver [Vitesse VSC8514] (mii_bus:phy_addr=1f8100000:12, irq=POLL)
[ 3.422604] Vitesse VSC8514 1f8100000:13: attached PHY driver [Vitesse VSC8514] (mii_bus:phy_addr=1f8100000:13, irq=POLL)
[ 3.433938] mdio_bus fixed-0:02: attached PHY driver [unbound] (mii_bus:phy_addr=fixed-0:02, irq=POLL)
[ 3.443608] mdio_bus fixed-0:03: attached PHY driver [unbound] (mii_bus:phy_addr=fixed-0:03, irq=POLL)
[ 3.453156] mscc_felix 0000:00:00.5: Felix Switch Driver - version 0.3 probed
[ 3.460896] VFIO - User Level meta-driver version: 0.3
[ 3.467459] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 3.474112] ehci-pci: EHCI PCI platform driver
[ 3.478604] ehci-platform: EHCI generic platform driver
[ 3.483919] ehci-orion: EHCI orion driver
[ 3.487992] ehci-exynos: EHCI EXYNOS driver
[ 3.492246] ehci-msm: Qualcomm On-Chip EHCI Host Controller
[ 3.497881] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
[ 3.504090] ohci-pci: OHCI PCI platform driver
[ 3.508577] ohci-platform: OHCI generic platform driver
[ 3.513872] ohci-exynos: OHCI EXYNOS driver
[ 3.518258] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[ 3.523777] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1
[ 3.541983] xhci-hcd xhci-hcd.0.auto: hcc params 0x0220f66d hci version 0x100 quirks 0x22010810
[ 3.550743] xhci-hcd xhci-hcd.0.auto: irq 83, io mem 0x03100000
[ 3.556970] hub 1-0:1.0: USB hub found
[ 3.560750] hub 1-0:1.0: 1 port detected
[ 3.564823] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[ 3.570338] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2
[ 3.578028] xhci-hcd xhci-hcd.0.auto: Host supports USB 3.0 SuperSpeed
[ 3.584917] hub 2-0:1.0: USB hub found
[ 3.588693] hub 2-0:1.0: 1 port detected
[ 3.592871] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
[ 3.598387] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 3
[ 3.616575] xhci-hcd xhci-hcd.1.auto: hcc params 0x0220f66d hci version 0x100 quirks 0x22010810
[ 3.625333] xhci-hcd xhci-hcd.1.auto: irq 84, io mem 0x03110000
[ 3.631535] hub 3-0:1.0: USB hub found
[ 3.635312] hub 3-0:1.0: 1 port detected
[ 3.639380] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
[ 3.644894] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 4
[ 3.652584] xhci-hcd xhci-hcd.1.auto: Host supports USB 3.0 SuperSpeed
[ 3.659467] hub 4-0:1.0: USB hub found
[ 3.663242] hub 4-0:1.0: 1 port detected
[ 3.667504] usbcore: registered new interface driver usb-storage
[ 3.674771] i2c /dev entries driver
[ 3.679851] i2c i2c-0: Added multiplexed i2c bus 1
[ 3.684953] i2c i2c-0: Added multiplexed i2c bus 2
[ 3.689957] i2c i2c-0: Added multiplexed i2c bus 3
[ 3.701397] rtc-pcf2127-i2c 4-0051: rtc core: registered rtc-pcf2127-i2c as rtc0
[ 3.708852] i2c i2c-0: Added multiplexed i2c bus 4
[ 3.713774] i2c i2c-0: Added multiplexed i2c bus 5
[ 3.718669] [drm] Cannot find any crtc or sizes
[ 3.723319] i2c i2c-0: Added multiplexed i2c bus 6
[ 3.728230] i2c i2c-0: Added multiplexed i2c bus 7
[ 3.733142] i2c i2c-0: Added multiplexed i2c bus 8
[ 3.737956] pca954x 0-0077: registered 8 multiplexed busses for I2C mux pca9547
[ 3.745376] IR NEC protocol handler initialized
[ 3.749926] IR RC5(x/sz) protocol handler initialized
[ 3.754995] IR RC6 protocol handler initialized
[ 3.759542] IR JVC protocol handler initialized
[ 3.764087] IR Sony protocol handler initialized
[ 3.768720] IR SANYO protocol handler initialized
[ 3.773440] IR Sharp protocol handler initialized
[ 3.778161] IR MCE Keyboard/mouse protocol handler initialized
[ 3.784015] IR XMP protocol handler initialized
[ 3.789353] sp805-wdt c000000.wdt: registration successful
[ 3.794957] sp805-wdt c010000.wdt: registration successful
[ 3.801047] qoriq_cpufreq: Freescale QorIQ CPU frequency scaling driver
[ 3.807903] sdhci: Secure Digital Host Controller Interface driver
[ 3.814110] sdhci: Copyright(c) Pierre Ossman
[ 3.818578] Synopsys Designware Multimedia Card Interface Driver
[ 3.824971] sdhci-pltfm: SDHCI platform and OF driver helper
[ 3.870746] mmc0: SDHCI controller on 2140000.esdhc [2140000.esdhc] using ADMA
[ 3.918726] mmc1: SDHCI controller on 2150000.esdhc [2150000.esdhc] using ADMA
[ 3.926490] ledtrig-cpu: registered to indicate activity on CPUs
[ 3.936655] caam 8000000.crypto: Instantiated RNG4 SH1
[ 3.941916] caam 8000000.crypto: device ID = 0x0a12070000000000 (Era 10)
[ 3.948679] caam 8000000.crypto: job rings = 3, qi = 0
[ 3.954115] iommu: Adding device 8010000.jr to group 7
[ 3.959482] caam_jr 8010000.jr: input ring iova = fffffffff000, output ring iova = ffffffffc000
[ 3.968383] iommu: Adding device 8020000.jr to group 8
[ 3.973805] caam_jr 8020000.jr: input ring iova = fffffffff000, output ring iova = ffffffffc000
[ 3.982643] iommu: Adding device 8030000.jr to group 9
[ 3.987987] caam_jr 8030000.jr: input ring iova = fffffffff000, output ring iova = ffffffffc000
[ 4.006656] caam algorithms registered in /proc/crypto
[ 4.013210] mmc0: new ultra high speed SDR104 SDHC card at address 0001
[ 4.020219] mmcblk0: mmc0:0001 SD16G 14.5 GiB
[ 4.020380] caam_jr 8010000.jr: registering rng-caam
[ 4.024725] caam 8000000.crypto: caam pkc algorithms registered in /proc/crypto
[ 4.025007] usbcore: registered new interface driver usbhid
[ 4.025008] usbhid: USB HID core driver
[ 4.026006] No fsl,qman node
[ 4.026113] Freescale USDPAA process driver
[ 4.026115] fsl-usdpaa: no region found
[ 4.026116] Freescale USDPAA process IRQ driver
[ 4.029659] sgtl5000 2-000a: sgtl5000 revision 0x11
[ 4.033319] sgtl5000 2-000a: Using internal LDO instead of VDDD: check ER1
[ 4.064724] random: fast init done
[ 4.075380] u32 classifier
[ 4.075381] Actions configured
[ 4.075393] Netfilter messages via NETLINK v0.30.
[ 4.075486] nf_conntrack version 0.5.0 (16384 buckets, 65536 max)
[ 4.075608] nf_tables: (c) 2007-2009 Patrick McHardy <[email protected]>
[ 4.075611] nf_tables_compat: (c) 2012 Pablo Neira Ayuso <[email protected]>
[ 4.075747] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 4.108403] Initializing XFRM netlink socket
[ 4.108459] NET: Registered protocol family 10
[ 4.113150] Segment Routing with IPv6
[ 4.113215] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[ 4.113670] NET: Registered protocol family 17
[ 4.113680] NET: Registered protocol family 15
[ 4.113700] Bridge firewalling registered
[ 4.113704] Ebtables v2.0 registered
[ 4.114753] can: controller area network core (rev 20170425 abi 9)
[ 4.114783] NET: Registered protocol family 29
[ 4.114803] can: raw protocol (rev 20170425)
[ 4.114805] can: broadcast manager protocol (rev 20170425 t)
[ 4.114810] can: netlink gateway (rev 20170425) max_hops=1
[ 4.114849] 8021q: 802.1Q VLAN Support v1.8
[ 4.114884] 9pnet: Installing 9P2000 support
[ 4.114959] tsn generic netlink module v1 init...
[ 4.114984] Key type dns_resolver registered
[ 4.115423] registered taskstats version 1
[ 4.115765] Btrfs loaded, crc32c=crc32c-generic
[ 4.136451] asoc-simple-card sound: sgtl5000 <-> f130000.sai mapping ok
[ 4.136466] asoc-simple-card sound: ASoC: no DMI vendor name!
[ 4.138244] mmc1: new HS200 MMC card at address 0001
[ 4.142907] mmcblk1: mmc1:0001 Q2J55L 7.13 GiB
[ 4.147447] rtc-pcf2127-i2c 4-0051: setting system clock to 2019-09-13 19:02:01 UTC (1568401321)
[ 4.147457] mmcblk1boot0: mmc1:0001 Q2J55L partition 1 2.00 MiB
[ 4.147585] ALSA device list:
[ 4.147587] #0: f130000.sai-sgtl5000
[ 4.151582] mmcblk1boot1: mmc1:0001 Q2J55L partition 2 2.00 MiB
[ 4.155263] mmcblk1rpmb: mmc1:0001 Q2J55L partition 3 4.00 MiB
[ 4.210728] usb 1-1: new full-speed USB device number 2 using xhci-hcd
[ 4.271424] mmcblk0: p1 p2 p3
[ 4.283754] EXT4-fs warning (device mmcblk0p3): ext4_clear_journal_err:4822: Filesystem error recorded from previous mount: IO failure
[ 4.295930] EXT4-fs warning (device mmcblk0p3): ext4_clear_journal_err:4823: Marking fs in need of filesystem check.
[ 4.317792] mmc0: Tuning failed, falling back to fixed sampling clock
[ 4.326756] mmcblk0: error -84 transferring data, sector 2277376, nr 8, cmd response 0x900, card status 0xc00
[ 4.345067] mmc0: Tuning failed, falling back to fixed sampling clock
[ 4.448514] mmcblk0: error -84 transferring data, sector 2277377, nr 7, cmd response 0x900, card status 0xc00
[ 4.466799] mmc0: Tuning failed, falling back to fixed sampling clock
[ 4.473574] print_req_error: I/O error, dev mmcblk0, sector 2277378
[ 4.479869] Buffer I/O error on dev mmcblk0p3, logical block 0, lost sync page write
[ 4.487798] hub 1-1:1.0: USB hub found
[ 4.491594] mmcblk0: error -110 sending stop command, original cmd response 0x900, card status 0x400e00
[ 4.491744] hub 1-1:1.0: 7 ports detected
[ 4.513424] mmc0: Tuning failed, falling back to fixed sampling clock
[ 4.521204] mmcblk0: error -84 transferring data, sector 15130648, nr 8, cmd response 0x900, card status 0xc00
[ 4.539565] mmc0: Tuning failed, falling back to fixed sampling clock
[ 4.546344] print_req_error: I/O error, dev mmcblk0, sector 15130649
[ 4.552726] Buffer I/O error on dev mmcblk0p3, logical block 1606659, lost sync page write
[ 4.561030] JBD2: Error -5 detected when updating journal superblock for mmcblk0p3-8.
[ 4.568902] Aborting journal on device mmcblk0p3-8.
[ 4.583620] mmc0: Tuning failed, falling back to fixed sampling clock
[ 4.591398] mmcblk0: error -84 transferring data, sector 15130648, nr 8, cmd response 0x900, card status 0xc00
[ 4.609919] mmc0: Tuning failed, falling back to fixed sampling clock
[ 4.616728] print_req_error: I/O error, dev mmcblk0, sector 15130649
[ 4.623110] Buffer I/O error on dev mmcblk0p3, logical block 1606659, lost sync page write
[ 4.631413] JBD2: Error -5 detected when updating journal superblock for mmcblk0p3-8.
[ 4.639449] EXT4-fs (mmcblk0p3): warning: mounting fs with errors, running e2fsck is recommended
[ 4.648279] EXT4-fs (mmcblk0p3): previous I/O error to superblock detected
[ 4.666179] mmc0: Tuning failed, falling back to fixed sampling clock
[ 4.675182] mmcblk0: error -84 transferring data, sector 2277376, nr 8, cmd response 0x900, card status 0xc00
[ 4.693631] mmc0: Tuning failed, falling back to fixed sampling clock
[ 4.700410] print_req_error: I/O error, dev mmcblk0, sector 2277377
[ 4.706706] Buffer I/O error on dev mmcblk0p3, logical block 0, lost sync page write
[ 4.714963] EXT4-fs (mmcblk0p3): recovery complete
[ 4.719777] EXT4-fs (mmcblk0p3): mounted filesystem with ordered data mode. Opts: (null)
[ 4.727927] VFS: Mounted root (ext4 filesystem) on device 179:3.
[ 4.737391] devtmpfs: mounted
[ 4.740914] Freeing unused kernel memory: 1216K
[ 4.766558] EXT4-fs (mmcblk0p3): previous I/O error to superblock detected
[ 4.784784] mmc0: Tuning failed, falling back to fixed sampling clock
[ 4.790733] usb 1-1.1: new full-speed USB device number 3 using xhci-hcd
[ 4.800480] mmcblk0: error -84 transferring data, sector 2277376, nr 8, cmd response 0x900, card status 0xc00
[ 4.818875] mmc0: Tuning failed, falling back to fixed sampling clock
[ 4.825689] print_req_error: I/O error, dev mmcblk0, sector 2277377
[ 4.831987] Buffer I/O error on dev mmcblk0p3, logical block 0, lost sync page write
[ 4.839768] EXT4-fs error (device mmcblk0p3): ext4_journal_check_start:61: Detected aborted journal
[ 4.848852] EXT4-fs (mmcblk0p3): Remounting filesystem read-only
[ 4.854883] EXT4-fs (mmcblk0p3): previous I/O error to superblock detected
[ 4.872653] mmc0: Tuning failed, falling back to fixed sampling clock
[ 4.881638] mmcblk0: error -84 transferring data, sector 2277376, nr 8, cmd response 0x900, card status 0xc00
[ 4.899929] mmc0: Tuning failed, falling back to fixed sampling clock
[ 4.906707] print_req_error: I/O error, dev mmcblk0, sector 2277377
[ 4.913001] Buffer I/O error on dev mmcblk0p3, logical block 0, lost sync page write
[ 4.920786] Starting init: /sbin/init exists but couldn't execute it (error -30)
[ 4.938625] Starting init: /etc/init exists but couldn't execute it (error -13)
/bin/sh: 0: can'[ 4.995897] input: HID 21d1:0015 as /devices/platform/soc/3100000.usb3/xhci-hcd.0.auto/usb1/1-1/1-1.1/1-1.1:1.0/0003:21D1:0015.0001/input/input0
t access tty; job control turned off
# [ 5.066982] hid-generic 0003:21D1:0015.0001: input: USB HID v1.11 Keyboard [HID 21d1:0015] on usb-xhci-hcd.0.auto-1.1/input0
[ 5.079152] input: HID 21d1:0015 as /devices/platform/soc/3100000.usb3/xhci-hcd.0.auto/usb1/1-1/1-1.1/1-1.1:1.1/0003:21D1:0015.0002/input/input1
[ 5.092223] hid-generic 0003:21D1:0015.0002: input: USB HID v1.11 Mouse [HID 21d1:0015] on usb-xhci-hcd.0.auto-1.1/input1
[ 5.104136] input: HID 21d1:0015 as /devices/platform/soc/3100000.usb3/xhci-hcd.0.auto/usb1/1-1/1-1.1/1-1.1:1.2/0003:21D1:0015.0003/input/input2
[ 5.174859] hid-generic 0003:21D1:0015.0003: input: USB HID v1.11 Device [HID 21d1:0015] on usb-xhci-hcd.0.auto-1.1/input2
[ 5.188201] input: HID 21d1:0015 as /devices/platform/soc/3100000.usb3/xhci-hcd.0.auto/usb1/1-1/1-1.1/1-1.1:1.3/0003:21D1:0015.0004/input/input3
[ 5.201277] hid-generic 0003:21D1:0015.0004: input: USB HID v1.11 Device [HID 21d1:0015] on usb-xhci-hcd.0.auto-1.1/input3
[ 5.290761] usb 1-1.2: new full-speed USB device number 4 using xhci-hcd

#
#
#
#

0 件の賞賛
返信

12,147件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

According to https://community.nxp.com/thread/515878 , this is SD card compatible problem with LS1028ARDB.

0 件の賞賛
返信

12,147件の閲覧回数
jeremy_impson
Contributor III

host-console-after-uboot-first-hung.txt

Script started on 2019-10-16 15:57:03-0400
user1@ubuntu:/mnt/DATA/UG3.1.3$ df
Filesystem 1K-blocks Used Available Use% Mounted on
udev 8181824 0 8181824 0% /dev
tmpfs 1641140 1948 1639192 1% /run
/dev/sda1 20509264 8723108 10721300 45% /
tmpfs 8205696 0 8205696 0% /dev/shm
tmpfs 5120 4 5116 1% /run/lock
tmpfs 8205696 0 8205696 0% /sys/fs/cgroup
/dev/loop4 1024 1024 0 100% /snap/gnome-logs/61
/dev/loop5 4224 4224 0 100% /snap/gnome-calculator/406
/dev/loop6 3840 3840 0 100% /snap/gnome-system-monitor/100
/dev/loop2 15104 15104 0 100% /snap/gnome-characters/296
/dev/loop1 55808 55808 0 100% /snap/core18/1066
/dev/loop3 153600 153600 0 100% /snap/gnome-3-28-1804/67
/dev/loop7 90624 90624 0 100% /snap/core/7270
/dev/loop0 43904 43904 0 100% /snap/gtk-common-themes/1313
tmpfs 1641136 44 1641092 1% /run/user/1000
/dev/sdb 205375464 35311876 159561444 19% /mnt/DATA
/dev/sdc2 999320 81288 849220 9% /media/user1/boot
/dev/sdc3 13762872 2849048 10194976 22% /media/user1/rootfs
user1@ubuntu:/mnt/DATA/UG3.1.3$ ls -la /media/user1/boot
total 70508
drwxr-xr-x 4 root root 4096 Oct 16 15:19 .
drwxr-x---+ 5 root root 4096 Oct 16 15:56 ..
-rw-rw-r-- 1 1001 1001 163946 Apr 16 2019 config-4.14.47
-rw-rw-r-- 1 1001 1001 22327 Apr 16 2019 fsl-ls1028a-qds.dtb
-rw-rw-r-- 1 1001 1001 20586 Apr 16 2019 fsl-ls1028a-rdb.dtb
-rw-rw-r-- 1 1001 1001 2176 Apr 16 2019 hdr_ls1028aqds_bs.out
-rw-rw-r-- 1 1001 1001 2176 Apr 16 2019 hdr_ls1028ardb_bs.out
-rwxrwxr-x 1 1001 1001 22776320 Apr 16 2019 Image
-rw-rw-r-- 1 1001 1001 9930242 Apr 16 2019 Image.gz
drwx------ 2 root root 16384 Oct 16 15:18 lost+found
-rw-rw-r-- 1 1001 1001 992 Apr 16 2019 ls1028aqds_boot.scr
-rw-rw-r-- 1 1001 1001 992 Apr 16 2019 ls1028ardb_boot.scr
-rw-rw-r-- 1 1001 1001 19710564 Apr 16 2019 lsdk_linux_arm64_LS_tiny.itb
-rw-rw-r-- 1 1001 1001 9572804 Apr 16 2019 ramdisk_rootfs_arm64.ext4.gz
drwxrwxr-x 4 1001 1001 4096 Apr 16 2019 secboot_hdrs
-rw-rw-r-- 1 1001 1001 992 Apr 16 2019 srk_hash.txt
-rw-rw-r-- 1 1001 1001 9930242 Apr 16 2019 vmlinuz-4.14.47
user1@ubuntu:/mnt/DATA/UG3.1.3$ ls -la /media/user1/rootfs/
total 96
drwxr-xr-x 21 root root 4096 Oct 16 15:19 .
drwxr-x---+ 5 root root 4096 Oct 16 15:56 ..
drwxr-xr-x 2 root root 4096 Oct 3 14:54 bin
drwxr-xr-x 2 root root 4096 Apr 24 2018 boot
drwxr-xr-x 4 root root 4096 Oct 3 14:50 dev
drwxr-xr-x 104 root root 4096 Oct 3 16:15 etc
drwxr-xr-x 3 root root 4096 Oct 3 14:15 home
drwxr-xr-x 17 root root 4096 Oct 3 14:53 lib
drwx------ 2 root root 16384 Oct 16 15:19 lost+found
drwxr-xr-x 2 root root 4096 Oct 3 13:47 media
drwxr-xr-x 2 root root 4096 Oct 3 13:47 mnt
drwxr-xr-x 6 root root 4096 Oct 3 15:13 opt
drwxr-xr-x 2 root root 4096 Apr 24 2018 proc
drwx------ 2 root root 4096 Oct 3 13:47 root
drwxr-xr-x 12 root root 4096 Oct 3 14:41 run
drwxr-xr-x 2 root root 4096 Oct 3 15:03 sbin
drwxr-xr-x 3 root root 4096 Oct 3 14:49 srv
drwxr-xr-x 2 root root 4096 Apr 24 2018 sys
drwxrwxrwt 3 root root 4096 Oct 3 15:03 tmp
drwxr-xr-x 15 root root 4096 Oct 3 15:03 usr
drwxr-xr-x 12 root root 4096 Oct 3 14:24 var
user1@ubuntu:/mnt/DATA/UG3.1.3$ sudo fdisk -l /dev/sdc
Disk /dev/sdc: 14.5 GiB, 15552479232 bytes, 30375936 sectors
Units: sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 512 bytes
I/O size (minimum/optimal): 512 bytes / 512 bytes
Disklabel type: dos
Disk identifier: 0x0a0dc4e1

Device Boot Start End Sectors Size Id Type
/dev/sdc1 132812 180223 47412 23.2M 83 Linux
/dev/sdc2 180224 2277375 2097152 1G 83 Linux
/dev/sdc3 2277376 30375935 28098560 13.4G 83 Linux
user1@ubuntu:/mnt/DATA/UG3.1.3$ sudo files -s /dev/sdc1
sudo: files: command not found
user1@ubuntu:/mnt/DATA/UG3.1.3$ sudo file [1P
/dev/sdc1: ISO-8859 text, with very long lines, with no line terminators
user1@ubuntu:/mnt/DATA/UG3.1.3$ sudo file -s /dev/sdc2
/dev/sdc2: Linux rev 1.0 ext4 filesystem data, UUID=0a219a73-ed92-4d5c-aabb-994d65b2672e, volume name "boot" (needs journal recovery) (extents) (64bit) (large files) (huge files)
user1@ubuntu:/mnt/DATA/UG3.1.3$ sudo file -s /dev/sdc3
/dev/sdc3: Linux rev 1.0 ext4 filesystem data, UUID=47e083e0-ed3e-4bea-95d1-8544f5435a2f, volume name "rootfs" (needs journal recovery) (extents) (64bit) (large files)
user1@ubuntu:/mnt/DATA/UG3.1.3$ mount /dev/sdc1 /mnt/tmp
mount: only root can do that
user1@ubuntu:/mnt/DATA/UG3.1.3$ [1@s [1@u [1@d [1@o [1@
NTFS signature is missing.
Failed to mount '/dev/sdc1': Invalid argument
The device '/dev/sdc1' doesn't seem to have a valid NTFS.
Maybe the wrong device is used? Or the whole disk instead of a
partition (e.g. /dev/sda, not /dev/sda1)? Or the other way around?
[23;0;0tuser1@ubuntu:/mnt/DATA/UG3.1.3$ exit
exit

Script done on 2019-10-16 15:58:54-0400

0 件の賞賛
返信

12,147件の閲覧回数
jeremy_impson
Contributor III

target-console-uboot-first-hung.log

=~=~=~=~=~=~=~=~=~=~=~= PuTTY log 2019.10.16 15:50:13 =~=~=~=~=~=~=~=~=~=~=~=


U-Boot 2018.03-00139-ge124969f47-dirty (Dec 20 2018 - 15:22:43 +0530)

SoC: LS1028AE Rev1.0 (0x870b0010)
Clock Configuration:
CPU0(A72):1300 MHz CPU1(A72):1300 MHz
Bus: 400 MHz DDR: 1600 MT/s
Reset Configuration Word (RCW):
00000000: 34004010 00000030 00000000 00000000
00000010: 00000000 008f0000 0030c000 00000000
00000020: 006031a0 00002580 00000000 00003296
00000030: 00000000 00000010 00000000 00000000
00000040: 00000000 00000000 00000000 00000000
00000050: 00000000 00000000 00000000 00000000
00000060: 00000000 00000000 20067054 00000000
00000070: bb580000 00000000
Model: NXP Layerscape 1028a RDB Board
Board: LS1028AE Rev1.0-RDB, Version: A, boot from NOR
FPGA: v6 (RELEASED: RDB_2018_1206_2148)
SERDES1 Reference : Clock1 = 100.00MHz Clock2 = 100.00MHz
I2C: ready
DRAM: Initializing DDR....
Detected UDIMM Fixed DDR on board
3.9 GiB
DDR 3.9 GiB (DDR4, 32-bit, CL=11, ECC on)
PPA Firmware: Version LSDK-18.09
Using SERDES1 Protocol: 47960 (0xbb58)
PCIe0: pcie@3400000 Root Complex: no link
PCIe1: pcie@3500000 Root Complex: no link
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from SPI Flash... SF: Detected mt35xu02g with page size 256 Bytes, erase size 128 KiB, total 2 GiB
OK
In: serial
Out: serial
Err: serial
Net: eth0: enetc#0
Warning: enetc#1 (eth1) using random MAC address - fe:ec:e4:6e:d5:b0
, eth1: enetc#1, eth2: enetc#2, eth3: netc_mdio
MDIO MUX: no MDIO MUX node
Hit any key to stop autoboot: 0 0
=> load mmc 0:2 a0000000 firmware_ls1028ardb_uboot_sdboot.img
** File not found firmware_ls1028ardb_uboot_sdboot.img **
=> mmc rescan
=> mmv c dev0 0
switch to partitions #0, OK
mmc0 is current device
=> mmc write a0000000 8 0x25000

MMC write: dev # 0, block # 8, count 151552 ... 151552 blocks written: OK
=> qixis_reset sd
=>

(end of log, system hangs)

0 件の賞賛
返信

12,147件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

It seems that image firmware_ls1028ardb_uboot_sdboot.img are not put in the second partition of SD card.

0 件の賞賛
返信

12,147件の閲覧回数
jeremy_impson
Contributor III

I agree that firmware is no being put in the second or any other partition of the SD card. I have already worked around that problem. I believe that the instructions you gave me in your first reply to this thread, which are the same from the Quick Start guide, are incorrect. Others have come to this conclusion as well.( https://community.nxp.com/message/1222653, https://community.nxp.com/thread/514671#comment-1216868)

I listed the workaround above in an earlier reply. I will copy it here:

Please note that I already have a workaround for the "load mmc..." failure, and when using it I am able to boot my Ubuntu rootfs, and that is when I get the mmc device and JBD2 errors that I have reported in the original post of this thread.

 

My workaround is that when I run flex-installer, I add "-f firmware_ls1028ardb_uboot_sdboot.img" to the command line. I've since found out from Pavel Chubakov that I can also just use the command "sudo dd if=firmware...img of=/dev/sdc bs=512 seek=8" if I've already run the installer without the "-f" flag. So I recreated the SD card this way, but did not capture a log of that process.

I have also laid out the correction to all the errors in the User Guide as I understand them so far in this post. When following those instructions, I am able to boot into the Ubuntu rootfs that I made, but get additional errors, which are at the beginning of this very thread, and which I will copy here:

I've built two such bootable removable SD cards. Both came with the Layerscape units that I bought, and both are Kingston brand Canvas Select 16 GB cards (SDS/16GB). I've had no problems reading and writing from them from my Ubuntu host PC. But every time I boot from them on the Layerscape box, there are the following I/O errors:

 

print_req_error: I/O error, dev mmcblk0 sector 1228801

Buffer I/O error on dev mmcblk0p2, logical block 131072, lost sync page write

 

The sector number will vary, the logical block number will vary, the device might be mmcblk0p3, and sometimes it says "lost async page write" instead of "lost sync page write".

 

Sometimes there is an accompanying filesystem error:

 

JBD2: Error -5 detected when updating journal superblock for mmcblk0ps-8

Aborting journal on device mmcblk0p2-8.

 

The referenced device will vary.

 

These errors will either cause the system boot up process to dump into emergency / maintenance mode, or other times it seems to boot correctly but then the root filesystem gets marked readonly. They have never booted up without these I/O and journal errors, which will continue at random intervals after boot.

Do you have this board? Are you able to run the commands to verify whether the Quick Start instructions as printed in version 0.3 of the User Guide are wrong? Can you confirm that my workaround / corrections are right? And when all that is done, can you help me figure out why I'm getting the I/O errors and read-only filesystem? 

Thank you.

0 件の賞賛
返信

12,147件の閲覧回数
jeremy_impson
Contributor III

host-console-flex-installer.txt

Script started on 2019-10-16 15:17:04-0400
user1@ubuntu:/mnt/DATA/UG3.1.3$ cd flexbuild/
user1@ubuntu:/mnt/DATA/UG3.1.3/flexbuild$ . ./setup.env
user1@ubuntu:/mnt/DATA/UG3.1.3/flexbuild$ flex-installer -i install -b boo tpartition_LS_arm64_lts_4.14.tgz -r ./build/
apps/ firmware/ images/ linux/ rfs/
user1@ub
images/rootfs_ubuntu_bionic_LS__arm64
rootfs_ubuntu_bionic_LS_arm64_201910031619.tgz
rootfs_ubuntu_bionic_LS_arm64.tgz
user1@ubuntu:/mnt/DATA/UG3.1.3/flexbuild$ flex-installer -i install -b boottpartition_LS_arm64_lts_4.14.tgz -r ./build/images/rootfs_ubuntu_bionic_LS__arm64_201910031619.tgz -d /dev/s
sda sdc sdc3 sg2 shm/ sr0 stdin
sda1 sdc1 sg0 sg3 snapshot sr1 stdout
sdb sdc2 sg1 sg4 snd/ stderr
user1@ubuntu:/mnt/DATA/UG3.1.3/flexbuild$ flex-installer -i install -b boottpartition_LS_arm64_lts_4.14.tgz -r ./build/images/rootfs_ubuntu_bionic_LS__arm64_201910031619.tgz -d /dev/s
sda sdc sdc3 sg2 shm/ sr0 stdin
sda1 sdc1 sg0 sg3 snapshot sr1 stdout
sdb sdc2 sg1 sg4 snd/ stderr
user1@ubuntu:/mnt/DATA/UG3.1.3/flexbuild$ flex-installer -i install -b boottpartition_LS_arm64_lts_4.14.tgz -r ./build/images/rootfs_ubuntu_bionic_LS__arm64_201910031619.tgz -d /dev/sdc
instruction: install
/dev/sdc found!
Partitioning /dev/sdc ...
Formatting partitions ...
mkfs.fat 4.1 (2017-01-24)
mke2fs 1.44.1 (24-Mar-2018)
/dev/sdc2 contains a ext4 file system labelled 'boot'
last mounted on /media/user1/boot on Wed Oct 16 15:12:41 2019
fs_types for mke2fs.conf resolution: 'ext4'
Filesystem label=boot
OS type: Linux
Block size=4096 (log=2)
Fragment size=4096 (log=2)
Stride=0 blocks, Stripe width=0 blocks
65536 inodes, 262144 blocks
13107 blocks (5.00%) reserved for the super user
First data block=0
Maximum filesystem blocks=268435456
8 block groups
32768 blocks per group, 32768 fragments per group
8192 inodes per group
Filesystem UUID: 0a219a73-ed92-4d5c-aabb-994d65b2672e
Superblock backups stored on blocks:
32768, 98304, 163840, 229376

Allocating group tables: done
Writing inode tables: done
Creating journal (8192 blocks): done
Writing superblocks and filesystem accounting information: done

mke2fs 1.44.1 (24-Mar-2018)
/dev/sdc3 contains a ext4 file system labelled 'rootfs'
last mounted on /media/user1/rootfs on Wed Oct 16 15:12:40 2019
fs_types for mke2fs.conf resolution: 'ext4'
Filesystem label=rootfs
OS type: Linux
Block size=4096 (log=2)
Fragment size=4096 (log=2)
Stride=0 blocks, Stripe width=0 blocks
879552 inodes, 3512320 blocks
175616 blocks (5.00%) reserved for the super user
First data block=0
Maximum filesystem blocks=2151677952
108 block groups
32768 blocks per group, 32768 fragments per group
8144 inodes per group
Filesystem UUID: 47e083e0-ed3e-4bea-95d1-8544f5435a2f
Superblock backups stored on blocks:
32768, 98304, 163840, 229376, 294912, 819200, 884736, 1605632, 2654208

Allocating group tables: done
Writing inode tables: done
Creating journal (16384 blocks): done
Writing superblocks and filesystem accounting information: done

partition and format /dev/sdc: [Done]
installing bootpartition, please wait ...
bootpartition installation: [Done]
installing rootfs, please wait ...
rootfs partition installation: [Done]
Filesystem Size Used Avail Use% Mounted on
udev 7.9G 0 7.9G 0% /dev
tmpfs 1.6G 2.0M 1.6G 1% /run
/dev/sda1 20G 8.4G 11G 45% /
tmpfs 7.9G 0 7.9G 0% /dev/shm
tmpfs 5.0M 4.0K 5.0M 1% /run/lock
tmpfs 7.9G 0 7.9G 0% /sys/fs/cgroup
/dev/loop4 1.0M 1.0M 0 100% /snap/gnome-logs/61
/dev/loop5 4.2M 4.2M 0 100% /snap/gnome-calculator/406
/dev/loop6 3.8M 3.8M 0 100% /snap/gnome-system-monitor/100
/dev/loop2 15M 15M 0 100% /snap/gnome-characters/296
/dev/loop1 55M 55M 0 100% /snap/core18/1066
/dev/loop3 150M 150M 0 100% /snap/gnome-3-28-1804/67
/dev/loop7 89M 89M 0 100% /snap/core/7270
/dev/loop0 43M 43M 0 100% /snap/gtk-common-themes/1313
tmpfs 1.6G 40K 1.6G 1% /run/user/1000
/dev/sdb 196G 34G 153G 19% /mnt/DATA
/dev/sdc2 976M 80M 830M 9% /run/media/sdc2
/dev/sdc3 14G 2.8G 9.8G 22% /run/media/sdc3
setting PARTUUID ...
UUID2 = 0a219a73-ed92-4d5c-aabb-994d65b2672e
PARTUUID2 = 0a0dc4e1-02
PARTUUID3 = 0a0dc4e1-03
install installation finished successfully
user1@ubuntu:/mnt/DATA/UG3.1.3/flexbuild$ [1@s [1@u [1@d [1@o [1@
user1@ubuntu:/mnt/DATA/UG3.1.3/flexbuild$ df
Filesystem 1K-blocks Used Available Use% Mounted on
udev 8181824 0 8181824 0% /dev
tmpfs 1641140 1948 1639192 1% /run
/dev/sda1 20509264 8723008 10721400 45% /
tmpfs 8205696 0 8205696 0% /dev/shm
tmpfs 5120 4 5116 1% /run/lock
tmpfs 8205696 0 8205696 0% /sys/fs/cgroup
/dev/loop4 1024 1024 0 100% /snap/gnome-logs/61
/dev/loop5 4224 4224 0 100% /snap/gnome-calculator/406
/dev/loop6 3840 3840 0 100% /snap/gnome-system-monitor/100
/dev/loop2 15104 15104 0 100% /snap/gnome-characters/296
/dev/loop1 55808 55808 0 100% /snap/core18/1066
/dev/loop3 153600 153600 0 100% /snap/gnome-3-28-1804/67
/dev/loop7 90624 90624 0 100% /snap/core/7270
/dev/loop0 43904 43904 0 100% /snap/gtk-common-themes/1313
tmpfs 1641136 40 1641096 1% /run/user/1000
/dev/sdb 205375464 35311872 159561448 19% /mnt/DATA
/dev/sdc2 999320 81288 849220 9% /run/media/sdc2
/dev/sdc3 13762872 2849048 10194976 22% /run/media/sdc3
/dev/sdc1 23640 0 23640 0% /mnt/tmp
user1@ubuntu:/mnt/DATA/UG3.1.3/flexbuild$ ls -la /run/media/sdc2
total 70504
drwxr-xr-x 4 root root 4096 Oct 16 15:19 .
drwxr-xr-x 5 root root 100 Oct 7 12:34 ..
-rw-rw-r-- 1 1001 1001 163946 Apr 16 2019 config-4.14.47
-rw-rw-r-- 1 1001 1001 22327 Apr 16 2019 fsl-ls1028a-qds.dtb
-rw-rw-r-- 1 1001 1001 20586 Apr 16 2019 fsl-ls1028a-rdb.dtb
-rw-rw-r-- 1 1001 1001 2176 Apr 16 2019 hdr_ls1028aqds_bs.out
-rw-rw-r-- 1 1001 1001 2176 Apr 16 2019 hdr_ls1028ardb_bs.out
-rwxrwxr-x 1 1001 1001 22776320 Apr 16 2019 Image
-rw-rw-r-- 1 1001 1001 9930242 Apr 16 2019 Image.gz
drwx------ 2 root root 16384 Oct 16 15:18 lost+found
-rw-rw-r-- 1 1001 1001 992 Apr 16 2019 ls1028aqds_boot.scr
-rw-rw-r-- 1 1001 1001 992 Apr 16 2019 ls1028ardb_boot.scr
-rw-rw-r-- 1 1001 1001 19710564 Apr 16 2019 lsdk_linux_arm64_LS_tiny.itb
-rw-rw-r-- 1 1001 1001 9572804 Apr 16 2019 ramdisk_rootfs_arm64.ext4.gz
drwxrwxr-x 4 1001 1001 4096 Apr 16 2019 secboot_hdrs
-rw-rw-r-- 1 1001 1001 992 Apr 16 2019 srk_hash.txt
-rw-rw-r-- 1 1001 1001 9930242 Apr 16 2019 vmlinuz-4.14.47
user1@ubuntu:/mnt/DATA/UG3.1.3/flexbuild$ ls -la /run/media/sdc3
total 92
drwxr-xr-x 21 root root 4096 Oct 16 15:19 .
drwxr-xr-x 5 root root 100 Oct 7 12:34 ..
drwxr-xr-x 2 root root 4096 Oct 3 14:54 bin
drwxr-xr-x 2 root root 4096 Apr 24 2018 boot
drwxr-xr-x 4 root root 4096 Oct 3 14:50 dev
drwxr-xr-x 104 root root 4096 Oct 3 16:15 etc
drwxr-xr-x 3 root root 4096 Oct 3 14:15 home
drwxr-xr-x 17 root root 4096 Oct 3 14:53 lib
drwx------ 2 root root 16384 Oct 16 15:19 lost+found
drwxr-xr-x 2 root root 4096 Oct 3 13:47 media
drwxr-xr-x 2 root root 4096 Oct 3 13:47 mnt
drwxr-xr-x 6 root root 4096 Oct 3 15:13 opt
drwxr-xr-x 2 root root 4096 Apr 24 2018 proc
drwx------ 2 root root 4096 Oct 3 13:47 root
drwxr-xr-x 12 root root 4096 Oct 3 14:41 run
drwxr-xr-x 2 root root 4096 Oct 3 15:03 sbin
drwxr-xr-x 3 root root 4096 Oct 3 14:49 srv
drwxr-xr-x 2 root root 4096 Apr 24 2018 sys
drwxrwxrwt 3 root root 4096 Oct 3 15:03 tmp
drwxr-xr-x 15 root root 4096 Oct 3 15:03 usr
drwxr-xr-x 12 root root 4096 Oct 3 14:24 var
user1@ubuntu:/mnt/DATA/UG3.1.3/flexbuild$ ls -la /mnt/tmp
total 20
drwxr-xr-x 2 root root 16384 Dec 31 1969 .
drwxr-xr-x 4 root root 4096 Oct 16 15:27 ..
user1@ubuntu:/mnt/DATA/UG3.1.3/flexbuild$ sudo umount /mnt/tmp
user1@ubuntu:/mnt/DATA/UG3.1.3/flexbuild$ sudo umount /run/media/sdc2
user1@ubuntu:/mnt/DATA/UG3.1.3/flexbuild$ sudo umount /run/media/sdc3
user1@ubuntu:/mnt/DATA/UG3.1.3/flexbuild$ exit
exit

Script done on 2019-10-16 15:28:48-0400

0 件の賞賛
返信

12,147件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Jeremy Impson,

Please execute the following commands

$ flex-installer -i install -b bootpartition_arm64_lts_<version>.tgz -r rootfs_ubuntu_bionic_arm64_<timestamp>.tgz -d /dev/mmcblk0

Under u-boot

=> load mmc 0:2 a0000000 firmware_ls1028ardb_uboot_sdboot.img

=> mmc rescan; mmc dev 0; mmc write a0000000 8 0x25000
=> qixis_reset sd

Would you please provide console log executing above commands?

Would you please provide detailed console log on the target board?

0 件の賞賛
返信