Hi there,
I would like to understand how should I create the RCW register values for a custom board based on a LS1027A. This board contains differences such as, DDR3L and other peripheral confs/pinmuxes I would like to include (comparing to the LS1028ARDb board).
I am using Yocto-based build using custom layers/recipes to build a new image.
So my question is:
- Should I create a PBL using Code Warrior and some how import it to the Yocto compilation? If so how?
- Or should I use the tools uploaded in CodeAurora for such purposes? For example, I have seen there is this repo. How could I customize the values? Should I create a new .rcw file for my board? I am not sure If, for instance, I can set DDR3L instead of DDR4 in that .rcw file.
Thanks,
imuguruza