LS1021A : When I bitbake fsl-image-full in the ubuntu14.04,errors occurs.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LS1021A : When I bitbake fsl-image-full in the ubuntu14.04,errors occurs.

跳至解决方案
3,811 次查看
2838219522
Contributor III

the errors like this:

WARNING: Could not copy license file /home/huanghao/QorIQ-SDK-V2.0-20160527-yocto/build_ls1021atwr/tmp/work/ls1021atwr-fsl-linux-gnueabi/linux-qoriq/4.1-r0/git/COPYING to /home/huanghao/QorIQ-SDK-V2.0-20160527-yocto/build_ls1021atwr/tmp/work/ls1021atwr-fsl-linux-gnueabi/linux-qoriq/4.1-r0/license-destdir/linux-qoriq/COPYING: [Errno 40] Too many levels of symbolic links: '/home/huanghao/QorIQ-SDK-V2.0-20160527-yocto/build_ls1021atwr/tmp/work/ls1021atwr-fsl-linux-gnueabi/linux-qoriq/4.1-r0/git/COPYING'
ERROR: Function failed: do_configure (log file is located at /home/huanghao/QorIQ-SDK-V2.0-20160527-yocto/build_ls1021atwr/tmp/work/ls1021atwr-fsl-linux-gnueabi/linux-qoriq/4.1-r0/temp/log.do_configure.6316)
ERROR: Logfile of failure stored in: /home/huanghao/QorIQ-SDK-V2.0-20160527-yocto/build_ls1021atwr/tmp/work/ls1021atwr-fsl-linux-gnueabi/linux-qoriq/4.1-r0/temp/log.do_configure.6316
Log data follows:
| DEBUG: Executing python function sysroot_cleansstate
| DEBUG: Python function sysroot_cleansstate finished
| DEBUG: Executing shell function do_configure
| cp: cannot stat '/home/huanghao/QorIQ-SDK-V2.0-20160527-yocto/build_ls1021atwr/tmp/work/ls1021atwr-fsl-linux-gnueabi/linux-qoriq/4.1-r0/git/arch/arm/configs/ls1021a_defconfig': Too many levels of symbolic links
| WARNING: exit code 1 from a shell command.
| ERROR: Function failed: do_configure (log file is located at /home/huanghao/QorIQ-SDK-V2.0-20160527-yocto/build_ls1021atwr/tmp/work/ls1021atwr-fsl-linux-gnueabi/linux-qoriq/4.1-r0/temp/log.do_configure.6316)
ERROR: Task 47 (/home/huanghao/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-freescale/recipes-kernel/linux/linux-qoriq_4.1.bb, do_configure) failed with exit code '1'
NOTE: Tasks Summary: Attempted 2607 tasks of which 151 didn't need to be rerun and 1 failed.
Waiting for 0 running tasks to finish:

Summary: 1 task failed:
/home/huanghao/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-freescale/recipes-kernel/linux/linux-qoriq_4.1.bb, do_configure

I have no idea about this.Can anyone help me?

标记 (1)
1 解答
3,378 次查看
Pavel
NXP Employee
NXP Employee

See also the following page in NXP community abut EULA:

https://community.nxp.com/thread/445051

 

Please apply the following patch to fix it:

http://git.freescale.com/git/cgit.cgi/yocto/meta-nxp-npi.git/commit/?h=jethro-sdk-v2.0-ga-17.03

 

Change the linux-qoriq_4.1.bbappend file. Attached file contains corrected linux-qoriq_4.1.bbappend file. Path for this file is the following:

/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-nxp-npi-1703/recipes-kernel/linux$ ls

linux-qoriq_4.1.bbappend


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

9 回复数
3,270 次查看
vr80
Contributor I

tried to build the full image,  bitbake fsl-image-full

please see the error, I found.

ERROR: Function failed: do_configure (log file is located at /home/vr/QorIQ-SDK-V2.0-20160527-yocto/build_b4860qds-64b/tmp/work/b4860qds_64b-fsl-linux/linux-qoriq/4.1-r0/temp/log.do_configure.1727)
ERROR: Logfile of failure stored in: /home/vr/QorIQ-SDK-V2.0-20160527-yocto/build_b4860qds-64b/tmp/work/b4860qds_64b-fsl-linux/linux-qoriq/4.1-r0/temp/log.do_configure.1727

Then I tried to apply the patch, mentioned above, but it is not available. 

Please suggest me how can I fix it.

 

0 项奖励
回复
3,379 次查看
Pavel
NXP Employee
NXP Employee

See also the following page in NXP community abut EULA:

https://community.nxp.com/thread/445051

 

Please apply the following patch to fix it:

http://git.freescale.com/git/cgit.cgi/yocto/meta-nxp-npi.git/commit/?h=jethro-sdk-v2.0-ga-17.03

 

Change the linux-qoriq_4.1.bbappend file. Attached file contains corrected linux-qoriq_4.1.bbappend file. Path for this file is the following:

/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-nxp-npi-1703/recipes-kernel/linux$ ls

linux-qoriq_4.1.bbappend


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,378 次查看
2838219522
Contributor III

Thank you, man.

everything is all right.

0 项奖励
回复
3,378 次查看
Pavel
NXP Employee
NXP Employee

Use the similar command sequence for NOR Flash. Create partition on your NOR Flash and use rootfs.tar.gz.file from this NOR Flash.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
3,378 次查看
2838219522
Contributor III

Hi,Pavel.

When I bitbake menuconfig,it shows errors that Too many levels of symbolic links again.

I can bitbake fsl-image-minimal correctly,but bitbake fsl-image-full and menuconfig can't work fine.

What 's the step 6 that install SDK 2.0-1703?

Does  it mean that after installing  QorIQ Linux SDK v2.0-1703,execute <sdk v2.0-1703-install-directory>/install,and specify the <QorIQ-ios-source-install-directory>?if it's right,I did it too.

0 项奖励
回复
3,378 次查看
Pavel
NXP Employee
NXP Employee

Look at the Sections 4.4.4.8.4 and 4.4.4.8.5 of NXP SDK 2.0-1703 documentation:

https://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf

These sections contain information about deployment rootfs on SD card and QSPI Flash.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,378 次查看
2838219522
Contributor III

Thank you ,Pavel.But I just use the nor flash to boot.

0 项奖励
回复
3,378 次查看
Pavel
NXP Employee
NXP Employee

Usually use the following command sequence for SDK installing under Ubuntu 14.04:

  1. sudo apt-get install ubuntu-minimal ubuntu-standard patch vim-common sed wget subversion git-core coreutils libbonobo2-common unzip texi2html texinfo libsdl1.2-dev docbook-utils gawk python-pysqlite2 diffstat make gcc build-essential xz-utils g++ desktop-file-utils chrpath libgl1-mesa-dev libglu1-mesa-dev autoconf automake groff libtool xterm libncurses5-dev cvs tofrodos

 

  1. a) command: ls -l /bin/sh

                Message:  /bin/sh -> dash

  1. b) command: sudo dpkg-reconfigure dash

                Answer after password – No

                Message:

                Removing 'diversion of /bin/sh to /bin/sh.distrib by dash'

                Adding 'diversion of /bin/sh to /bin/sh.distrib by bash'

                Removing 'diversion of /usr/share/man/man1/sh.1.gz to /usr/share/man/man1/sh.distrib.1.gz by dash'

                Adding 'diversion of /usr/share/man/man1/sh.1.gz to /usr/share/man/man1/sh.distrib.1.gz by bash'

  1. c) command for checking: ls -l /bin/sh

                Message: /bin/sh -> bash

 

  1. mount SDK 2.0 .iso file
  2. cd <sdk-install-dir>.
  3. ./sources/meta-freescale/scripts/host-prepare.sh

Usually Linux recommends also run the following command: sudo usr/sbin/visudo

  1. install SDK 2.0-1703
  2. bitbake fsl-image-minimal

 

See also the following page in NXP community abut EULA:

https://community.nxp.com/thread/445051


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,378 次查看
2838219522
Contributor III

Thank you,Pavel.

And one more question,how can I change the rootfs?

Should I mount the image.ext2.gz.uboot to change the rootfs?

0 项奖励
回复