LS1021A GPIO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1021A GPIO

2,323 Views
damonmeng
Contributor II

I think GPIO might have weak pull-up or drop-down by default, how to disable, we need pure signal.
We test on the customer board if the direction is set to input, but at this time already register the value on the pin, and the value is to take certain ability to drive,
Is this?

0 Kudos
Reply
3 Replies

2,178 Views
alexander_yakov
NXP Employee
NXP Employee

There is no weak pull-up or pull-down resistors on GPIO pins.

Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,178 Views
damonmeng
Contributor II

But we test the GPIO(GPIO3_16) is pull up or pull down.Can you test it?

0 Kudos
Reply

2,178 Views
alexander_yakov
NXP Employee
NXP Employee

Design team confirmed - there are no internal pull-up or pull-down resistors. When multiplexing is selected for GPIO and GPIO is in input mode, the chip is not driving anything. If you see anything driven on the pin in this case, than there must be something other connected to this pin on the board, which is causing this abnormal behavior.


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply