Hi,
I'm new to yocto projects. I'm having an LS1021A-IOT Board rev1, and yocto sdk v1.8. The UART1 in the board is working properly while using the default RCW.
| 00000000: 0608000a 00000000 00000000 00000000 | |
| 00000010: 20000000 08407900 60025a00 21046000 | |
| 00000020: 00000000 00000000 00000000 00038000 | |
| 00000030: 20024800 881b1340 00000000 00000000 |
I've edited the RCW to enable LPUART1 as
| 00000000: 0608000a 00000000 00000000 00000000 | |
| 00000010: 20000000 08407900 60025a00 21046000 | |
| 00000020: 00000000 00000000 00000000 10038000 | |
| 00000030: 20024800 881b1340 00000000 00000000 |
While using the modified RCW in our board, we are not getting u-boot as well as filesystem console in UART1, but kernel prints are getting. I've also probed the 1st and 2nd (LPUART1 SIN & SOUT) pin in J17 connector, but I didn't notice any deflection. Can you please help me to solve this problem?
LPUART1 support is enabled in the device tree source
in ls1021a.dtsi,
| lpuart0: serial@2950000 { | ||
| compatible = "fsl,ls1021a-lpuart"; | ||
| reg = <0x2950000 0x1000>; | ||
| interrupts = <GIC_SPI 80 IRQ_TYPE_LEVEL_HIGH>; | ||
| clocks = <&sysclk>; | ||
| clock-names = "ipg"; | ||
| status = "disabled"; | ||
}; |
and in ls1021a-iot.dts file as
&lpuart0 {
status = "okay";
};
解決済! 解決策の投稿を見る。
I just Found this is an erratum of SOC Rev 1. ie uart1 is enabled along with LPUART or UART2 make uart is malfunction......!
This is solved in rev 2 SOC.
I just Found this is an erratum of SOC Rev 1. ie uart1 is enabled along with LPUART or UART2 make uart is malfunction......!
This is solved in rev 2 SOC.
Thanks Prabin... I think this issue may be resolved in rev2. Thanks for your effort...
You are welcome :smileyhappy:
I am also having the same issue!
I Have the same issue on my ls1021a-iot board rev1....Thanks for posting this forum.....!