Hi,i have some questions about the intergrated switch T1040rdb.
As the following chart in attached file:
we want to match the specific packets which are untagged and ethertype is ARP of port 0.
When matched, two actions:
1. Add double vlan tag to untagged arp packets: vlan101+40
2. Redirect vlan=101 packets to port8
My questions are:
(1) Does IS1 can support action 1? If not, how can we do to achieve this ?
The switch can do what you described, but there is no way to configure for that using the CLI tool available in QorIQ SDK. It requires advanced features/APIs which are not in public access. Consider NXP paid Professional Services to create a switch configuration customized for your specific task(s):
Professional Services Software Technologies (QorIQ 2017) | NXP Semiconductors
Have a great day,
Platon
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------