Is it possible force P1010 in USB 1.1 mode ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is it possible force P1010 in USB 1.1 mode ?

724 Views
fabricedecrop
Contributor I

Now, I'm using P1010 with EHCI controller under VxWorks 6.9.46.

Due to USB issue, I'm wondering if it's possible to force P1010 to be in USB 1.1 configuration using UHCI or OHCI controller ?

Thanks in advance for your reply,

Regards,

Fabrice DECROP

0 Kudos
6 Replies

616 Views
Pavel
NXP Employee
NXP Employee

Add 1.5k resistor from the D+ line to USB_VBUS


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

616 Views
Pavel
NXP Employee
NXP Employee

Add 1.5k pull-up resistor on the D+ line.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

616 Views
fabricedecrop
Contributor I

To what voltage is the pull-up resistor ?

Thanks in advance,

Regards,

Fabrice DECROP

0 Kudos

616 Views
Pavel
NXP Employee
NXP Employee

You can also add an external resistor for disabling high-speed mode.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

616 Views
fabricedecrop
Contributor I

Could please tell me wich resistor is it ?

Thanks in advance,

Regards,

Fabrice DECROP

0 Kudos

616 Views
Pavel
NXP Employee
NXP Employee

The P1010 USB hardware can be used to support for connection only in full-speed mode. See the PORTSC[PFSC[ field.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos