Is 1066 Mhz DDR3 devices supported in P1010 processor ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is 1066 Mhz DDR3 devices supported in P1010 processor ?

Jump to solution
1,090 Views
ismailkk
Contributor I

Hi,  I use P1010 in my project. On the current evaluation board i have DDR3 1333 MHZ 9-9-9. but for our design we prefer 1066 Mhz 7-7-7 instead.

Will this be okay with this class of processor? Any way the processor seems to support maximum frequency of 800Mhz. Request an emergency reply.

Regards  Ismail k k

0 Kudos
Reply
1 Solution
895 Views
r8070z
NXP Employee
NXP Employee

DDR3 1066MHz can operate using clock up to 533 MHz . A DDR3 RAM should operate down to 300 MHz (minimal clock frequency supported by DDR3 internal PLL) . Check the prefered DDR3 data sheet for the minimal supported clock frequency. If it supports 400 MHz  then you can use it.

7-7-7-7 or 9-9-9-9 is question to the DDR3 hardware specs, I do not expect that DDR3 1066 noticably faster then DDR3 1333  at same clock of 400MHz.

View solution in original post

0 Kudos
Reply
3 Replies
896 Views
r8070z
NXP Employee
NXP Employee

DDR3 1066MHz can operate using clock up to 533 MHz . A DDR3 RAM should operate down to 300 MHz (minimal clock frequency supported by DDR3 internal PLL) . Check the prefered DDR3 data sheet for the minimal supported clock frequency. If it supports 400 MHz  then you can use it.

7-7-7-7 or 9-9-9-9 is question to the DDR3 hardware specs, I do not expect that DDR3 1066 noticably faster then DDR3 1333  at same clock of 400MHz.

0 Kudos
Reply
895 Views
addiyi
NXP Employee
NXP Employee

According with the P1010 Reference Manual, DDR memory controller operating a maximum 800 Mbps data rate (this means 400 MHz).

Adrian

895 Views
Wlodek_D_
Senior Contributor II

Hello,

Thank you for your post, however please consider moving it to the right community place (e.g. QorIQ Processors ) to get it visible for active members.

For details please see general advice Where to post a Discussion? (https://community.freescale.com/docs/DOC-99909 )

Thank you for using Freescale Community.

0 Kudos
Reply