Installation of SDK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Installation of SDK

635 Views
sanjaykumar-r56
NXP Employee
NXP Employee

I am trying to install SDK V1.6 in external Seagate harddisk in Ubuntu 10.04. Install folder location is given as /media/Seagate \Backup\ Plus\ Drive/ . It gives error readlink: extra operand 'Backup'. Am I missing something here ?

0 Kudos
3 Replies

417 Views
alexander_yakov
NXP Employee
NXP Employee

Why several slashes "/" are changed to backslashes "\" and why there is a space after "Seagate" ?

If this is a folder location it shoud be /media/Seagate/Backup/Plus/Drive/ 

0 Kudos

417 Views
sanjaykumar-r56
NXP Employee
NXP Employee

Folder name is "Backup Plus Driver" .If I don't give backslash, Ubuntu doesn't recognize it as one folder.

I can se folder contents only using these backslashes and space

$ ls /media/Seagate\ Backup\ Plus\ Drive/

aaa

Autorun.inf

BackupPlus.ico

Downloads

QorIQ-SDK-T1040QDS-SOURCE-20140212-yocto.iso.part1

QorIQ-SDK-T1040QDS-SOURCE-20140212-yocto.iso.part2

sdk

sdk1v6

Seagate

Seagate Dashboard Installer.dmg

Seagate Dashboard Installer.exe

tmp

ubuntu

Unused_pins_sanjay

Video

r56700@r56700-desktop:~$

0 Kudos

417 Views
alexander_yakov
NXP Employee
NXP Employee

Ok, thanks for clarification.

In this case I think "extra operand" error just means the installator does not understand spaces in folder name. Try using brackets or rename folder to "Backup_Plus_Driver" or to "Backup", or simply move the file to another location.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos