Inquiry about ls1024A CS2 and NAND CS.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Inquiry about ls1024A CS2 and NAND CS.

1,260件の閲覧回数
h201668
Contributor III

ECC occurs when CS2 and NAND CS are used together.

ECC doesn't happen on NAND unless CS2 is used.

On page 56 of the datasheet, NAND_RE and NAND_WE are toggled when there is an access to CS#0-3.

There is a phrase like this, but it is judged that CS2 affects NAND RE/WE, so NAND CS also affects it.

What can I do to solve this problem?

I definitely need to use CS2.

Your help is much needed.

タグ(3)
0 件の賞賛
8 返答(返信)

1,203件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Chavira_0-1673893672538.png

probably the error is here because I can see the CS2 and NAND CS are low at the same time but the image is not clear.
Can you send a new image with zoom when that happens again?

0 件の賞賛

1,183件の閲覧回数
h201668
Contributor III

Thank you for the reply.

There is one thing I realized during the exam.

If CS2 is not used, ECC does not occur in NAND.

I am currently using CS2 with 20ms intervals.

Please refer to the picture below.

h201668_0-1673916623784.png

Enlarging photo (above)

h201668_1-1673916300191.png

It can be confirmed that NAND_CS_n is active low and then changed to high.

With CS2, this situation arises.

I would like to know what part I need to pay attention to to solve this.

タグ(3)
0 件の賞賛

1,178件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Yes that part is the correct one as you can see you have two CS signals active in low at the same time (nand cs and cs2)

you only can put one cs signal on low.

Chavira_0-1673972539963.png

 

0 件の賞賛

1,171件の閲覧回数
h201668
Contributor III

Thank you for answer

There's something wrong about what you saw

Please take a good look at the last photo I replied to

It can be confirmed that NAND CS is low active and high.

I don't know why the trigger got stuck, but I sensed something strange about this part.

It is judged that nand_cs is freed and proceeded again.

You need to check this part.

The part recognized by nand_cs is compared and passed.

It seems that the problem is not easily solved, but I think it will be solved if you help.

 

1. ECC Error (NAND_CS bad signal)

h201668_0-1674016488456.png

When NAND_CS is initially in a low active state, RE must be low active.
By the way, the re signal comes out as active, but I think that an error occurs in the data reading the nand flash because NAND_CS has become High.

 

2. NAND_CS signal ok

h201668_1-1674016888304.png

NAND_CS is operating normally.

 

 

0 件の賞賛

1,162件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

both parts look good I think the real problem is the part that I refer before because exist two cs signals in a low state at the same time information

0 件の賞賛

1,156件の閲覧回数
h201668
Contributor III

Thank you for answering.

If NAND_CS and CS2 should not be Low Active at the same time, ECC should be continuously output when CS2 operates.

However, the ECC symptoms appear only when pasting files.

I think the cause is that the NAND_WE signal was not read early when NAND_CS went from LOW Active to HIGH.

But that doesn't mean you're wrong.

There is one thing I'd like to ask you.

Is there any way to unpack NAND_CS when reading CS2?

I think you should check when to operate CS2 and disable NAND_CS.

If you tell me how, I'll check that out.

タグ(4)
0 件の賞賛

1,246件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Thank you for contacting NXP support!

In theory, you don't have o experiment with any problem if you have a proper connection.

I attached for you an image of the proper connection of generic peripheral devices to LS1024A.

The pins NAND_RE and NAND_WE are independent of CS[0-3] and when you assert cs2 those pins don't affect the NAND function because NAND_CS_N (GPIO28) is not asserted.

The signals NAND_RE and NAND_WE always can be toggled because each signal indicates if the memory will be reeded o written and never should be asserted together

Please check your connections or share your schematic to check if exist a wrong connection.

0 件の賞賛

1,233件の閲覧回数
h201668
Contributor III

Thank you for answer.

The circuit is like LS1024ARDB.

h201668_0-1673228877216.png

LS1024ARDB used NAND Flash same.(MT29F16G08CBACAWP ) 

As a result of measurement with a logic analyzer, it was confirmed that CS2 and NAND_CS do not operate normally.

If CS2 is not used, NAND_CS operates normally.

 

1. Use CS2, use NAND_CS_n => Logic analyzer measurement

h201668_1-1673252813588.png

NAND_CS_n photo enlargement

h201668_3-1673252977276.png

There are cases in which NAND_CS_n recognizes it as high at the point where it should become low active and then recognizes it as low again.

 

2. CS2 not used, NAND_CS_n used => Logic analyzer measurement

h201668_1-1673405374012.png

NAND_CS_n photo enlargement

h201668_0-1673405326911.png

 

タグ(3)
0 件の賞賛