In LS1043A, configuring the fpga using FPP x8 mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

In LS1043A, configuring the fpga using FPP x8 mode

756 Views
logeshs
Contributor II

Hi,

We are using LS1043 and altera cyclone V fpga in our design. We like to configure the fpga using FPP x8 mode. Please refer the Cyclone V configuration datasheet

 

https://documentation.altera.com/#/00005773-AA$NT00072849

 

 

In our earlier design we have used NXP processors from MPC85xx series and we used the local bus to configure the altera fpga in FPP x8 mode. But in the LS1043 local bus (IFC bus) there is no UPM machine support (user programmable machine) . So how the programming can be implemented in the LS1043 system without glue logic.

Thanks

0 Kudos
Reply
1 Reply

619 Views
r8070z
NXP Employee
NXP Employee

Have a great day,

I do not see possibility to use IFC instead of LBC in the very flexible UPM mode for the FPP 8x. From my point of view using the GPIOs is the only way to implement the FPP 8x without glue logic on the LS1043. The problem is that it will require for many GPIO pins.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply