IVOR6 0x0700 PROGRAM INTERUPT "illegal instruction exception"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IVOR6 0x0700 PROGRAM INTERUPT "illegal instruction exception"

2,636件の閲覧回数
pierre-antoinem
Contributor III

Hi,

I'm having a strange problem on a P5020 processor.

In fact core0 is generating IVOR6 0x0700 exception "ESR register showing illegal instruction exception" on a simple printf while core1 as no problem running and is on the exact same TLC configuration script.

The TCL was modified in ord to use CPC1 and CPC2 as SDRAM.

The DDR controller 1 and 2 are separatly mapped by 2 LAW's each of 2 GB.

TLB entries were made for each too.

/******************************************************************

**************************   MAIN ********************************/

int main()

{

    nt i=0;

   

    unsigned long proc_id;

    asm ("mfpir %0" : "=r" (proc_id));

   

#if SMPTARGET

    initSmp();

#endif

   

    printf("Core%d: printf de test !\r\n", proc_id>>5);

    //asm("sc"); // generate a system call exception to demonstrate the ISR

    return 0;

}

0 件の賞賛
返信
6 返答(返信)

1,703件の閲覧回数
pierre-antoinem
Contributor III

Problem solved.

Used init_sram.tcl for CPC SRAM configuration. (thanks to marius viorel grigoras, it was very helpfull for setting the SRAM mode of the CPC)

Remapped the DDR to 0x0000_0000 -> 3FFF_FFFF which is 1GB in size with DDR1 512MB and DDR2 512MB.

- DDR controllers not interleaved.

- Banks not interleabed in each DDR.

CPC1 and CPC2 are map from 0x4000_0000 to 0x401F_FFFF  1MB each.

Cache L2 disable

Cache L1 data disable

Cache L1 instruction enable.

DDR configuration was the main problem, caution during configuration is the main solution.

Cheers.

0 件の賞賛
返信

1,703件の閲覧回数
marius_grigoras
NXP Employee
NXP Employee

Thanks for sharing your final integration solution!

Regards,

Marius

0 件の賞賛
返信

1,703件の閲覧回数
pierre-antoinem
Contributor III

Builded a new configuration and i'm trying to turn off the interleaving mode of the DDR controllers.

My goal is to have 2GB of menory managed by DDR controller 1 and 2 other GB of memory managed by controller 2.

There is 2 DRR dimms on my card, each of 2gb. (running cpu's at 2.0Ghz and DDR at 1333Mhz)

What would be the best configuation for DDR registers, LAW's and TLB's to achieve this ?

Tested CPC1, CPC2, Dissableling cache L2 and L1 data and it had no problems running simple code.

But when it comes to configure the DDR controllers I get data tlb miss or machine check exceptions.

Any help is appreciated.

Thanks.

0 件の賞賛
返信

1,703件の閲覧回数
pierre-antoinem
Contributor III

Sorry miss clicked and the post was sent..

Here is the TCL scrip used.

Any help would be appreciated !

########################################################################################

# Initialization file for P5020 DS

# Clock Configuration:

#       CPU0:2000 MHz, CPU1:2000 MHz, CCB: 800 MHz,

#       DDR: 1333 MHz, SYSCLK: 133 MHz, LBC: 100 MHz

########################################################################################

variable master_core 0

variable CCSRBAR 0xFE000000

proc CCSR {reg_off} {

    global CCSRBAR

   

    return i:0x[format %x [expr {$CCSRBAR + $reg_off}]]

}

proc init_board {} {

    # disable Boot Space Translation

    # LCC_BSTAR

    mem [CCSR 0x28] = 0x00000000

   

    # invalidate again BR0 to prevent flash data damage in case

    # the boot sequencer re-enables CS0 access

    # LCC_BSTAR

    mem [CCSR 0x124000] = 0x00001000

   

    ##################################################################################

    # Local Access Windows Setup

   

    # LAW0 to eLBC (NOR) - 256M

    # LAW_LAWBARH0

    mem [CCSR 0xC00] = 0x00000000

    # LAW_LAWBARL0

    mem [CCSR 0xC04] = 0xE0000000

    # LAW_LAWAR0

    mem [CCSR 0xC08] = 0x81F0001B

   

    # LAW1 to BMAN - 2MB

    # LAW_LAWBARH1

    mem [CCSR 0xC10] = 0x00000000

    # LAW_LAWBARL1

    mem [CCSR 0xC14] = 0xF4000000

    # LAW_LAWAR1

    mem [CCSR 0xC18] = 0x81800014

   

    # LAW2 to QMAN - 2MB

    # LAW_LAWBARH2

    mem [CCSR 0xC20] = 0x00000000

    # LAW_LAWBARL2

    mem [CCSR 0xC24] = 0xF4200000

    # LAW_LAWAR2

    mem [CCSR 0xC28] = 0x83C00014

    # LAW3 to eLBC (PIXIS) - 4KB

    # LAW_LAWBARH3

    mem [CCSR 0xC30] = 0x00000000

    # LAW_LAWBARL3

    mem [CCSR 0xC34] = 0xFFDF0000

    # LAW_LAWAR3

    mem [CCSR 0xC38] = 0x81F0000B

    # LAW4 to DCSR - 4MB

    # LAW_LAWBARH4

    mem [CCSR 0xC40] = 0x00000000

    # LAW_LAWBARL4

    mem [CCSR 0xC44] = 0xF0000000

    # LAW_LAWAR4

    mem [CCSR 0xC48] = 0x81D00015

    # LAW5 to PEX1 - 512MB

    # LAW_LAWBARH5

#    mem [CCSR 0xC50] = 0x00000000

    # LAW_LAWBARL5

#    mem [CCSR 0xC54] = 0x80000000

    # LAW_LAWAR5

#    mem [CCSR 0xC58] = 0x8000001C

   

    # LAW6 to PEX1 - 64KB

    # LAW_LAWBARH6

    mem [CCSR 0xC60] = 0x00000000

    # LAW_LAWBARL6

    mem [CCSR 0xC64] = 0xF8000000

    # LAW_LAWAR6

    mem [CCSR 0xC68] = 0x8000000F

   

    # LAW7 to PEX2 - 512MB

    # LAW_LAWBARH7

    mem [CCSR 0xC70] = 0x00000000

    # LAW_LAWBARL7

    mem [CCSR 0xC74] = 0xA0000000

    # LAW_LAWAR7

    mem [CCSR 0xC78] = 0x8010001C

   

    # LAW8 to PEX2 - 64KB

    # LAW_LAWBARH8

    mem [CCSR 0xC80] = 0x00000000

    # LAW_LAWBARL8

    mem [CCSR 0xC84] = 0xF8010000

    # LAW_LAWAR8

    mem [CCSR 0xC88] = 0x8010000F

   

    # LAW9 to PEX3 - 512MB

    # LAW_LAWBARH9

    mem [CCSR 0xC90] = 0x00000000

    # LAW_LAWBARL9

    mem [CCSR 0xC94] = 0xC0000000

    # LAW_LAWAR9

    mem [CCSR 0xC98] = 0x8020001C

   

    # LAW10 to PEX3 - 64KB

    # LAW_LAWBARH10

    mem [CCSR 0xCA0] = 0x00000000

    # LAW_LAWBARL10

    mem [CCSR 0xCA4] = 0xF8020000

    # LAW_LAWAR10

    mem [CCSR 0xCA8] = 0x8020000F

   

    # LAW11 to eLBC (NAND) - 1M

    # LAW_LAWBARH11

    mem [CCSR 0xCB0] = 0x00000000

    # LAW_LAWBARL11

    mem [CCSR 0xCB4] = 0xF8200000

    # LAW_LAWAR11

    mem [CCSR 0xCB8] = 0x81F00013

   

    # LAW31 to Interleaved DDR - 2GB

    # LAW_LAWBARH31

#    mem [CCSR 0xDF0] = 0x00000000

    # LAW_LAWBARL31

#    mem [CCSR 0xDF4] = 0x00000000

    # LAW_LAWAR31

#    mem [CCSR 0xDF8] = 0x8140001E

#ajout

    # LAW28 CPC1 1MB 0x8000_0000

    # LAW_LAWBARH28

    mem [CCSR 0xDC0] = 0x00000000

    # LAW_LAWBARL28

    mem [CCSR 0xDC4] = 0x80000000

    # LAW_LAWAR28

    mem [CCSR 0xDC8] = 0x81000013

    # LAW29 CPC2 1MB 0x8010_0000

    # LAW_LAWBARH29

    mem [CCSR 0xDD0] = 0x00000000

    # LAW_LAWBARL29

    mem [CCSR 0xDD4] = 0x80100000

    # LAW_LAWAR29

    mem [CCSR 0xDD8] = 0x81100013

    # LAW30 DDR1 | 0x00000000 - 0x0_8000_0000 | 2GB

    # LAW_LAWBARH31

    mem [CCSR 0xDE0] = 0x00000000

    # LAW_LAWBARL31

    mem [CCSR 0xDE4] = 0x00000000

    # LAW_LAWAR31

    mem [CCSR 0xDE8] = 0x8100001E

    # LAW31 DDR2 | 0x1_0000_0000 - 0x1_8000_0000 | 2GB

    # LAW_LAWBARH31

#    mem [CCSR 0xDF0] = 0x00000001

    # LAW_LAWBARL31

#    mem [CCSR 0xDF4] = 0x00000000

    # LAW_LAWAR31

#    mem [CCSR 0xDF8] = 0x8110001E

   

   

    ##################################################################################

    # DDR Controllers Setup - the names are from the new drop but the registers

    # are from the old drop

   

    # DDR1_DDR_SDRAM_CFG

    mem [CCSR 0x8110] = 0x47044000

    # DDR1_CS0_BNDS

    mem [CCSR 0x8000] = 0x000000ff

    # DDR1_CS1_BNDS

    mem [CCSR 0x8008] = 0x00000000

    # DDR1_CS0_CONFIG

    mem [CCSR 0x8080] = 0x80014202

    # DDR1_CS1_CONFIG

    mem [CCSR 0x8084] = 0x80014202

    # DDR1_CS0_CONFIG_2

    mem [CCSR 0x80C0] = 0x00000000

    # DDR1_CS1_CONFIG_2

    mem [CCSR 0x80C4] = 0x00000000

    # DDR1_TIMING_CFG_3

    mem [CCSR 0x8100] = 0x00020000

    # DDR1_TIMING_CFG_0

    mem [CCSR 0x8104] = 0x50110104

    # DDR1_TIMING_CFG_1

    mem [CCSR 0x8108] = 0x6f6b4644

    # DDR1_TIMING_CFG_2

    mem [CCSR 0x810C] = 0x0fa888cc

    # DDR1_DDR_SDRAM_CFG_2

    mem [CCSR 0x8114] = 0x24401001

    # DDR1_DDR_SDRAM_MODE

    mem [CCSR 0x8118] = 0x00441420

    # DDR1_DDR_SDRAM_MODE_2

    mem [CCSR 0x811C] = 0x00000000

    # DDR1_DDR_SDRAM_MODE_3

    mem [CCSR 0x8200] = 0x00001420

    # DDR1_DDR_SDRAM_MODE_4

    mem [CCSR 0x8204] = 0x00000000

    # DDR1_DDR_SDRAM_MODE_5

    mem [CCSR 0x8208] = 0x00001420

    # DDR1_DDR_SDRAM_MODE_6

    mem [CCSR 0x820C] = 0x00000000

    # DDR1_DDR_SDRAM_MODE_7

    mem [CCSR 0x8210] = 0x00001420

    # DDR1_DDR_SDRAM_MODE_8

    mem [CCSR 0x8214] = 0x00000000

    # DDR1_DDR_SDRAM_MD_CNTL

    mem [CCSR 0x8120] = 0x00000000

    # DDR1_DDR_SDRAM_INTERVAL

    mem [CCSR 0x8124] = 0x0c300100

    # DDR1_DDR_DATA_INIT

    mem [CCSR 0x8128] = 0xdeadbeef

    # DDR1_DDR_SDRAM_CLK_CNTL

    mem [CCSR 0x8130] = 0x02800000

    # DDR1_DDR_INIT_ADDR

    mem [CCSR 0x8148] = 0x00000000

    # DDR1_DDR_INIT_EXT_ADDRESS

    mem [CCSR 0x814C] = 0x00000000

    # DDR1_TIMING_CFG_4

    mem [CCSR 0x8160] = 0x00000001

    # DDR1_TIMING_CFG_5

    mem [CCSR 0x8164] = 0x02401400

    # DDR1_DDR_ZQ_CNTL

    mem [CCSR 0x8170] = 0x89080600

    # DDR1_DDR_WRLVL_CNTL

    mem [CCSR 0x8174] = 0x8675f606

    # DDR1_DDR_WRLVL_CNTL_2

    mem [CCSR 0x8190] = 0x00000000

    # DDR1_DDR_WRLVL_CNTL_3

    mem [CCSR 0x8194] = 0x00000000

    # DDR1_DDR_SR_CNTR

    mem [CCSR 0x817C] = 0x00000000

    # DDR1_DDRCDR_1

    mem [CCSR 0x8B28] = 0x80000000

    # DDR1_DDRCDR_2

    mem [CCSR 0x8B2C] = 0x00000000

    # DDR1_ERR_SBE

    mem [CCSR 0x8E58] = 0x00000000

   

    # DDR2_DDR_SDRAM_CFG

    mem [CCSR 0x9110] = 0x47044000

    # DDR2_CS0_BNDS

    mem [CCSR 0x9000] = 0x000000ff

    # DDR2_CS1_BNDS

    mem [CCSR 0x9008] = 0x00000000

    # DDR2_CS0_CONFIG

    mem [CCSR 0x9080] = 0x80014202

    # DDR2_CS1_CONFIG

    mem [CCSR 0x9084] = 0x80014202

    # DDR2_CS0_CONFIG_2

    mem [CCSR 0x90C0] = 0x00000000

    # DDR2_CS1_CONFIG_2

    mem [CCSR 0x90C4] = 0x00000000

    # DDR2_TIMING_CFG_3

    mem [CCSR 0x9100] = 0x00020000

    # DDR2_TIMING_CFG_0

    mem [CCSR 0x9104] = 0x50110104

    # DDR2_TIMING_CFG_1

    mem [CCSR 0x9108] = 0x6f6b4644

    # DDR2_TIMING_CFG_2

    mem [CCSR 0x910C] = 0x0fa888cc

    # DDR2_DDR_SDRAM_CFG_2

    mem [CCSR 0x9114] = 0x24401111

    # DDR2_DDR_SDRAM_MODE

    mem [CCSR 0x9118] = 0x00441420

    # DDR2_DDR_SDRAM_MODE_2

    mem [CCSR 0x911C] = 0x00000000

    # DDR2_DDR_SDRAM_MODE_3

    mem [CCSR 0x9200] = 0x00001420

    # DDR2_DDR_SDRAM_MODE_4

    mem [CCSR 0x9204] = 0x00000000

    # DDR2_DDR_SDRAM_MODE_5

    mem [CCSR 0x9208] = 0x00001420

    # DDR2_DDR_SDRAM_MODE_6

    mem [CCSR 0x920C] = 0x00000000

    # DDR2_DDR_SDRAM_MODE_7

    mem [CCSR 0x9210] = 0x00001420

    # DDR2_DDR_SDRAM_MODE_8

    mem [CCSR 0x9214] = 0x00000000

    # DDR2_DDR_SDRAM_MD_CNTL

    mem [CCSR 0x9120] = 0x00000000

    # DDR2_DDR_SDRAM_INTERVAL

    mem [CCSR 0x9124] = 0x0c300100

    # DDR2_DDR_DATA_INIT

    mem [CCSR 0x9128] = 0xdeadbeef

    # DDR2_DDR_SDRAM_CLK_CNTL

    mem [CCSR 0x9130] = 0x02800000

    # DDR2_DDR_INIT_ADDR

    mem [CCSR 0x9148] = 0x00000000

    # DDR2_DDR_INIT_EXT_ADDRESS

    mem [CCSR 0x914C] = 0x00000000

    # DDR2_TIMING_CFG_4

    mem [CCSR 0x9160] = 0x00000001

    # DDR2_TIMING_CFG_5

    mem [CCSR 0x9164] = 0x02401400

    # DDR2_DDR_ZQ_CNTL

    mem [CCSR 0x9170] = 0x89080600

    # DDR2_DDR_WRLVL_CNTL

    mem [CCSR 0x9174] = 0x8675f606

    # DDR2_DDR_WRLVL_CNTL_2

    mem [CCSR 0x9190] = 0x00000000

    # DDR2_DDR_WRLVL_CNTL_3

    mem [CCSR 0x9194] = 0x00000000

    # DDR2_DDR_SR_CNTR

    mem [CCSR 0x917C] = 0x00000000

    # DDR2_DDRCDR_1

    mem [CCSR 0x9B28] = 0x80000000

    # DDR2_DDRCDR_2

    mem [CCSR 0x9B2C] = 0x00000000

    # DDR2_ERR_SBE

    mem [CCSR 0x9E58] = 0x00000000

   

    # delay before enable

    wait 500

    # DDR1_DDR_SDRAM_CFG

    mem [CCSR 0x8110] = 0xe7044000

    # DDR2_DDR_SDRAM_CFG

    mem [CCSR 0x9110] = 0xe7044000

    # wait for DRAM data initialization

    wait 1500

       

    ##################################################################################

    # eSPI Setup

    # ESPI_SPMODE

    mem [CCSR 0x110000] = 0x80000403

    # ESPI_SPIM - catch all events

    mem [CCSR 0x110008] = 0x00000000

    # ESPI_SPMODE0

    mem [CCSR 0x110020] = 0x30170008

       

    ##################################################################################

    # LBC Controller Setup

   

    # CS0 - NOR,     addr at 0xE8000000, 128MB size, 16-bit, GCPM, Valid

    # eLBC_BR0

    mem [CCSR 0x124000] = 0xe8001001

    # eLBC_ORg0

    mem [CCSR 0x124004] = 0xf8000f85

   

    # CS1 - PromJet, addr at 0xE0000000, 128MB size, 16-bit, GCPM, Valid

    # eLBC_BR1

    mem [CCSR 0x124008] = 0xe0001001

    # eLBC_ORg1

    mem [CCSR 0x12400C] = 0xf8000ff7

   

    # CS2 - NAND,    addr at 0xF8200000, 256KB size, 8-bit, FCM, Valid

    # eLBC_BR2

    mem [CCSR 0x124010] = 0xF8200C21

    # eLBC_ORf2

    mem [CCSR 0x124014] = 0xFFFF87CC

   

    # CS3 - PIXIS,   addr at 0xFFDF0000,   1MB size,  8-bit, GCPM, Valid 

    # eLBC_BR3

    mem [CCSR 0x124018] = 0xffdf0801

    # eLBC_ORg3

    mem [CCSR 0x12401C] = 0xffff8ff7

#ajout

    # CS4 - NAND,    addr at 0xF8200000, 256KB size, 8-bit, FCM, Valid

    #BR4 = 0xF8200C21

    mem [CCSR 0x124020] = 0xF8200C21

    #OR4 = 0xFFFF87CC

    mem [CCSR 0x124024] = 0xFFFF87CC

    # CS5 - NAND,    addr at 0xF8200000, 256KB size, 8-bit, FCM, Valid

    #BR5 = 0xF8200C21

    mem [CCSR 0x124028] = 0xF8200C21

    #OR5 = 0xFFFF87CC

    mem [CCSR 0x12402C] = 0xFFFF87CC

     # CS6 - NAND,    addr at 0xF8200000, 256KB size, 8-bit, FCM, Valid

    #BR6 = 0xF8200C21

    mem [CCSR 0x124030] = 0xF8200C21

    #OR6 = 0xFFFF87CC

    mem [CCSR 0x124034] = 0xFFFF87CC

#fin ajout

   

    # eLBC_LBCR

    mem [CCSR 0x1240D0] = 0x40000000

   

    # LCRR CLKDIV = 16

    # eLBC_LCRR

    mem [CCSR 0x1240D4] = 0x80000002

   

    # eLBC_FMR

    mem [CCSR 0x1240E0] = 0x0000F000

   

    ##################################################################################

    # CoreNet Platform Cache 1

    # configure internal CPC1 as SRAM

    # CNetPC1_CPCSRCR0  - SRBARL=0, INTLVEN=0, SRAMSZ=0101, SRAMEN=1

    mem [CCSR 0x10104] = 0x8000000B

    # CPC_CPCSRCR1

    mem [CCSR 0x10100] = 0x00000000

    # CNetPC1_CPCEWCR0 - disable stashing

    mem [CCSR 0x10010] = 0x00000000

    # CNetPC1_CPCERRDIS

    mem [CCSR 0x10E44] = 0x00000000

    # CNetPC1_CPCERRINTEN

    mem [CCSR 0x10E48] = 0x00000000

    # CPC_CPCERRCTL

    mem [CCSR 0x10E58] = 0x00ffffff

    # No error injection

     mem [CCSR 0x10E00] = 0x00000000

    mem [CCSR 0x10E04] = 0x00000000

    mem [CCSR 0x10E08] = 0x00000000

    # No speculative memory access

    mem [CCSR 0x10F00] = 0x08000000

    # invalidate(CPCFI) and No flash lock clear(CPCLFC)

    # CNetPC1_CPCCSR0

    mem [CCSR 0x10000] = 0x00200400

    wait 500

    # enable L3 SRAM

    # CNetPC1_CPCCSR0

    mem [CCSR 0x10000] = 0x80000000

    #CNerPC1_CPCCFG0   

   

    ##################################################################################

    # CoreNet Platform Cache 2

    # configure internal CPC2 as SRAM

    # CNetPC2_CPCSRCR0  - SRBARL=0, INTLVEN=0, SRAMSZ=0101, SRAMEN=1

    mem [CCSR 0x11104] = 0x8010000B

    # CPC2_CPCSRCR1

    mem [CCSR 0x11100] = 0x00000000

    # CNetPC2_CPCEWCR0 - disable stashing

    mem [CCSR 0x11010] = 0x00000000

    # CNetPC2_CPCERRDIS

    mem [CCSR 0x11E44] = 0x00000000

    # CNetPC2_CPCERRINTEN

    mem [CCSR 0x11E48] = 0x00000000

    # CPC2_CPCERRCTL

    mem [CCSR 0x11E58] = 0x00ffffff

    # No error injection

     mem [CCSR 0x11E00] = 0x00000000

    mem [CCSR 0x11E04] = 0x00000000

    mem [CCSR 0x11E08] = 0x00000000

    # No speculative memory access

    mem [CCSR 0x11F00] = 0x08000000

    # invalidate(CPCFI) and No flash lock clear(CPCLFC)

    # CNetPC2_CPCCSR0

    mem [CCSR 0x11000] = 0x00200400

    wait 500

    # enable L3 SRAM

    # CNetPC2_CPCCSR0

    mem [CCSR 0x11000] = 0x80000000

   

  ##################################################################################

    # Serial RapidIO - enable timeouts such that cores can be stopped succesfully

    # set timers to max values

    # SRIO_PLTOCCSR

    mem [CCSR 0xC0120] = 0xFFFFFF00

    # SRIO_PRTOCCSR

    mem [CCSR 0xC0124] = 0xFFFFFF00

   

    # SRIO_P1LOPTTLCR

    mem [CCSR 0xD0124] = 0xFFFFFF00

    # SRIO_P2LOPTTLCR

    mem [CCSR 0xD01A4] = 0xFFFFFF00

   

    # set all bits

    # SRIO_P1ERECSR

    mem [CCSR 0xC0644] = 0x007E0037

    # SRIO_P2ERECSR

    mem [CCSR 0xC0684] = 0x007E0037

}

proc P5020DS_init_core_cacheon {} {

   

    ##################################################################################

    #   

    #    Memory Map

    #

    #   0x00000000  0x7FFFFFFF  DDR1       2G

    #     ##0x80000000  0x9FFFFFFF  PEX1       512M##

    #   0x80000000  0x80100000  CPC1       1M

    #   0x80000000  0x80100000  CPC2       1M

    #   0xA0000000  0xBFFFFFFF  PEX2       512M

    #   0xC0000000  0xDFFFFFFF  PEX3       512M

    #   0xE0000000    0xEFFFFFFF  LocalBus   256M

    #   0xF0000000    0xF3FFFFFF  DCSR       4M

    #   0xF4000000    0xF41FFFFF  BMAN       2M

    #   0xF4200000    0xF43FFFFF  QMAN       2M

    #   0xF8000000  0xF800FFFF  PEX1 I/O   64K

    #   0xF8010000  0xF801FFFF  PEX2 I/O   64K

    #   0xF8020000  0xF802FFFF  PEX3 I/O   64K

    #   0xF8200000  0xF82FFFFF  NAND       1M   

    #   0xFE000000  0xFEFFFFFF  CCSR Space 16M

    #   0xFFDF0000  0xFFDF0FFF  PIXIS      4K

    #   0xFFFFF000  0xFFFFFFFF  Boot Page  4k

    #   0x100000000 0x17FFFFFFF DDR2       2G

    #

    ##################################################################################

   

   

    ##################################################################################

    # MMU initialization

   

    global master_core

    variable CAM_GROUP "regPPCTLB1/"

    variable SPR_GROUP "e5500 Special Purpose Registers/"

    variable GPR_GROUP "General Purpose Registers/"

    # define 16MB  TLB entry  1 : 0xFE000000 - 0xFEFFFFFF for CCSR    cache inhibited, guarded

    reg ${CAM_GROUP}L2MMU_CAM1  = 0x7000000A1C08000000000000FE00000000000000FE000001   

   

    # define 256MB TLB entry  2 : 0xE0000000 - 0xEFFFFFFF for LB      cache inhibited, guarded

    reg ${CAM_GROUP}L2MMU_CAM2  = 0x9000000A1C08000000000000E000000000000000E0000001   

   

    # define  1GB  TLB entry  3 : 0x80000000 - 0xBFFFFFFF for PEX1/2  cache inhibited, guarded

    #reg ${CAM_GROUP}L2MMU_CAM3  = 0xA000000A1C08000000000000800000000000000080000001

     # ajout, CPC1 cacheable + coherency

    reg ${CAM_GROUP}L2MMU_CAM3  = 0x500000041C08000000000000800000000000000080000001   

    # define 256MB TLB entry  4 : 0xC0000000 - 0xCFFFFFFF for PEX3    cache inhibited, guarded

    reg ${CAM_GROUP}L2MMU_CAM4  = 0x9000000A1C08000000000000C000000000000000C0000001

   

    # define 256MB TLB entry  5 : 0xD0000000 - 0xDFFFFFFF for PEX3    cache inhibited, guarded

    reg ${CAM_GROUP}L2MMU_CAM5  = 0x9000000A1C08000000000000D000000000000000D0000001

   

    # define 256KB TLB entry  6 : 0xF8000000 - 0xF803FFFF for PEX I/0 cache inhibited, guarded

    reg ${CAM_GROUP}L2MMU_CAM6  = 0x4000000A1C08000000000000F800000000000000F8000001

       

    # define   1GB TLB entry  7 : 0x00000000 - 0x3FFFFFFF for DDR     cacheable

    reg ${CAM_GROUP}L2MMU_CAM7  = 0xA00000041C08000000000000000000000000000000000001

    # define   1GB TLB entry  8 : 0x40000000 - 0x7FFFFFFF for DDR     cacheable

    reg ${CAM_GROUP}L2MMU_CAM8  = 0xA00000041C08000000000000400000000000000040000001

    # define   1MB TLB entry  9 : 0xF4000000 - 0xF40FFFFF for BMAN    cacheable

    reg ${CAM_GROUP}L2MMU_CAM9  = 0x500000041C08000000000000F400000000000000F4000001

   

    # define   1MB TLB entry 10 : 0xF4100000 - 0xF41FFFFF for BMAN    cache inhibited, guarded

    reg ${CAM_GROUP}L2MMU_CAM10 = 0x5000000A1C08000000000000F410000000000000F4100001

   

    # define   1MB TLB entry 11 : 0xF4200000 - 0xF42FFFFF for QMAN    cacheable

    reg ${CAM_GROUP}L2MMU_CAM11 = 0x500000041C08000000000000F420000000000000F4200001

   

    # define   1MB TLB entry 12 : 0xF4300000 - 0xF43FFFFF for QMAN    cache inhibited, guarded

    reg ${CAM_GROUP}L2MMU_CAM12 = 0x5000000A1C08000000000000F430000000000000F4300001

    # define   4MB TLB entry 13 : 0xF0000000 - 0xF03FFFFF for DCSR    cache inhibited, guarded

    reg ${CAM_GROUP}L2MMU_CAM13 = 0x6000000A1C08000000000000F000000000000000F0000001

    # define   4KB TLB entry 14 : 0xFFDF0000 - 0xFFDF0FFF for PIXIS   cache inhibited, guarded

    reg ${CAM_GROUP}L2MMU_CAM14 = 0x1000000A1C08000000000000FFDF000000000000FFDF0001

  # define   1MB TLB entry 16 : 0xF8200000 - 0xF82FFFFF; for NAND,  cache inhibited, guarded

  reg ${CAM_GROUP}L2MMU_CAM16 = 0x5000000A1C08000000000000F820000000000000F8200001

      #define 1MB TLB entry 15 : 0x8010_0000  for CPC2 cacheable + coherency

      reg ${CAM_GROUP}L2MMU_CAM15  = 0x500000041C08000000000000801000000000000080100001

    # init board, only when the init is run for master core

    variable proc_id [expr {[reg ${SPR_GROUP}PIR %d -np] >> 5 }]

    if {$proc_id == $master_core} {

        init_board

    }

   

    ##################################################################################

    # Interrupt vectors initialization

    # interrupt vectors in RAM at 0x[expr {${proc_id} << 2}]0000000

    # IVPR (default reset value)

    set Ret [catch {evaluate __start__SMP}]

   

    if {$Ret} {

        reg ${SPR_GROUP}IVPR = 0x[expr {${proc_id} << 2}]0000000

    } else {

        # SMP project, same interrupt vectors for all cores

        reg ${SPR_GROUP}IVPR = 0x00000000

   }

   

    # interrupt vector offset registers

    # IVOR0 - critical input

    reg ${SPR_GROUP}IVOR0 = 0x00000100   

    # IVOR1 - machine check

    reg ${SPR_GROUP}IVOR1 = 0x00000200   

    # IVOR2 - data storage

    reg ${SPR_GROUP}IVOR2 = 0x00000300   

    # IVOR3 - instruction storage

    reg ${SPR_GROUP}IVOR3 = 0x00000400   

    # IVOR4 - external input

    reg ${SPR_GROUP}IVOR4 = 0x00000500   

    # IVOR5 - alignment

    reg ${SPR_GROUP}IVOR5 = 0x00000600   

    # IVOR6 - program

    reg ${SPR_GROUP}IVOR6 = 0x00000700

    # IVOR7 - floating point unavailable

    reg ${SPR_GROUP}IVOR7 = 0x00000800   

    # IVOR8 - system call

    reg ${SPR_GROUP}IVOR8 = 0x00000c00   

    # IVOR10 - decrementer

    reg ${SPR_GROUP}IVOR10 = 0x00000900   

    # IVOR11 - fixed-interval timer interrupt

    reg ${SPR_GROUP}IVOR11 = 0x00000f00   

    # IVOR12 - watchdog timer interrupt

    reg ${SPR_GROUP}IVOR12 = 0x00000b00   

    # IVOR13 - data TLB errror

    reg ${SPR_GROUP}IVOR13 = 0x00001100   

    # IVOR14 - instruction TLB error

    reg ${SPR_GROUP}IVOR14 = 0x00001000   

    # IVOR15 - debug

    reg ${SPR_GROUP}IVOR15 = 0x00001500   

    # IVOR35 - performance monitor

    reg ${SPR_GROUP}IVOR35 = 0x00001900   

# Doorbell

reg ${SPR_GROUP}IVOR36 = 0x00001200

    ###################################################################

    # Enable caches

   

    # L1 init: CFI, CE, ICFI, ICE

#    reg ${SPR_GROUP}L1CSR0 = 0x00000003

#    reg ${SPR_GROUP}L1CSR1 = 0x00000003

   

  # ajout #############################

  # desactive L1 dcache

  reg ${SPR_GROUP}L1CSR0 = 0x00000002

  # active L1 icache

  reg ${SPR_GROUP}L1CSR1 = 0x00010001

  #####################################

    # L2 init: L2E, L2FI

#    reg ${SPR_GROUP}L2CSR0 = 0x80200000

  # ajout

  # desactive L2 cache (unifie)

  reg ${SPR_GROUP}L2CSR0 = 0x00000000

   

  ##################################################################################

  # Enable branch prediction

# reg ${SPR_GROUP}BUCSR = 0x01400201

 

  # ajout

  # disable branch prediction

  reg ${SPR_GROUP}BUCSR = 0x00000200 

  ##################################################################################

    # Debugger settings

   

    # enable machine check

    #reg ${SPR_GROUP}HID0 = 0x80000000

  # ajout

  # Enable machine check signal + L2MMU multihits detection

   reg ${SPR_GROUP}HID0 = 0xc0000000

   

    # enable floating point

    reg ${SPR_GROUP}MSR = 0x00002000

   

    # infinite loop at program exception to prevent taking the exception again

    mem v:0x${proc_id}0000700 = 0x48000000

   

    # prevent stack unwinding at entry_point/reset when stack pointer is not initialized

    reg ${GPR_GROUP}SP = 0x000000000000000F

   

    if {$proc_id == $master_core} {

        # BRRL - enable all cores

        # DCFG_BRR

        mem [CCSR 0xE00E4] = 0x00000003

        # CTBENL - enable all cores' timebase

        # RCPM_CTBENR

        mem [CCSR 0xE2084] = 0x00000003

    }   

}

proc envsetup {} {

    # Environment Setup

    radix x

    config hexprefix 0x

    config MemIdentifier v

    config MemWidth 32

    config MemAccess 32

    config MemSwap off

}

#-------------------------------------------------------------------------------

# Main                                                                         

#-------------------------------------------------------------------------------

  envsetup

 

  P5020DS_init_core_cacheon

0 件の賞賛
返信

1,703件の閲覧回数
marius_grigoras
NXP Employee
NXP Employee

Hi,

First of all can you tell me please why you need such a configuration?

What you need in your program? Full DDR working, SRAM configuration...or DDR+cache activated?

I'm asking because you somehow did a mix between all these 3 configurations. Moreover, the DDR1 is configured (both TLB, LAW and Controller) from 0x0, but in the same time you initialized and the SRAM memory from the same address - 0x0. Secondly, the DDR2 LAW is commented, but the DDR Controller is still initialized.

If you really need the all 3 configurations in the same time, try to mix the init_core.tcl file (this will initialize the DDR from 0x0), take the SRAM initialization (L3) from init_sram.tcl file, but re-mapping it from another address - be sure to not be in the same space with DDR (I guess you want to use it as another memory, right?) and if you need and the L1/L2 caches activated take the initialization from init_core_cacheon.tcl file (removes the L3 cache part because you're using it as SRAM).

Thank you,

Marius

1,703件の閲覧回数
pierre-antoinem
Contributor III

Thanks for replying Marius.

So in the absolute the DDR mustn't be interleaved, so DDR1 with 2GB menory space and DDR2 with another 2GB memory space. (DDR2 was desactivated because it wasn't working)

Cache L2 desactivated L1 cache instruction activated and data desactivated.

CPC1 and CPC2 as SDRAM.

This is the configuration that I need.

Actualy I was porting some code and saw that core0 had alot of trouble it crash's with the same error as shown but just before going on a return 0, in the main() when the program was finished.

I started testing ans saw that a simple printf() on the core0 makes it crash.. so I thought it might be related.

normaly DDR1 is from 0x0 to 0x7777_777C

the CPC1 starts at 0x8000_0000 to 0x800F_FFFC

and CPC2 from 0x8010_0000 to 0x801F_FFFC

tested DDR1, CPC1 and CPC2 all worked, I was able to read and write at these adress's.

Can't explain why core0 gets illegal instruction exception.

I'll recheck the TCL.

0 件の賞賛
返信