IFC and memory stall on multi core

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IFC and memory stall on multi core

1,843 Views
eduard_stefes
Contributor I

Hi,

we use the LS1020a QoriQ and have something connected via IFC GPCM ASIC mode. Currently we run into race conditions then independent parts of the software try to read via IFC at the same time. Chapter 24 of LS1021ARM.pdf does not mention anything about memory stalling.

my question:

Is it possible to stall both cores when one core is doing an operation via IFC or does this need to be handled via software mutexes?

0 Kudos
Reply
3 Replies

1,765 Views
eduard_stefes
Contributor I

This is not what we see. here a detailed description of our problem:

Setup:

+----+  read#1        +--------+
|CPU0+------+         |        |                 +---------+
+----+      +-------->+ IFC    |                 | Device  |
                      | mapped |   +-------+     |         |
+----+      +-------->+ memory +---> IFC   +---->+         |
|CPU1+------+         |        |   +-------+     |         |
+----+  read#2        |        |                 +---------+
                      |        |
                      +--------+


Problem:
- the Software issues read#1 on cpu0

- cpu0 stalls and waits for read to finish

- software issues read#2 on cpu1

- even trough read#1 is still in progress the IFC starts the next read and does not wait for read#0 to finish

=> the stall on cpu0 is not release => the system crashes

Possible solutions:

- stall both cpus then read#1 happens.

- implement a software mutex for the complete IFC mapped memory area (this is hard because we use IFC to access multiple devices).

0 Kudos
Reply

1,765 Views
Bulat
NXP Employee
NXP Employee

Are you able to look at IFC behavior with a scope or a logic analyser? Do you see two different CS's are asserted simultaneously?

Regards,

Bulat

0 Kudos
Reply

1,765 Views
Bulat
NXP Employee
NXP Employee

I do not understand the problem with "memory stalling". The IFC will execute both requests from both cores in the order as they come. No "stall" condition is expected.

Regards,

Bulat

0 Kudos
Reply