IFC Timing Calculation for T2081 Custom Board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IFC Timing Calculation for T2081 Custom Board

2,707 Views
hemanttiwari199
Contributor III

Hi All,

I have interface Micron MT28FW02GBBA1HPC-0AAT Parallel NOR Flash to my custom T2081 IFC Controller. I want to calculate the IFC Timing Details in order to access the NOR Flash. 

Please suggest a way to calculate the timing details. 

Regards

Hemant

0 Kudos
Reply
5 Replies

2,702 Views
yipingwang
NXP TechSupport
NXP TechSupport
0 Kudos
Reply

2,694 Views
hemanttiwari199
Contributor III

Hi yipingwang,

Thanks for the prompt response.

I am trying to calculate the IFC Timing Calculation using the Excel sheet provide in the link shared by you.

But in order to calculate IFC_FTIM0 as per T2080 RM we require TACSE,TEADC,TAVDS and TEAHC but in the excel FTIM0 only consist of TACSE, TEADC and TEAHC.

hemanttiwari199_0-1634017982016.png

 

Please confirm the whether we can go ahead with the same calculation sheet.

 

Regards

0 Kudos
Reply

2,687 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please go ahead with this calculation sheet.

For TAVDS, we use zero for this field for NOR flash connection.

 

0 Kudos
Reply

2,653 Views
hemanttiwari199
Contributor III

thanks for the suggestion. 

Also, Can you suggest NOR Flash in CodeWarrior device list to do flash programing which is equivalent to the part number (MT28FW02GBBA1HPC-0AAT) which i have used in my custom board.

Regards

Hemant

0 Kudos
Reply

2,636 Views
yipingwang
NXP TechSupport
NXP TechSupport

There is no this flash in CodeWarrior device list.

You could refer to C:\Freescale\CW_PA_v10.5.1\PA\PA_Tools\FlashToolKit\Documentation\AppNote-FlashProgrammer-PowerArchitecture.pdf to add new flash algorithm and a new flash device in CodeWarrior.

0 Kudos
Reply