I'm using LS1043A in my design, and we are not using QE in our board. In RCW what should i Set for bit 166(HDLC1_MODE) and 167(HDLC2_MODE)?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I'm using LS1043A in my design, and we are not using QE in our board. In RCW what should i Set for bit 166(HDLC1_MODE) and 167(HDLC2_MODE)?

279 Views
logeshs
Contributor II

We are not using QUICC Engine in LS1043A, In RCW setting what should we keep, 0 or 1 in the bit 166 and 167?

0 Kudos
1 Reply

218 Views
r8070z
NXP Employee
NXP Employee

Have a great day,

Set these bits to 0. It has sense when the TxD pins are open and does not has pull-ups. In all other cases while you do not use these pins as the TxD these bits are irrelevant.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos