I am installing QorIQ SDKV1.7 on Ubuntu 14.04 and getting following error while executing host-prepare.sh in QorIQ-SDK-V1.7-20141218-yocto/poky/scripts folder
Package texinfo is not available, but is referred to by another package.
This may mean that the package is missing, has been obsoleted, or
is only available from another source
However the following packages replace it:
info install-info
Package git-core is not available, but is referred to by another package.
This may mean that the package is missing, has been obsoleted, or
is only available from another source
Package autoconf is not available, but is referred to by another package.
This may mean that the package is missing, has been obsoleted, or
is only available from another source
Package libtool is not available, but is referred to by another package.
This may mean that the package is missing, has been obsoleted, or
is only available from another source
E: Unable to locate package subversion
E: Package 'git-core' has no installation candidate
E: Unable to locate package texi2html
E: Package 'texinfo' has no installation candidate
E: Unable to locate package libsdl1.2-dev
E: Couldn't find any package by regex 'libsdl1.2-dev'
E: Unable to locate package docbook-utils
E: Unable to locate package fop
E: Unable to locate package gawk
E: Unable to locate package python-pysqlite2
E: Unable to locate package build-essential
E: Unable to locate package xsltproc
E: Unable to locate package chrpath
E: Unable to locate package libgl1-mesa-dev
E: Unable to locate package libglu1-mesa-dev
E: Package 'autoconf' has no installation candidate
E: Unable to locate package automake
E: Package 'groff' has no installation candidate
E: Package 'libtool' has no installation candidate
E: Unable to locate package libxml-parser-perl
E: Unable to locate package cvs
E: Unable to locate package tofrodos
E: Unable to locate package libstring-crc32-perl
E: Unable to locate package libbonobo2-common
E: Unable to locate package libncurses5-dev
ERROR: Fail to install pkgs on host! See message above...
-
It looks like that there is no internet connection for your Linux host.
Test your Ubuntu using “ping” command.
Do you see connection for the following command: “ping www.google.com”.
Hi Pavel,
I got through this and successfully run the host-prepare.sh file but now I want to install the tool chain, I am getting this error on my terminal. Pls suggest.
mhnayeem@mhnayeem-ThinkCentre-A58:~/Desktop/QorIQ-SDK-V1.7-20141218-yocto/build_p2020rdb_release$ bitbake fsl-toolchain
bitbake: command not found
See instructions on the following page:
Yes I am following these instructions only but when I am executing bitbake fsl-toolchain , I am getting error bitbake: command not found
It looks like that the following command was not issued from SDK installing folder:
Hi Pavel,I already executed this command for p2020rdb. Pls suggest.
Do you see the following message on the screen after "source ./poky/fsl-setup-poky" command?
Run the following commands to start a build:
bitbake fsl-image-lsb-sdk
bitbake fsl-image-minimal
bitbake fsl-image-kvm
bitbake fsl-image-full
bitbake fsl-image-core
bitbake fsl-image-flash
After running the command source ./poky/fsl-setup-poky -m p2020rdb , I am getting following message -
/home/mhnayeem/Desktop/QorIQ-SDK-V1.7-20141218-yocto/build_p2020rdb_release was created before. Override its configuration files? Y|n
Ok I did it
Now pls tell me relevance of following line ... I mean what needs to be done -
To use the installed toolchain, go the the location where the toolchain is installed and source the
environment-setup-<core>
file. This will set up the correct path to the build tools and also export some environment variables relevant for development
Pls also tell me 1 thing
I am new to the SDK Environment
I need to write a serial application to configure a UART port of P2020rdb using SDK V1.7
Pls advise me how to proceed.
Thanks in advance.
There are a lot information in internet.
http://ftp1.digi.com/support/documentation/uart_appkit_digiel.pdf
http://esatjournals.org/Volumes/IJRET/2014V03/I07/IJRET20140307066.pdf
Thanks Pavel.
Any information relevant for QorIQ processor (P2020RDB specifically) for serial application using SDK v 1.7
The QorIQ SDK Linux does not require special information for UART using.
No,
I am asking any pdf document for UART Programming of the P2020RDB using SDK
Press 'Y' or 'n'