How to enable UART2 in P2040

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to enable UART2 in P2040

1,491 Views
gouravjain
Contributor IV

Hi All,

In my custom board which is based on P2041RDB, by default console prints are coming in UART1. But i wanted to get the output prints on UART2 instead UART1.  Following changes have been made from my end,

1) changed RCW[366:368] from 011 to 101

2) changed uboot parameter "consoldev" from ttyS0 to ttyS1.

but still prints are coming in UART1.

Note: As of now i'm trying at uboot level only. 

Can some one guide me what else change is required ??

Thanks,

Gourav

0 Kudos
Reply
4 Replies

1,332 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello gourav jain,

Please edit u-boot configuration file include/configs/P2041RDB.h, please find the section "Serial Port", and change the variable "CONFIG_CONS_INDEX" to "2" instead of "1", then rebuild u-boot.

In addition, in Kernel bootargs, please change bootargs as "root=/dev/ram rw console=ttyS1,115200" rather than "console=ttyS0".


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,332 Views
gouravjain
Contributor IV

Hi Yiping,

Thanks for your help. Its working now.

Have one dobt can't we enable both the UART together ??

--

Gourav

0 Kudos
Reply

1,332 Views
gouravjain
Contributor IV

Hi Yiping,

Waiting for your response....

0 Kudos
Reply

1,332 Views
gouravjain
Contributor IV

Hi Yiping Wang,

UART-1 and UART-2 both are working individually. How can i get the data in both the UARTs simultaneously ??

regards,

Gourav

0 Kudos
Reply