How to do a SW reset for A72

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to do a SW reset for A72

1,236 Views
vijaykumardesai
Contributor II

I am using LS1046A[A72] processor, I wanted to do a software reset. Is writing to RMR_EL3 the only way to trigger SW reset.

It is an EL3 register u-boot leaves in EL2, so I can not set this register.

Is there any alternate way to perform the SW reset.

0 Kudos
Reply
1 Reply

1,073 Views
Pavel
NXP Employee
NXP Employee

Look at the Section 4.4.3 of the LS1046A Reference Manual Rev 1:

https://www.nxp.com/webapp/Download?colCode=LS1046ARM

 

This Section contains command sequence for core soft reset.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply