How to conect BSC9131 and MAX2580 properly for both TDD and FDD?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to conect BSC9131 and MAX2580 properly for both TDD and FDD?

557 Views
EduardKantsypa
Contributor I

Is there any application circuits for combination BSC9131 + MAX2580?

0 Kudos
1 Reply

424 Views
lunminliang
NXP Employee
NXP Employee

Hello EduardKantsypa,

Yes BSC9131RDB use connector to work with RF Card, Public Wireless Incorporation has ever designed such an RFIC daughter card, exactly based on MAX2580. You may contact them for the schematic.


Have a great day,
Lunmin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos