Hello,
I am currently working on a T4240RDB board. I am using the pre-built u-boot and linux OS on the T4 board. I am able to connect to the console via serial port.
Problems:
1. Every time when reboot the board, it brings up a brand new system, and wiped out all the changes I did on the board before reboot. Is there any solution to this problem?
2. We will need to use DHCP to get IP address, where can I find any instructions to configuration on T4 board?
Thanks very much for your input!
Regards,
Peng
已解决! 转到解答。
Hi Peng,
1, This is normal, because you load the rootfs in ram from tftp or flash, and at every reset the initial image will be loaded.
2. Recommended is to use nsf boot. The advantage is you can customize the rootfs, and all the changes will be saved on nfs server. You can find useful info here: Deployment on Target Board.
Adrian
Hi Peng,
1, This is normal, because you load the rootfs in ram from tftp or flash, and at every reset the initial image will be loaded.
2. Recommended is to use nsf boot. The advantage is you can customize the rootfs, and all the changes will be saved on nfs server. You can find useful info here: Deployment on Target Board.
Adrian
Hi, Peng
For boot of T4240RDB board, you may refer to the thread: Re: Boot-up options for T4240RDB