How to activate ALTIVEC2 in gcc ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to activate ALTIVEC2 in gcc ?

跳至解决方案
4,202 次查看
aloishahn
Contributor III

Hi,

this is a specific question about using the new altivec instructions (altivec2 extensions) of the e6500 in gcc

I use the target specific option -mcpu=e6500.

Building file: main.cpp

"/home/freescale/CodeWarrior_PA_10.4.0/eclipse/../Cross_Tools/gcc-4.8.2-Ee6500-aeabi/bin/powerpc-aeabi-g++" "../Sources/main.cpp" @"Sources/main_1.args" -o"Sources/main.o"

Sources/main_1.args : -O0 -g -Wall -std=c++0x -trigraphs -fno-use-cxa-atexit -fno-exceptions -frtti -fno-threadsafe-statics --param max-inline-recursive-depth=8 -c -mbig-endian -fno-builtin -fomit-frame-pointer -Wno-unknown-pragmas -m32 -mcpu=e6500 

With this option he compiler sets the predefined macro __ALTIVEC__,

which ist checked

e.g. in #include <altivec.h>

altivec.h

#if !defined(__VEC__) || !defined(__ALTIVEC__)

#error Use the "-maltivec" flag to enable PowerPC AltiVec support

#endif

altivec.h checks __ALTIVEC2__ as well

#ifdef __ALTIVEC2__

/* New Altivec instructions */

#define vec_absd __builtin_vec_absd

#define vec_lvexbx __builtin_vec_lvexbx

#define vec_lvexhx __builtin_vec_lvexhx

#define vec_lvexwx __builtin_vec_lvexwx

#define vec_stvexbx __builtin_vec_stvexbx

#define vec_stvexhx __builtin_vec_stvexhx

#define vec_stvexwx __builtin_vec_stvexwx

#define vec_lvswx __builtin_vec_lvswx

#define vec_lvswxl __builtin_vec_lvswxl

#define vec_stvswx __builtin_vec_stvswx

#define vec_stvswxl __builtin_vec_stvswxl

#define vec_lvsm __builtin_vec_lvsm

#define vec_lvtlx __builtin_vec_lvtlx

#define vec_lvtlxl __builtin_vec_lvtlxl

#define vec_lvtrx __builtin_vec_lvtrx

#define vec_lvtrxl __builtin_vec_lvtrxl

#define vec_stvflx __builtin_vec_stvflx

#define vec_stvflxl __builtin_vec_stvflxl

#define vec_stvfrx __builtin_vec_stvfrx

#define vec_stvfrxl __builtin_vec_stvfrxl

#endif

Apparently __ALTIVEC2__ is not set by the -mcpu=e6500 setting.

Seems that -maltivec2 option does the job and sets __ALTIVEC2__.

Should I use -maltivec2 option? Are there any recommendations ?
Does gcc generate new altivec instructions when I just use -mcpu=e6500 w/o-maltivec2 ?

best regards

Alois

1 解答
2,801 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Alois,

In order to active ALTIVEC2 in the compiler, you need to define "#include <altivec.h>" in you source file, and add build option "-maltivec2" from Project->Properties->C/C++ Build->Setting->PowerPC AEABI e6500 C Compiler->Miscellaneous->other flags in CodeWarrior 10.4. In CodeWarrior 10.3.3(GCC 4.7), "-maltivec2" is enabled automatically if -mcpu=e6500 enabled, you could find this information from the attached patch gcc.e6500-FSF47 for CW 10.3.3. The patch gcc.e6500-FSF-48 is for CW 10.4.

Please refer to the following content in gcc.e6500-FSF47.

-@gccoptlist{-maltivec  -mfprnd  -mhard-float  -mmfcrf  -mmultiple @gol

--mnew-mnemonics  -mpopcntb -mpopcntd  -mpower  -mpower2  -mpowerpc64 @gol

--mpowerpc-gpopt  -mpowerpc-gfxopt  -msingle-float -mdouble-float @gol

--msimple-fpu -mstring  -mmulhw  -mdlmzb  -mmfpgpr -mvsx}

+@gccoptlist{-maltivec -maltivec2 -mfprnd -mhard-float -mmfcrf

+-mmultiple @gol -mnew-mnemonics -mpopcntb -mpopcntd -mpower -mpower2

+-mpowerpc64 @gol -mpowerpc-gpopt -mpowerpc-gfxopt -msingle-float

+-mdouble-float @gol -msimple-fpu -mstring -mmulhw -mdlmzb -mmfpgpr

+-mvsx}


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,801 次查看
aloishahn
Contributor III

addon:

seems that gcc-4.7.2-Ee6500 and gcc-4.8.2-Ee6500 behave different in that respect

freescale@freescale-sdk:~/LinuxShared/workspace_01_10.4.0/Hello_Hip-core00/RAM$ "/home/freescale/CodeWarrior_PA_10.3.3/eclipse/../Cross_Tools/gcc-4.7.2-Ee6500-aeabi/bin/powerpc-aeabi-g++" "../Sources/hipLinInterpolateVect4.cpp" -O0 -g -Wall -std=c++0x -trigraphs -fno-use-cxa-atexit -fno-exceptions -frtti -fno-threadsafe-statics --param max-inline-recursive-depth=8 -c -mbig-endian -fno-builtin -fomit-frame-pointer -Wno-unknown-pragmas -m32 -mcpu=e6500 -o"Sources/hipLinInterpolateVect4.o"

freescale@freescale-sdk:~/LinuxShared/workspace_01_10.4.0/Hello_Hip-core00/RAM$ "/home/freescale/CodeWarrior_PA_10.4.0/eclipse/../Cross_Tools/gcc-4.8.2-Ee6500-aeabi/bin/powerpc-aeabi-g++" "../Sources/hipLinInterpolateVect4.cpp" -O0 -g -Wall -std=c++0x -trigraphs -fno-use-cxa-atexit -fno-exceptions -frtti -fno-threadsafe-statics --param max-inline-recursive-depth=8 -c -mbig-endian -fno-builtin -fomit-frame-pointer -Wno-unknown-pragmas -m32 -mcpu=e6500 -o"Sources/hipLinInterpolateVect4.o"

../Sources/hipLinInterpolateVect4.cpp: In function 'void hipLinInterpolateVect4_vec(sVECT_d4*, ucVECT4*, ucVECT4*, sVECT_d4*, short unsigned int, unsigned int, unsigned int)':

../Sources/hipLinInterpolateVect4.cpp:92:79: error: 'vec_lvtlxl' was not declared in this scope

    const vector int16_t vi16OffsetTemp_dp = vec_lvtlxl (0, (int16_t*)ptOffset);

                                                                              ^

../Sources/hipLinInterpolateVect4.cpp:191:73: error: 'vec_lvtlx' was not declared in this scope

        vu8VectUL = vec_lvtlx (0, (uint8_t*)(ptSrcVect                ));

                                                                        ^

0 项奖励
回复
2,802 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Alois,

In order to active ALTIVEC2 in the compiler, you need to define "#include <altivec.h>" in you source file, and add build option "-maltivec2" from Project->Properties->C/C++ Build->Setting->PowerPC AEABI e6500 C Compiler->Miscellaneous->other flags in CodeWarrior 10.4. In CodeWarrior 10.3.3(GCC 4.7), "-maltivec2" is enabled automatically if -mcpu=e6500 enabled, you could find this information from the attached patch gcc.e6500-FSF47 for CW 10.3.3. The patch gcc.e6500-FSF-48 is for CW 10.4.

Please refer to the following content in gcc.e6500-FSF47.

-@gccoptlist{-maltivec  -mfprnd  -mhard-float  -mmfcrf  -mmultiple @gol

--mnew-mnemonics  -mpopcntb -mpopcntd  -mpower  -mpower2  -mpowerpc64 @gol

--mpowerpc-gpopt  -mpowerpc-gfxopt  -msingle-float -mdouble-float @gol

--msimple-fpu -mstring  -mmulhw  -mdlmzb  -mmfpgpr -mvsx}

+@gccoptlist{-maltivec -maltivec2 -mfprnd -mhard-float -mmfcrf

+-mmultiple @gol -mnew-mnemonics -mpopcntb -mpopcntd -mpower -mpower2

+-mpowerpc64 @gol -mpowerpc-gpopt -mpowerpc-gfxopt -msingle-float

+-mdouble-float @gol -msimple-fpu -mstring -mmulhw -mdlmzb -mmfpgpr

+-mvsx}


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,801 次查看
aloishahn
Contributor III

Hi Yiping,

OK, thats fine for me now.

Just to be sure: so -maltivec2 (and -mcpu=e6500) will be required in future versions of gcc as well?

regards

Alois

0 项奖励
回复
2,801 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Alois,

Yes, and I suggest you add "-maltivec2" in the compiler options in your project from CodeWarrior IDE, no need to consider about GCC version.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------