How to Enable USB wifi Dongle for LS1012A in linux kernel

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to Enable USB wifi Dongle for LS1012A in linux kernel

1,332 Views
minalnemade
Contributor II

Hi,

We are using LS1012A FRDM board. We want to configure usb wifi dongle Edimax EW-7811Un. After connecting USB dongle to LS1012AFRDM board I am getting following messages in kernel log during bootup.

........

.........

Configuring network interfaces... done.  
Starting system message bus: dbus.  
Starting HOSTAP Daemon: Configuration file: /etc/hostapd.conf  
ioctl[PRISM2_IOCTL_PRISM2_PARAM]: Invalid argument  
Could not enable hostapd mode for interface wlan0  
hostap driver initialization failed.  
wlan0: interface state UNINITIALIZED->DISABLED  
wlan0: AP-DISABLED   
hostapd_free_hapd_data: Interface wlan0 wasn't started  
Starting system log daemon...0  
Starting kernel log daemon...0  
Starting internet superserver: xinetd.

As can be observed form above log hostap driver initialization is failing so kindly suggest How to resolve this issue.

Thanks & regards

Minal

Tags (1)
0 Kudos
Reply
2 Replies

1,086 Views
Pavel
NXP Employee
NXP Employee

Look at attached file.

It is snapshot from SDK 2.0-1703 kernel menu for the LS1012a FRDM board.

This file shows supported WiFi board.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,086 Views
minalnemade
Contributor II

Hi Pavel,

Thanks for the information.

I have done the required configuration in kernel config for Edmax wifi

dongle (realtek 8192cu). please go through attached file.

I am getting following messages. Details log file attached

1. IPv6: ADDRCONF(NETDEV_UP): wlan0: link is not ready

2. hostap driver initialization failed.

3. cfg80211: Calling CRDA to update world regulatory domain

So please help us to resolve above errors

Thanks & Regards

Minal

0 Kudos
Reply