How do we configure a specific port in SJA1105 Ethernet Switch Chip

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How do we configure a specific port in SJA1105 Ethernet Switch Chip

Jump to solution
1,281 Views
ramesh_mali
Contributor II

How do we configure a specific port in SJA1105, how can we disable a port or configure it based on the trans receiver connected to them?

We are referring to Software user manual - UM11040 for general configuration.sja1105 #ethernet switch

Tags (2)
1 Solution
1,129 Views
bpe
NXP Employee
NXP Employee

I assume you are asking about SJA1105P/Q/R/S series switch because
the document you mentioned is no applicable to SJA1105/05T.
Posts can be deactivated by setting xMII_MODE[n]. See UM11040, Table 29.

The rest of per-port parameters are configured in RGU, CGU and
ACU tables, see UM11040 Sections 5.3 through 5.5 and 6.2 through 6.4.

Hope this helps
Platon

View solution in original post

2 Replies
1,130 Views
bpe
NXP Employee
NXP Employee

I assume you are asking about SJA1105P/Q/R/S series switch because
the document you mentioned is no applicable to SJA1105/05T.
Posts can be deactivated by setting xMII_MODE[n]. See UM11040, Table 29.

The rest of per-port parameters are configured in RGU, CGU and
ACU tables, see UM11040 Sections 5.3 through 5.5 and 6.2 through 6.4.

Hope this helps
Platon

1,129 Views
ramesh_mali
Contributor II

Thanks for your quick response Platon. This surely helps.

0 Kudos