How can I recover P4080PCIE BANK0?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can I recover P4080PCIE BANK0?

Jump to solution
1,439 Views
JHY
Contributor IV

It was erased BANK0 of P4080PCIE by mistake.

After that, there is no message in console when power up.

In this case, what is needed for restoring bootloader?

Labels (1)
0 Kudos
1 Solution
1,256 Views
addiyi
NXP Employee
NXP Employee

You should use CodeWarrior for PA to recover the board. Flash Programmer allow you to program the new uboot into the flash. If you want to use Flash Programmer, you have to select S29GL01GP. A preconfigured target task already exists in:

PA_10.0\bin\plugins\support\TargetTask\FlashProgrammer\QorIQ_P4\P4080PCIe_NOR_FLASH.xml.

Please refer to Flash Programmer for CodeWarrior Power Architecture for more information about how to use Flash Programmer.

Adrian

View solution in original post

0 Kudos
2 Replies
1,256 Views
lunminliang
NXP Employee
NXP Employee

Hi,

As suggested by Stoica, please download CodeWarrior for PA from Freescale website:

CodeWarrior Dev Tools for Power Architecture|Freescale

The latest version is 10.4 and it contains 30 days evaluation license.

Regards

0 Kudos
1,257 Views
addiyi
NXP Employee
NXP Employee

You should use CodeWarrior for PA to recover the board. Flash Programmer allow you to program the new uboot into the flash. If you want to use Flash Programmer, you have to select S29GL01GP. A preconfigured target task already exists in:

PA_10.0\bin\plugins\support\TargetTask\FlashProgrammer\QorIQ_P4\P4080PCIe_NOR_FLASH.xml.

Please refer to Flash Programmer for CodeWarrior Power Architecture for more information about how to use Flash Programmer.

Adrian

0 Kudos