How can I configure the the SerDes1 & SerDes2 register to achieve three x4 PCIe & two x4 SATA in T2080 processor ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can I configure the the SerDes1 & SerDes2 register to achieve three x4 PCIe & two x4 SATA in T2080 processor ?

1,119 Views
soumyasephalika
Contributor I

Hi,

I am planning to used T2080 processor in my board. I need to achieve three x4 PCIe & two x4 SATA by using SerDes1 & SerDes2.

As per the SerDes register details given in the Table 19-2. SerDes Lanes Assignments and Multiplexing in the T2080_T2081 Reference Manual RevC.1(refer attachment) the there are two different register for two SerDes such as SRDS_PRTCL_S1 & SRDS_PRTCL_S2.

How to achieve three x4 PCIe & two x4 SATA ?

Regards

Soumya

0 Kudos
Reply
2 Replies

967 Views
LPP
NXP Employee
NXP Employee

This configuration is not supported.

Please, refer to T2080 RM Table 19-1 SerDes Lanes Assignments and Multiplexing.

- two x1 SATA are available (no x4 SATA)

- three x4 PCIe configuration can't coexist with SATA.

Closest match is : two x4 PCIe, one x2 PCIe and two x1 SATA

[SRDS_PRTCL_S1,SRDS_PRTCL_S2] = [6C,16]

[SRDS_PRTCL_S1,SRDS_PRTCL_S2] = [A4,16]

[SRDS_PRTCL_S1,SRDS_PRTCL_S2] = [96,16]

[SRDS_PRTCL_S1,SRDS_PRTCL_S2] = [8A,16]

[SRDS_PRTCL_S1,SRDS_PRTCL_S2] = [66,16]

[SRDS_PRTCL_S1,SRDS_PRTCL_S2] = [66,15]


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

967 Views
soumyasephalika
Contributor I

Hi,

Thank you for the reply.

My requirement is three x4 PCIe & two x1 SATA.

Can I able to configure the two Serder interface independently ?

Otherwise I need to go for the two x4 PCIe, two x1 PCIe & two x1 SATA.

Kindly let me know why can't we configure the two serdes registers independently.

Regards

Soumya

0 Kudos
Reply