Hi, Let us know if nxp provides the BSP for "RD_P1020WLANS: QorIQ P1020-WLAN Access Point/Router" that can supports on OpenWrt.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Hi, Let us know if nxp provides the BSP for "RD_P1020WLANS: QorIQ P1020-WLAN Access Point/Router" that can supports on OpenWrt.

780 次查看
niranjankumar
Contributor I

@niranjan.kumar@logic-fruit.com,@dhruv.saxena@logic-fruit.com,

Does NXP or any other third part provides the complete board package for the below mentioned board which will be compatible with the OpenWrt. If it is, please gives the deatils of BSP and the link from where we can get it.

Board Deatils:

RD_P1020WLANS: QorIQ P1020-WLAN Access Point/Router

Thanks,

0 项奖励
回复
1 回复

651 次查看
Pavel
NXP Employee
NXP Employee

NXP offers LTIB Linux BSP for this board:

http://www.nxp.com/products/microcontrollers-and-processors/power-architecture-processors/qoriq-plat...

 

Find the "P1020 WLAN Software Bundle(REV 0)" on this page.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复