Getting started with B4860QDS Board 'out of the box'

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Getting started with B4860QDS Board 'out of the box'

6,140 Views
billchadwick
Contributor III

Sadly, after installing Code Warrior (SC 10.8) and following the instructions in the CW for StarCore getting started guide, we are failing to get a USB TAP connection working with our board (Win XP host).

We need to run some performance tests on the SC3900 cores but are stumped for now.

Any tips for getting the board up and running would be much appreciated.

The images below may help in a diagnosis.

4860qds_fail.PNG.png

4860qds_fail_2.PNG.png

0 Kudos
Reply
35 Replies

3,604 Views
lunminliang
NXP Employee
NXP Employee

Also have you observed LED on the boards? What's the status of D1 and D2?

0 Kudos
Reply

3,604 Views
billchadwick
Contributor III

from CCS I can find the B4860QDS board via USB thus

(bin) 1 % findcc cwtaps

FSL031A32 (00:04:9f:03:1a:32): Embedded CodeWarrior TAP (0)

Power Architecture JTAG/COP Probe Tip

Boot Loader v0.9.2

Operating System v1.0.1

(bin) 2 %

and also like this

(bin) 14 % findcc cwtaps -verbose

FSL031A32 (00:04:9f:03:1a:32:1087):

Main Board = Embedded CodeWarrior TAP (0) {0x0 0x0}

Probe Tip = Power Architecture JTAG/COP

Firmware = Boot Loader {0.9.2}

Firmware = Operating System {1.0.1}

8087&PID_0024 5&1257EA4F&0&1

8087&PID_0024 5&1257EA4F&0&1

no devices found

(bin) 14 %

0 Kudos
Reply

3,604 Views
lunminliang
NXP Employee
NXP Employee

Status of D1 and LD2 are normal.I have produced the same result as yours.

After firmware update, the error disappear.

Please enter below command in CCS windows:

% updatecwtap FSL031A32

After this the versions are:

  Boot Loader v1.0.1

  Operating System v1.0.2

Then connect and try again.

0 Kudos
Reply

3,604 Views
billchadwick
Contributor III

lunminliang

I have done the update. It looked to work OK.

Now I am getting

Error launching TryUpdated_Debug_B4860_Download_core00

CCSProtocolPlugin : CCS: Core not supported

Any ideas what is wrong now ?

Bill.

0 Kudos
Reply

3,604 Views
billchadwick
Contributor III

CCS shows log below.The connection #1 lines are from an attempt to connect the CodeWarrior debugger.

Does the "no command converters" bit matter (it is shown in red) ?

CodeWarrior Connection Server console display active (Tcl8.4.12 / Tk8.4.12)

Loading CCSAPI Tcl interface (C:/Freescale/CW_SC_v10.8.0/SC/ccs/bin/ccstcl.dll)...

Loading Svfburner (C:/Freescale/CW_SC_v10.8.0/SC/ccs/bin/svfburner.dll)...

There are no command converters configured

Server listening on port: 41475

Clients allowed from all hosts

No clients denied

CCSAPI connection #1 accepted from localhost at Tue Sep 23 08:55:19 2014

CCSAPI connection #1 from localhost closed at Tue Sep 23 08:55:32 2014

(bin) 1 % findcc cwtaps -verbose

{amphisbaena} FSL031A32 (00:04:9f:03:1a:32:1087):

  Main Board          = Embedded CodeWarrior TAP (0)   {0x0 0x0}

  Probe Tip           = Power Architecture JTAG/COP    {0x8}

  Firmware            = Boot Loader                    {1.0.1}

  Firmware            = Operating System               {1.0.2}

8087&PID_0024 5&1257EA4F&0&1

8087&PID_0024 5&1257EA4F&0&1

no devices found

0 Kudos
Reply

3,604 Views
addiyi
NXP Employee
NXP Employee

Bill,

Please go to ccs console and type:

% source IDcode.tcl

then specify the connection. After that enter:

% scanboard

and see what ccs return. Yoy should get something like:

TDO -----

        |

        * Device 0  IDCODE: 1192001D  Device: FSL B4420/B4860 rev 2.x

        |

TDI -----

Other method to check the response of the board is (also from ccs):

% config cc cwtap: FSL031A32

% show cc

% ccs::config_chain b4860

If no error is displayed, connection to the board is done.

Adrian

0 Kudos
Reply

3,604 Views
billchadwick
Contributor III

Here is what I get

(bin) 2 % source IDcode.tcl

Scanning for available TAPs connected via USB.....

++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++

+

+      Available Remote Connections

+

+   1 -  CodeWarriorTAP  -  00:04:9f:03:1a:32

+   2 -  CodeWarriorTAP  -  <Specify IP Address>

+   3 -  EthernetTAP  -  <Specify IP Address>

+   4 -  GigabitTAP  -  <Specify IP Address>

+

+   x  - Exit Script without Changes

+

++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++

Specify connection:

1

Configuring TAP Interface....

Configured Connection: cwtap : 00:04:9f:03:1a:32

TDO -----

        |

        * Device 0  IDCODE: FFFFFFFF  Device: Unknown Device

        * Device 1  IDCODE: FFFFFFFF  Device: Unknown Device

        * Device 2  IDCODE: FFFFFFFF  Device: Unknown Device

        * Device 3  IDCODE: FFFFFFFF  Device: Unknown Device

        * Device 4  IDCODE: FFFFFFFF  Device: Unknown Device

        * Device 5  IDCODE: FFFFFFFF  Device: Unknown Device

        * Device 6  IDCODE: FFFFFFFF  Device: Unknown Device

        * Device 7  IDCODE: FFFFFFFF  Device: Unknown Device

        |

TDI -----

###################################################

#

#    configTAP -  Redefine TAP interface

#

#    scanboard -  Scans the target system

#    and returns the JTAG IDCode                

#

#    ir  -  Loopback test

#

###################################################

(bin) 3 % scanboard

TDO -----

        |

        * Device 0  IDCODE: FFFFFFFF  Device: Unknown Device

        * Device 1  IDCODE: FFFFFFFF  Device: Unknown Device

        * Device 2  IDCODE: FFFFFFFF  Device: Unknown Device

        * Device 3  IDCODE: FFFFFFFF  Device: Unknown Device

        * Device 4  IDCODE: FFFFFFFF  Device: Unknown Device

        * Device 5  IDCODE: FFFFFFFF  Device: Unknown Device

        * Device 6  IDCODE: FFFFFFFF  Device: Unknown Device

        * Device 7  IDCODE: FFFFFFFF  Device: Unknown Device

        |

TDI -----

(bin) 4 %

0 Kudos
Reply

3,604 Views
addiyi
NXP Employee
NXP Employee

The cwtap used is the one embedded on b4860qds board, or is an external one? Also, please provide the rev of the board and CPU.

Thanks,

Adrian

0 Kudos
Reply

3,604 Views
billchadwick
Contributor III

I am using the cwtap embedded on the B4860QDS board with a USB connection to my WinXP PC.

The board has two stickers. They read

SCH-27234 Rev C1

and

700-27234 Rev H

The board was provided by Arrow Electronics UK

0 Kudos
Reply

3,604 Views
billchadwick
Contributor III

Underneath the board are two more stickers

K140732944-060

and

TDA4761

0 Kudos
Reply

3,604 Views
catalindemergia
Contributor IV

Hi,

I tried on the embedded tap of a B4860 rev H using ccs from CodeWarrior 10.8.0 build 383

and I got a good response to scanboard. I was thinking, can you try to set the switches so that

you boot the board with the u-boot that comes with it and see if you have the u-boot prompt ?

Catalin

0 Kudos
Reply

3,604 Views
billchadwick
Contributor III

Catalin,

The Quick Start Guide (Rev A2 11/2012) does not explain how to select U-Boot so you are going to have to tell me how.

Do you want me to watch for boot log on the J15 RS232 ? At what Baud Rate ?

My CW is also 10.8.0 Build 383.

Bill.

0 Kudos
Reply

3,604 Views
catalindemergia
Contributor IV

Hi,

You can find at this link

B4860QDS

information about the positioning of switches so that it boots from NOR flash

(but it could be already set to NOR, it's the default)

After that check the boot log on J15 RS232. The baud rate is 115200.

Catalin

0 Kudos
Reply

3,604 Views
billchadwick
Contributor III

Catalin,

Your web portal curtailed my response. The boot log is below in full.

14.10.54 14.10.54 U-Boot 2013.01QorIQ-SDK-V1.5 (Dec 16 2013 - 05:57:03)

14.10.54 CPU0: B4860E, Version: 2.1, (0x86880021)

14.10.54 Core: E6500, Version: 2.0, (0x80400020)

14.10.54 Clock Configuration:

14.10.54 CPU0:1600 MHz, CPU1:1600 MHz, CPU2:1600 MHz, CPU3:1600 MHz,

14.10.54 CCB:666.667 MHz,

14.10.54 DDR:933.333 MHz (1866.667 MT/s data rate) (Asynchronous), IFC:166.667 MHz

14.10.54 FMAN1: 666.667 MHz

14.10.54 QMAN: 333.333 MHz

14.10.54 L1: D-cache 32 kB enabled

14.10.54 I-cache 32 kB enabled

14.10.54 Reset Configuration Word (RCW):

14.10.54 00000000: 140e0018 0f001218 00000000 00000000

14.10.54 00000010: 548d0000 a000a000 dc025000 a9000000

14.10.54 00000020: 01000000 00000000 00000000 0001b1f8

14.10.54 00000030: 00000000 14000020 00000000 00000011

14.10.54 Board: B4860QDS, Sys ID: 0x21, Sys Ver: 0x13, vBank: 0

14.10.54 FPGA: v12 (B4860QDS_1210_2010), build 65280 on Mon Dec 10 18:10:07 2012

14.10.54 SERDES Reference Clocks: Bank1=122.88MHz Bank2=125MHz

14.10.54 I2C: ready

14.10.54 SPI: ready

14.10.54 DRAM: Initializing....using SPD

14.10.54 Detected UDIMM

14.10.54 Detected UDIMM

14.10.54 Not enough bank(chip-select) for CS0+CS1 on controller 1, interleaving disabled!

14.10.54 2 GiB left unmapped

14.10.54 DDR: 4 GiB (DDR3, 64-bit, CL=13, ECC on)

14.10.54 DDR Chip-Select Interleaving Mode: CS0+CS1

14.10.55 VID: VID not used

14.10.55 Setting refclk1:122.88 and refclk2:122.88

14.10.55 SerDes1 Refclks have been set.

14.10.55 IDT configuration not supported for:8d S2 Protocol.

14.10.55 SerDes2 Refclks have been set.

14.10.55 VSC:VSC3316/3308 successfully configured.

14.10.55 Flash: 128 MiB

14.10.55 L2: 2048 KB enabled

14.10.55 Corenet Platform Cache: 1024 KB enabled

14.10.55 Using SERDES1 Protocol: 42 (0x2a)

14.10.55 Using SERDES2 Protocol: 141 (0x8d)

14.10.55 SRIO1: disabled

14.10.55 SRIO2: enabled

14.10.55 NAND: 512 MiB

14.10.55 PCIe1: disabled

14.10.55 In: serial

14.10.55 Out: serial

14.10.55 Err: serial

14.10.55 Net: Initializing Fman

14.10.55 Fman1: Uploading microcode version 106.4.10

14.10.55 PHY reset timed out

14.10.56 PHY reset timed out

14.10.56 FM1@DTSEC3, FM1@DTSEC4, FM1@DTSEC5 , FM1@DTSEC6

14.10.59 Hit any key to stop autoboot: 3 2 1 0

14.10.59 WARNING: adjusting available memory to 30000000

14.10.59 ## Booting kernel from Legacy Image at ec020000 ...

14.10.59 Image Name: Linux-3.8.13-rt9-QorIQ-SDK-V1.5

14.10.59 Created: 2013-12-15 22:01:29 UTC

14.10.59 Image Type: PowerPC Linux Kernel Image (gzip compressed)

14.10.59 Data Size: 4759960 Bytes = 4.5 MiB

14.10.59 Load Address: 00000000

14.10.59 Entry Point: 00000000

14.11.00 Verifying Checksum ... OK

14.11.00 ## Loading init Ramdisk from Legacy Image at ed300000 ...

14.11.00 Image Name: fsl-image-flash-b4860qds-2013121

14.11.00 Created: 2013-12-15 22:26:38 UTC

14.11.00 Image Type: PowerPC Linux RAMDisk Image (gzip compressed)

14.11.00 Data Size: 6765129 Bytes = 6.5 MiB

14.11.00 Load Address: 00000000

14.11.00 Entry Point: 00000000

14.11.02 Verifying Checksum ... OK

14.11.02 ## Flattened Device Tree blob at ec800000

14.11.02 Booting using the fdt blob at 0xec800000

14.11.04 Uncompressing Kernel Image ... OK

14.11.06 Loading Ramdisk to 2f98c000, end 2ffffa49 ... OK

14.11.06 Loading Device Tree to 03fe1000, end 03fffa19 ... OK

14.11.06 Using B4 QDS machine description

14.11.06 MMU: Supported page sizes

14.11.06 4 KB as direct

14.11.06 1024 KB as direct

14.11.06 2048 KB as direct & indirect

14.11.06 4096 KB as direct

14.11.06 16384 KB as direct

14.11.06 65536 KB as direct

14.11.06 262144 KB as direct

14.11.06 1048576 KB as direct

14.11.06 MMU: Book3E HW tablewalk enabled

14.11.06 Found initrd at 0xc00000002f98c000:0xc00000002ffffa49

14.11.06 No /soc@ffe000000/qman@318000 property 'fsl,qman-fqd', using memblock_alloc(0000000000400000)

14.11.06 No /soc@ffe000000/qman@318000 property 'fsl,qman-pfdr', using memblock_alloc(0000000002000000)

14.11.06 Qman ver:0a01,03,01

14.11.06 No /soc@ffe000000/bman@31a000 property 'fsl,bman-fbpr', using memblock_alloc(0000000001000000)

14.11.06 Bman ver:0a02,02,01

14.11.06 No USDPAA memory, no 'usdpaa_mem' bootarg

14.11.06 bootconsole enabled

14.11.06 CPU maps initialized for 2 threads per core

14.11.06 Starting Linux PPC64 #1 SMP Mon Dec 16 06:00:29 CST 2013

14.11.06

0 Kudos
Reply

3,604 Views
catalindemergia
Contributor IV

Hi,

It could be the JTAG clock speed (in CodeWarrior go to your Debug Configuration and Edit Connection, there is a

JTAG clock speed edit box). By putting a bigger value there I managed to reproduce the "core not supported" message

in my setup. So, set the value that you have to something smaller. In my setup it works with 10230 kHz.

Catalin

0 Kudos
Reply

3,600 Views
billchadwick
Contributor III

I have

and

0 Kudos
Reply

3,600 Views
catalindemergia
Contributor IV

Hi,

can you check one more thing - enter the commands like bellow (in ccs console) and

see if you have the same output.

(bin) 51 % dele a

(bin) 52 % config cc cwtap

(bin) 53 % show cc

0: CodeWarrior TAP (cwtap) CC software ver. {0.0}

(bin) 54 %

(bin) 54 % ::ccs::config_server 0 1000

(bin) 55 % ::ccs::config_chain t4amp

(bin) 56 % ::ccs::all_run_mode

t4amp: Debug Mode

e6500_thread0: Debug Mode

e6500_thread1: Debug Mode

e6500_thread0: Debug Mode

e6500_thread1: Debug Mode

e6500_thread0: Debug Mode

e6500_thread1: Debug Mode

e6500_thread0: Debug Mode

e6500_thread1: Debug Mode

sc3900: Debug Mode

sc3900: Debug Mode

sc3900: Debug Mode

sc3900: Debug Mode

sc3900: Debug Mode

sc3900: Debug Mode

Catalin

0 Kudos
Reply

3,600 Views
billchadwick
Contributor III

I get

(bin) 7 % dele a

(bin) 8 % config cc cwtap

(bin) 9 % show cc

0: CodeWarrior TAP (cwtap) CC software ver. {0.0}

(bin) 10 % ::ccs::config_server 0 1000

(bin) 11 % ::ccs::config_chain t4amp

T4AMP SoC: Core not responding

(bin) 12 %

0 Kudos
Reply

3,600 Views
addiyi
NXP Employee
NXP Employee

Could you please check if the SW settings are the same as in link provided by Catalin? If your board have other SW settings please use the one from info center and try again, If the Core not responding issue is still present, it is very possible ecwtap is defect.


Adrian

0 Kudos
Reply

3,600 Views
billchadwick
Contributor III

With my second board I look to be getting a bit further

CodeWarrior Connection Server console display active (Tcl8.4.12 / Tk8.4.12)

Loading CCSAPI Tcl interface (C:/Freescale/CW_SC_v10.8.0/SC/ccs/bin/ccstcl.dll)...

Loading Svfburner (C:/Freescale/CW_SC_v10.8.0/SC/ccs/bin/svfburner.dll)...

There are no command converters configured

Server listening on port: 41475

Clients allowed from all hosts

No clients denied

(bin) 1 % findcc cwtaps -verbose

FSL031A4A (00:04:9f:03:1a:4a:1087):

Main Board = Embedded CodeWarrior TAP (0) {0x0 0x0}

Probe Tip = Power Architecture JTAG/COP

Firmware = Boot Loader {0.9.2}

Firmware = Operating System {1.0.1}

8087&PID_0024 5&1257EA4F&0&1

8087&PID_0024 5&1257EA4F&0&1

no devices found

(bin) 2 %

(bin) 3 % updatecwtap FSL031A4A

FSL031A4A is running OS version 1.0.1

Update contains OS version 1.0.2

WARNING: UPDATING FLASH - DO NOT INTERRUPT!

Sending code to CodeWarrior TAP.........done

Running package script

Erasing kernel partition...

Flashing kernel partition...

Erasing root1 partition...

Flashing root1 partition...

Activating root1

Update completed; rebooting.

Waiting for reboot...

FSL031A4A is running Boot Loader version 0.9.2

Update contains Boot Loader version 1.0.1

WARNING: UPDATING FLASH - DO NOT INTERRUPT!

Sending code to CodeWarrior TAP.........done

Running package script

Erasing uboot partition...

Flashing uboot partition...

Update completed; rebooting.

Waiting for reboot...

All updates completed successfully.

(bin) 4 % source IDcode.tcl

Scanning for available TAPs connected via USB.....

++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++

+

+ Available Remote Connections

+

+ 1 - CodeWarriorTAP - 00:04:9f:03:1a:4a

+ 2 - CodeWarriorTAP -

+

+ x - Exit Script without Changes

+

++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++

Specify connection:

1

Configuring TAP Interface....

Configured Connection: cwtap : 00:04:9f:03:1a:4a

CodeWarrior TAP Boot Loader version 1.0.1

CodeWarrior TAP OS version 1.0.2

Sending code to CodeWarrior TAP.........done

Running package script

TDO

0 Kudos
Reply