Function of net "GPIO_CKE_ISO" in "T1040RDB_Rev_B" design

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Function of net "GPIO_CKE_ISO" in "T1040RDB_Rev_B" design

Jump to solution
482 Views
abhijit_pethkar
Contributor II

We are using the design "T1040RDB_Rev_B" for our design reference. I would like to know what is the function of the net "GPIO_CKE_ISO" in this design. 

Also the net is supposed to be working at LVDD 2.5V and the processor is not configured for LVDD 1.8V. What is the reason? I felt that if LVDD was configured for 2.5V the interfacing would have been easier.

0 Kudos
1 Solution
439 Views
ufedor
NXP Employee
NXP Employee

The "GPIO_CKE_ISO" is not functional in the design.

You wrote:

> net is supposed to be working at LVDD 2.5V

Which "net"?

View solution in original post

1 Reply
440 Views
ufedor
NXP Employee
NXP Employee

The "GPIO_CKE_ISO" is not functional in the design.

You wrote:

> net is supposed to be working at LVDD 2.5V

Which "net"?