Execute in place in iMX6 sabrelite

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Execute in place in iMX6 sabrelite

406 Views
abanwer
Contributor I

Hi, I am working on a bootloader for sabrelite board. We have a 2MB NOR flash on this board. Do we have support for Execute in place in sabrelite?

0 Kudos
1 Reply

340 Views
art
NXP Employee
NXP Employee

The code, located in the parallel NOR Flash memory, can be executed in place, but the execution speed will be much more slower than executing the code from RAM. For other types of NOR Flash memory (e.g. SPI NOR) the execution in place is not supported.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos