Ethernet connection on T1040RDB evaluation board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ethernet connection on T1040RDB evaluation board

Jump to solution
841 Views
steffendedekind
Contributor II

Hi all,

I currently try to "quickle" run some indivdual test and benchmark code on the T1040RDB evaluation board I currently have. Unfortunately the currently installed kernel does not include any coepages needed to use MMC cards or USB sticks. And I have no clue how to get the network working - there are several interfaces:

root@t1040rdb:~# ip link show

1: lo: <LOOPBACK,UP,LOWER_UP> mtu 65536 qdisc noqueue state UNKNOWN mode DEFAULT

    link/loopback 00:00:00:00:00:00 brd 00:00:00:00:00:00

2: fm1-gb0: <BROADCAST,MULTICAST,UP,LOWER_UP> mtu 1500 qdisc mq state UNKNOWN mode DEFAULT qlen 1000

    link/ether 00:04:9f:03:3a:97 brd ff:ff:ff:ff:ff:ff

3: fm1-gb1: <BROADCAST,MULTICAST,UP,LOWER_UP> mtu 1500 qdisc mq state UNKNOWN mode DEFAULT qlen 1000

    link/ether 00:04:9f:03:3a:98 brd ff:ff:ff:ff:ff:ff

4: fm1-gb2: <NO-CARRIER,BROADCAST,MULTICAST,UP> mtu 1500 qdisc mq state DOWN mode DEFAULT qlen 1000

    link/ether 00:04:9f:03:3a:99 brd ff:ff:ff:ff:ff:ff

5: fm1-gb3: <BROADCAST,MULTICAST,UP,LOWER_UP> mtu 1500 qdisc mq state UP mode DEFAULT qlen 1000

    link/ether 00:04:9f:03:3a:9a brd ff:ff:ff:ff:ff:ff

6: fm1-gb4: <NO-CARRIER,BROADCAST,MULTICAST,UP> mtu 1500 qdisc mq state DOWN mode DEFAULT qlen 1000

    link/ether 00:04:9f:03:3a:9b brd ff:ff:ff:ff:ff:ff

7: tunl0: <NOARP> mtu 1480 qdisc noop state DOWN mode DEFAULT

    link/ipip 0.0.0.0 brd 0.0.0.0

8: sit0: <NOARP> mtu 1480 qdisc noop state DOWN mode DEFAULT

    link/sit 0.0.0.0 brd 0.0.0.0

9: ip6tnl0: <NOARP> mtu 1452 qdisc noop state DOWN mode DEFAULT

    link/tunnel6 :: brd ::

root@t1040rdb:~#

My cable is connected to "ETH0" (labled on the eval boards case) - but even if I bring up fm1-gb0-4 with different IPs (and the default route is also present, MAC addresses are properly set) I'm not able to connect or ping the board. If I try a "ping" in the uboot promt it tries different interfaces (FM1@DTSEC2, FM1@DTSEC3, FM1@DTSEC4) and it tells me finally

Using FM1@DTSEC4 device

host 192.168.1.1 is alive

On Freescales homepage I haven't found any useful documentation.

Anyone can help with this?

Tags (2)
0 Kudos
1 Solution
657 Views
steffendedekind
Contributor II

Seems to be solved in the moment of writing :smileywink:

If I noticed correctly one has to use "ifconfig ...up" before plugin the ethernet cabe! Otherwise around it does not work.

root@t1040rdb:~# ifconfig fm1-gb3 192.168.1.23 up

... plug in ethernet cable ...

root@t1040rdb:~# ifconfig

fm1-gb3  Link encap:Ethernet  HWaddr 00:04:9f:03:3a:9a

          inet addr:192.168.1.23  Bcast:192.168.1.255  Mask:255.255.255.0

          inet6 addr: fe80::204:9fff:fe03:3a9a/64 Scope:Link

          UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1

          RX packets:0 errors:0 dropped:17 overruns:0 frame:0

          TX packets:5 errors:0 dropped:0 overruns:0 carrier:0

          collisions:0 txqueuelen:1000

          RX bytes:0 (0.0 B)  TX bytes:398 (398.0 B)

          Memory:fe4e6000-fe4e6fff

lo        Link encap:Local Loopback

          inet addr:127.0.0.1  Mask:255.0.0.0

          inet6 addr: ::1/128 Scope:Host

          UP LOOPBACK RUNNING  MTU:65536  Metric:1

          RX packets:0 errors:0 dropped:0 overruns:0 frame:0

          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0

          collisions:0 txqueuelen:0

          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

root@t1040rdb:~# route

Kernel IP routing table

Destination    Gateway        Genmask        Flags Metric Ref    Use Iface

192.168.1.0    *              255.255.255.0  U    0      0        0 fm1-gb3

root@t1040rdb:~# ping 192.168.1.1

PING 192.168.1.1 (192.168.1.1): 56 data bytes

64 bytes from 192.168.1.1: icmp_seq=0 ttl=128 time=0.846 ms

64 bytes from 192.168.1.1: icmp_seq=1 ttl=128 time=0.388 ms

64 bytes from 192.168.1.1: icmp_seq=2 ttl=128 time=0.373 ms

64 bytes from 192.168.1.1: icmp_seq=3 ttl=128 time=0.365 ms

64 bytes from 192.168.1.1: icmp_seq=4 ttl=128 time=0.370 ms

--- 192.168.1.1 ping statistics ---

5 packets transmitted, 5 packets received, 0% packet loss

round-trip min/avg/max/stddev = 0.365/0.468/0.846/0.189 ms

root@t1040rdb:~#

View solution in original post

0 Kudos
1 Reply
658 Views
steffendedekind
Contributor II

Seems to be solved in the moment of writing :smileywink:

If I noticed correctly one has to use "ifconfig ...up" before plugin the ethernet cabe! Otherwise around it does not work.

root@t1040rdb:~# ifconfig fm1-gb3 192.168.1.23 up

... plug in ethernet cable ...

root@t1040rdb:~# ifconfig

fm1-gb3  Link encap:Ethernet  HWaddr 00:04:9f:03:3a:9a

          inet addr:192.168.1.23  Bcast:192.168.1.255  Mask:255.255.255.0

          inet6 addr: fe80::204:9fff:fe03:3a9a/64 Scope:Link

          UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1

          RX packets:0 errors:0 dropped:17 overruns:0 frame:0

          TX packets:5 errors:0 dropped:0 overruns:0 carrier:0

          collisions:0 txqueuelen:1000

          RX bytes:0 (0.0 B)  TX bytes:398 (398.0 B)

          Memory:fe4e6000-fe4e6fff

lo        Link encap:Local Loopback

          inet addr:127.0.0.1  Mask:255.0.0.0

          inet6 addr: ::1/128 Scope:Host

          UP LOOPBACK RUNNING  MTU:65536  Metric:1

          RX packets:0 errors:0 dropped:0 overruns:0 frame:0

          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0

          collisions:0 txqueuelen:0

          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

root@t1040rdb:~# route

Kernel IP routing table

Destination    Gateway        Genmask        Flags Metric Ref    Use Iface

192.168.1.0    *              255.255.255.0  U    0      0        0 fm1-gb3

root@t1040rdb:~# ping 192.168.1.1

PING 192.168.1.1 (192.168.1.1): 56 data bytes

64 bytes from 192.168.1.1: icmp_seq=0 ttl=128 time=0.846 ms

64 bytes from 192.168.1.1: icmp_seq=1 ttl=128 time=0.388 ms

64 bytes from 192.168.1.1: icmp_seq=2 ttl=128 time=0.373 ms

64 bytes from 192.168.1.1: icmp_seq=3 ttl=128 time=0.365 ms

64 bytes from 192.168.1.1: icmp_seq=4 ttl=128 time=0.370 ms

--- 192.168.1.1 ping statistics ---

5 packets transmitted, 5 packets received, 0% packet loss

round-trip min/avg/max/stddev = 0.365/0.468/0.846/0.189 ms

root@t1040rdb:~#

0 Kudos