Ethernet Independent mode in DPAA QorIQ processors

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Ethernet Independent mode in DPAA QorIQ processors

跳至解决方案
2,124 次查看
talhaimran
Contributor II

I am implementing Ethernet independent mode in DPAA, Does independent DPAA mode require FMan ucode?

标记 (5)
1 解答
1,768 次查看
bpe
NXP Employee
NXP Employee

Yes, FMan microcode is required for FMan Independent mode.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
1,769 次查看
bpe
NXP Employee
NXP Employee

Yes, FMan microcode is required for FMan Independent mode.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,768 次查看
talhaimran
Contributor II

Thanks Paton. One more thing I am confused about is the MDIO interface present in the Fman controller. If we use the internal MDIO interface for each MAC we access the MDIO registers of SERDES which automatically reports the the AN as complete and link status as up, even if no cable is attached to port. While if we use the external MDIO interface and access the PHY for same MAC then we access the standard PHY register which reports correct link and auto negotiation status. So what link status are the SERDES MDIO registers referring to?

0 项奖励
回复