ETA for Yocto 2.3 based QorIQ SDK?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ETA for Yocto 2.3 based QorIQ SDK?

1,282 Views
kuta42
Contributor III

Is there an ETA for when will there be a QorIQ SDK that's based on Yocto 2.3? I am not so much interested in a newer kernel, but rather in the newer versions of the other components, especially the toolchain, that Yocto 2.3 supplies. Thanks.

      ~=Herb=~

Tags (1)
0 Kudos
Reply
3 Replies

1,173 Views
Pavel
NXP Employee
NXP Employee

Look at information about LSDK on the following page:

https://www.nxp.com/support/developer-resources/run-time-software/linux-sdk/layerscape-software-deve...


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,173 Views
Pavel
NXP Employee
NXP Employee

Usually new version of NXP SDK contains new kernel version.

There is no information about Yocto version in new SDK verion.  

Perhaps this SDK will not be based on Yocto.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,173 Views
kuta42
Contributor III

Is there an ETA for the next release of the SDK for the LS1012A?

0 Kudos
Reply