Hello!
Dose P2020 support 1000base-X? I can not find detail descriptions about 1000Base-X in the RM.
If P2020 dose support 1000Base-X, how can I config it?
Thanks!
1000Base-X is supported.
Please refer to the AN3869 - Implementing SGMII Interfaces on the PowerQUICC™ III:
https://www.nxp.com/webapp/Download?colCode=AN3869&location=null
Thanks a lot.
So, it means that P2020 can use Serdes to connect with other devices (such as another P2020) point-to-point, and can delete SGMII PHY?
AN3869 refers to PQ3, and P2020 is a QorIQ processor. Are they the same feature?
1) Correct.
2) The AN is applicable for the P2020 as well.
Thank you very much for your prompt reply!