Does the TWR board support SATA?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does the TWR board support SATA?

3,139 Views
hwei
Contributor III

I get an ls1021a TWR board, and there is "SATA basic support" in SDK 1.2 RN, but how to enable this SATA support?

I have tried to change SW3[6], but the result is still the same:

SATA link 0 timeout.

AHCI 0001.0300 1 slots 1 ports ? Gbps 0x1 impl SATA mode

flags: 64bit ncq pm clo only pmp fbss pio slum part ccc

scanning bus for devices...

Found 0 device(s).

Besides that, I cannot access any SATA devices in kernel too.

Does the TWR board come with SATA support? If so, how to enable it in u-boot and kernel?

Thanks

Tags (3)
0 Kudos
Reply
9 Replies

2,551 Views
sinanakman
Senior Contributor III

I just took a look at what comes with SDK images. On the SDK

use one of the images in ls1021atwr/rcw/RSR_PPS_70. In that

directory name 70 refers to Serdes Protocol 0x70 and it enables

SATA1 on Lane B. Use one of these images as your RCW and boot

your board with it. You should be able to see SATA enabled.

Regards

Sinan Akman

0 Kudos
Reply

2,551 Views
hwei
Contributor III

Hi Sinan,

Thanks for your reply.

I have tried to set Serdes Protocol to 0x70, but I still get the same result:

U-Boot 2014.01Layerscape-SDK-V1.1+g2b4d7d7 (Aug 29 2014 - 11:57:41)

CPU:   Freescale LayerScape LS1021E, Version: 1.0, (0x87081110)

Clock Configuration:

       CPU0(ARMV7):1000 MHz,

       Bus:300  MHz, DDR:800  MHz (1600 MT/s data rate),

Reset Configuration Word (RCW):

       00000000: 0608000a 00000000 00000000 00000000

       00000010: 70000000 00407900 e0025a00 21046000

       00000020: 00000000 00000000 00000000 00038000

       00000030: 00080000 881b7340 00000000 00000000

Board: LS1021ATWR

CPLD:  V2.3

PCBA:  V3.0

VBank: 0

I2C:   ready

DRAM:  1 GiB (DDR3, 32-bit, CL=10, ECC off)

Using SERDES1 Protocol: 112 (0x70)

Flash: 128 MiB

MMC:   FSL_SDHC: 0

EEPROM: NXID v1

Firmware 'Microcode version 0.0.0 for T1040 r1.0' for 1040 V1.0

QE: uploading microcode 'Microcode for T1040 r1.0'

In:    serial

Out:   serial

Err:   serial

SATA link 0 timeout.

AHCI 0001.0300 1 slots 1 ports ? Gbps 0x1 impl SATA mode

flags: 64bit ncq pm clo only pmp fbss pio slum part ccc

scanning bus for devices...

Found 0 device(s).

Net:   eTSEC2 is in sgmii mode.

eTSEC1 [PRIME], eTSEC2, eTSEC3

Hit any key to stop autoboot:  0

=> scsi scan

scanning bus for devices...

Found 0 device(s).

I still cannot figure it out.

0 Kudos
Reply

2,551 Views
sinanakman
Senior Contributor III

Hi H Wei

OK, I have to debug this and see what that SDK uboot has implemented.

Meanwhile, I am just curious, are you getting similar results with Linux

kernel as well ?

Regards

Sinan Akman

0 Kudos
Reply

2,551 Views
hwei
Contributor III

Hi Sinan,

No matter what I try, the result in kernel is still:

root@ls1021atwr:~# ls /dev/sd*

ls: /dev/sd*: No such file or directory

Thanks

0 Kudos
Reply

2,551 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello H Wei,

In the recent LS1021A Linux SDK(1.2), only Sata disk detecting is supported in u-boot, SATA Linux driver is under developing now.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,551 Views
hwei
Contributor III

Hi Yiping,

Does the SATA drive get supported in SDK 1.7?

I find it still doesn't work on my board.

Thanks

0 Kudos
Reply

2,551 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello H Wei,


SATA 3.0 doesn't get support in SDK 1.7, it is still under investigation.

Thanks,

Yiping

0 Kudos
Reply

2,551 Views
sinanakman
Senior Contributor III

Hi H Wei, you will probably have to make sure SRDS_PRTCL_S1[128:135] RCW

value is set accordingly for SerDes protocol that configures the board to use SATA. I am

not sure if there is a prebuilt RCW image available for this as part of SDK at this

point.

Hope this helps.

Sinan Akman

2,551 Views
sinanakman
Senior Contributor III

Hi H Wei

What RCW are you using to test out your SATA ?

Regards

Sinan Akman

0 Kudos
Reply