Device Tree Binding for Marvell DSA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Device Tree Binding for Marvell DSA

1,696 Views
kesav123
Contributor I

Hi,

was there any patch available for the below mentioned issue ? I was facing the same problem (using linux-fsl-sdk-v1.6) with a different board.

dev_to_net_device() (net/dsa/dsa.c) is failing for the fsl Ethernet driver. It looks like , it works fine for other in-tree Ethernet drivers. Looking for some help here !!!

Link to the description of issue.

Re: Device Tree Binding for Marvell DSA on P1023RDB — Linux Network Development

-Thnx,

Kesav.

Tags (2)
0 Kudos
Reply
1 Reply

964 Views
jagsgediya
Contributor II

Hi Kesav,

We are using the marvell 88e6065 switch with the imx6 processor. If you have successfully configured the marvell switch related changes in the device tree then could you please share it?

Thanks,

jags

0 Kudos
Reply